Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum creating templates with Circuitstudio
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 2 replies
  • Subscribers 89 subscribers
  • Views 3718 views
  • Users 0 members are here
  • circuitstudio
  • circuit studio
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

creating templates with Circuitstudio

kiyoshi7
kiyoshi7 over 5 years ago

Hi, I`m trying to create a template, which I can choose when creating a project with some schematic sheets and a pcb layout. Can someone tell me how to do this? On kicad I would just have to save my project to a directory with some other documents, but I cannot find out how to do this with CS.

 

 

any help is appreciated thanks for reading.

  • Cancel
Parents
  • tlc8126
    tlc8126 over 5 years ago

    Hi Kiyoshi7,

     

    There are several ways I create templates, but the easiest for me is to open one of the files in the Templates folder. If you installed CS to the default directories this would be:

     

           \Users\Public\Public Documents\Altium\CS\Templates\

     

    Schematic templates have the extension "SchDot". In CS you can just go to the File tab and select "Open Document..." from the drop down menu. From there go to the Templates directory and open the template that is closest to the one you want to create. Make sure you immediately save it as a New Filename to keep from overwriting the original. And if you don't see the "*.SchDot" files check that the "All files (*.*)" type is selected in the drop down list above the "Open" and "Cancel" buttons in the lower right of the "Choose Document to Open" dialog box.

     

    Opening a "SchDot" file in CS will allow you to create, edit, or update Title Blocks and Revision Blocks, as well as add new Text Fields, etc., to a Schematic Template of your own design - just as if you were editing any typical schematic or component symbol. (It's like having a Symbol Editor just for Schematic Templates!)

     

    Once the new SchDot file is created you can select it from the "Templates" tab of any Schematic Sheets "Document Options..." dialog box. Or make it the default Schematic Template by selecting it in the System Preferences \ Schematic \ General \ Defaults \ Template selection list.

     

    P.S. I forgot to mention that CircuitStudio ("CS") has Schematic Templates, PCB Layout Templates, and Project Templates. Use the 'Open Document...' menu item mentioned above to open either SchDot or CSPcbDoc files in the Templates folder to get an idea of what they are.

     

    And if you want to make a 'Project Template', just create a SchDot and CSPcbDoc file and add them to a normal Project using the 'Add Existing to Project..." pop-up menu item when you right-click on the Projects "*.PrjPcb" file in the Projects panel. Next, save the Schematic as a normal schematic document file ("*.SchDoc"). Save the PCB using the normal extension, which is the same as the PCB Template - "CSPcbDoc". Lastly, save the project. (The Schematic, PCB, and Project files should all have the same name when you save them in the the new PCB Project. )

     

    From this new project folder you can copy out the "*.SchDoc", "*.CSPcbDoc", and "*.PrjPcb" files and place them into the "PCB Projects" sub-folder in the Templates folder mentioned above. (An EMF file is also part of the default Projects provided by Altium and represent  an "Enhanced MetaFile" - i.e. Graphics - that is displayed in the "Create New Project From Template" dialog when you create a new Project. You don't need an EMF file, but if you know about creating graphics you can try to create one and add it to the PCB Projects directory, too.) Finally, edit the "PCB Project Templates.ini" file to add your new Project Template (Just copy one of the existing PCB Projects in the file and edit it to reflect your new Project Template). The next time you create a new Project from the "New PCB Project..." menu item of the main menu File tab you should see your new Template project listed.

     

    Good Luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • tlc8126
    tlc8126 over 5 years ago

    Hi Kiyoshi7,

     

    There are several ways I create templates, but the easiest for me is to open one of the files in the Templates folder. If you installed CS to the default directories this would be:

     

           \Users\Public\Public Documents\Altium\CS\Templates\

     

    Schematic templates have the extension "SchDot". In CS you can just go to the File tab and select "Open Document..." from the drop down menu. From there go to the Templates directory and open the template that is closest to the one you want to create. Make sure you immediately save it as a New Filename to keep from overwriting the original. And if you don't see the "*.SchDot" files check that the "All files (*.*)" type is selected in the drop down list above the "Open" and "Cancel" buttons in the lower right of the "Choose Document to Open" dialog box.

     

    Opening a "SchDot" file in CS will allow you to create, edit, or update Title Blocks and Revision Blocks, as well as add new Text Fields, etc., to a Schematic Template of your own design - just as if you were editing any typical schematic or component symbol. (It's like having a Symbol Editor just for Schematic Templates!)

     

    Once the new SchDot file is created you can select it from the "Templates" tab of any Schematic Sheets "Document Options..." dialog box. Or make it the default Schematic Template by selecting it in the System Preferences \ Schematic \ General \ Defaults \ Template selection list.

     

    P.S. I forgot to mention that CircuitStudio ("CS") has Schematic Templates, PCB Layout Templates, and Project Templates. Use the 'Open Document...' menu item mentioned above to open either SchDot or CSPcbDoc files in the Templates folder to get an idea of what they are.

     

    And if you want to make a 'Project Template', just create a SchDot and CSPcbDoc file and add them to a normal Project using the 'Add Existing to Project..." pop-up menu item when you right-click on the Projects "*.PrjPcb" file in the Projects panel. Next, save the Schematic as a normal schematic document file ("*.SchDoc"). Save the PCB using the normal extension, which is the same as the PCB Template - "CSPcbDoc". Lastly, save the project. (The Schematic, PCB, and Project files should all have the same name when you save them in the the new PCB Project. )

     

    From this new project folder you can copy out the "*.SchDoc", "*.CSPcbDoc", and "*.PrjPcb" files and place them into the "PCB Projects" sub-folder in the Templates folder mentioned above. (An EMF file is also part of the default Projects provided by Altium and represent  an "Enhanced MetaFile" - i.e. Graphics - that is displayed in the "Create New Project From Template" dialog when you create a new Project. You don't need an EMF file, but if you know about creating graphics you can try to create one and add it to the PCB Projects directory, too.) Finally, edit the "PCB Project Templates.ini" file to add your new Project Template (Just copy one of the existing PCB Projects in the file and edit it to reflect your new Project Template). The next time you create a new Project from the "New PCB Project..." menu item of the main menu File tab you should see your new Template project listed.

     

    Good Luck!