Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Top layer pad with hole
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 11 replies
  • Subscribers 88 subscribers
  • Views 2506 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Top layer pad with hole

ffb.boy.30
ffb.boy.30 over 3 years ago

Hi,

I've an old Altium (2016) and I would like to create a top layer pad with a hole.

Actually, when I create a top layer pad the hole disappear.

My goal is to create a 0.8mm pad with a hole of 0.4mm.

The bottom of my pcb will be in contact with metal that why I don't want to use multilayer pad

Thanks for your help

  • Cancel

Top Replies

  • GabeFromSpace
    GabeFromSpace over 3 years ago +1
    Out of sheer curiosity, why do you need this hole on the pad? Is it a test point for a multimeter probe or test fixture? If you need a via to get the signal to another layer, why not just tent the via…
Parents
  • opeongo80
    opeongo80 over 3 years ago

    I solved a similar problem by just making a NP hole and then on the top layer using the circle/arc placement

    and then adjusting the arc track width to the diameter that you want.

    You then adjust the arc radius until it is slightly larger that the hole.

    You will probably have to then reduce the arc width to suit.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • ffb.boy.30
    ffb.boy.30 over 3 years ago in reply to opeongo80

    I like your idea. I've tried to create the hole with a cutout but it don't work.

    How do you make your hole ?

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • opeongo80
    opeongo80 over 3 years ago in reply to ffb.boy.30

    Just make a hole/pad dia. 0.4mm and make sure it is unplated, like an unplated mounting hole.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • opeongo80
    opeongo80 over 3 years ago in reply to ffb.boy.30

    Just make a hole/pad dia. 0.4mm and make sure it is unplated, like an unplated mounting hole.