Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Top layer pad with hole
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 11 replies
  • Subscribers 88 subscribers
  • Views 2506 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Top layer pad with hole

ffb.boy.30
ffb.boy.30 over 3 years ago

Hi,

I've an old Altium (2016) and I would like to create a top layer pad with a hole.

Actually, when I create a top layer pad the hole disappear.

My goal is to create a 0.8mm pad with a hole of 0.4mm.

The bottom of my pcb will be in contact with metal that why I don't want to use multilayer pad

Thanks for your help

  • Cancel

Top Replies

  • GabeFromSpace
    GabeFromSpace over 3 years ago +1
    Out of sheer curiosity, why do you need this hole on the pad? Is it a test point for a multimeter probe or test fixture? If you need a via to get the signal to another layer, why not just tent the via…
Parents
  • GabeFromSpace
    GabeFromSpace over 3 years ago

    Out of sheer curiosity, why do you need this hole on the pad? Is it a test point for a multimeter probe or test fixture? If you need a via to get the signal to another layer, why not just tent the via?

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • ffb.boy.30
    ffb.boy.30 over 3 years ago in reply to GabeFromSpace

    No I just need to solder a wire that come from the other side of the pcb . The wire need to pass throught the metal and the pcb, and the pcb is glue to the métal . It is a led pcb

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to ffb.boy.30

    Given that, does the wire actually need to solder to a pad around the hole or could it extend a bit further to a pad on the board away from the hole?  That sounds do-able without stressing the PCB manufacturers.  With such a small hole, soldering the wire so close to it could well wick solder down and bridge to the metal plate.

    Would it be possible to cut a groove through the surface of one of the blocks sides to sit the wire in (deep enough so it is flush, the wire can’t be too heavy gauge if a 0.8mm hole suffices) and bring it to the top of the board and a pad without using a hole? 

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • Andrew J
    Andrew J over 3 years ago in reply to ffb.boy.30

    Given that, does the wire actually need to solder to a pad around the hole or could it extend a bit further to a pad on the board away from the hole?  That sounds do-able without stressing the PCB manufacturers.  With such a small hole, soldering the wire so close to it could well wick solder down and bridge to the metal plate.

    Would it be possible to cut a groove through the surface of one of the blocks sides to sit the wire in (deep enough so it is flush, the wire can’t be too heavy gauge if a 0.8mm hole suffices) and bring it to the top of the board and a pad without using a hole? 

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • ffb.boy.30
    ffb.boy.30 over 3 years ago in reply to Andrew J

    Unfortunately the LED is 3x3 and my PCB is a round 5.6.

    I've found the solution. Making a circle to create the pad and I will make the hole by myself it is not a problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • ffb.boy.30
    ffb.boy.30 over 3 years ago in reply to ffb.boy.30

    I've make it like this , uggly but it will do the job.