Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Trying to create a component with different numbers of pins
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 2 replies
  • Subscribers 88 subscribers
  • Views 752 views
  • Users 0 members are here
  • altium
  • circuitstudio
  • libraries
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Trying to create a component with different numbers of pins

GoobFromSpace
GoobFromSpace over 2 years ago

I've made a library component for the Attinyxx26, but the component comes in 3 packages. 2 have 20 pins. The 3rd has 21 pins from a thermal pad. I'd like to have 1 library component that I can switch between the 3 footprints. Is there any way to do this without

1: having the thermal pad also be set as pin 20

2: The software complaining about extra pins when it compiles

  • Cancel

Top Replies

  • GoobFromSpace
    GoobFromSpace over 2 years ago in reply to aswinvenu +1
    The "xx" is a variable for the amount of memory. One of the full part numbers is Attiny3226. There's a 20 pin SOIC, a 20 pin SSOP, and a 20 pin + thermal pad VQFN. ww1.microchip.com/.../ATtiny3224-3226…
Parents
  • aswinvenu
    0 aswinvenu over 2 years ago

    From a quick search I can see Attiny26 comes in 20 pin PDIP and SOIC. The third option is a 32pin QFN. Am I missing something here?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • GoobFromSpace
    0 GoobFromSpace over 2 years ago in reply to aswinvenu

    The "xx" is a variable for the amount of memory. One of the full part numbers is Attiny3226. There's a 20 pin SOIC, a 20 pin SSOP, and a 20 pin + thermal pad VQFN.

    ww1.microchip.com/.../ATtiny3224-3226-3227-Data-Sheet-DS40002345A.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • GoobFromSpace
    0 GoobFromSpace over 2 years ago in reply to aswinvenu

    The "xx" is a variable for the amount of memory. One of the full part numbers is Attiny3226. There's a 20 pin SOIC, a 20 pin SSOP, and a 20 pin + thermal pad VQFN.

    ww1.microchip.com/.../ATtiny3224-3226-3227-Data-Sheet-DS40002345A.pdf