Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Capacitors connected GND to GND
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 7 replies
  • Subscribers 93 subscribers
  • Views 4506 views
  • Users 0 members are here
  • rf adc
  • adc to fmc
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Capacitors connected GND to GND

saravananeceait
saravananeceait over 8 years ago

Why capcitors connected Ground to ground ? what is the need? and what is the value of these capacitors?

Attachments:
image
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +5
    Hi, It's just to get rid of any static charges, when the board is inserted into the chassis. This is because the edge is going to be the first bit that touches the chassis, and the capacitors have physically…
  • adamwebber
    adamwebber over 8 years ago +2
    Just a wild guess but maybe there are two isolated grounds on the PCB. Also, this forum is not necessarily for circuit-technical questions. It's pretty much for CircuitStudio-related questions.
  • jw0752
    jw0752 over 8 years ago +1
    Your question came through on main Forum Stream too so there is a pretty good chance that someone smarter than me will respond. What makes you think that both sides of the capacitor are connected to ground…
Parents
  • shabaz
    shabaz over 8 years ago

    Hi,

     

    It's just to get rid of any static charges, when the board is inserted into the chassis. This is because the edge is going to be the first bit that touches the chassis, and the capacitors have physically been placed with one end close to the chassis, and the other end connected to the PCB ground. As rachaelp says, its for the AC signal, that brief spike and then in theory the board ground and the chassis ground should be at a closer potential. Sometimes there is a parallel resistor too (>1M), to provide a high impedance DC path. In the duplicate thread (which makes it awkward to provide a good response, because it is only by chance that I saw it), it showed the portion of the schematic, with the ground connection on each side. However, it should have been drawn better, with a different symbol on each side to show the difference between board ground and chassis ground.

    • Cancel
    • Vote Up +5 Vote Down
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago

    Hi,

     

    It's just to get rid of any static charges, when the board is inserted into the chassis. This is because the edge is going to be the first bit that touches the chassis, and the capacitors have physically been placed with one end close to the chassis, and the other end connected to the PCB ground. As rachaelp says, its for the AC signal, that brief spike and then in theory the board ground and the chassis ground should be at a closer potential. Sometimes there is a parallel resistor too (>1M), to provide a high impedance DC path. In the duplicate thread (which makes it awkward to provide a good response, because it is only by chance that I saw it), it showed the portion of the schematic, with the ground connection on each side. However, it should have been drawn better, with a different symbol on each side to show the difference between board ground and chassis ground.

    • Cancel
    • Vote Up +5 Vote Down