Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum wasted ability to choose different footprints?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 9 replies
  • Subscribers 90 subscribers
  • Views 1136 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

wasted ability to choose different footprints?

Sparkylabs
Sparkylabs over 8 years ago

The ability to assign multiple footprints to a part is nice but it immediately creates a conflict for BOM's as supplier links or other ordering information entered into the parts "parameters" become useless as for example I could create an opamp part and assign both DIP8 and SOIC8 footprints to it but there is as far as I know, no way to assign different parameters based on footprints. Is this correct or is there some functionality I don't know about?

  • Cancel
Parents
  • Sparkylabs
    Sparkylabs over 8 years ago

    Well if that is the case the only way to keep them separate is to have separate symbols which is a little silly as now the the schematic symbol library is no longer driven by part functionality but by both part functionality and footprint. I rather liked the idea of being able to place a part and then alter the footprint if required, but it makes no sense.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tarribred61
    tarribred61 over 8 years ago in reply to Sparkylabs

    On the other hand, this is useful if I want to use multiple footprints for the same package.  For example, if I use an EIA0603 resistor and I want to choose from the least, most or nominal solder options then I can just have the various footprints available. Then I can choose the proper footprint depending on whether the board is reflow or wave or hand soldered. I would argue that the SOIC, MSOP, TSSOP and CSP versions of a chip are different and warrant a different schematic library symbol.  Sometimes there are even different numbers of pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • tarribred61
    tarribred61 over 8 years ago in reply to Sparkylabs

    On the other hand, this is useful if I want to use multiple footprints for the same package.  For example, if I use an EIA0603 resistor and I want to choose from the least, most or nominal solder options then I can just have the various footprints available. Then I can choose the proper footprint depending on whether the board is reflow or wave or hand soldered. I would argue that the SOIC, MSOP, TSSOP and CSP versions of a chip are different and warrant a different schematic library symbol.  Sometimes there are even different numbers of pins.