Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum physical features on mech4
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 1 reply
  • Subscribers 88 subscribers
  • Views 518 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

physical features on mech4

frog
frog over 7 years ago

Hi,

This is probably a question for you Peter, but any other contributions will be welcome.

I know that I can add polygonal board cutouts, but there are a couple of other things I'd like to be able to do:

1. add cutouts with arcs (including but not limited to circular cutouts)

2. For some PCBs I have relatively complex route paths which I typically put on Mechanical Layer 4; is there any way to make these appear in a STEP export?

 

Thanks,

Frog

  • Cancel
Parents
  • e14softwareuk
    e14softwareuk over 7 years ago

    Hi Frog.

     

    When drawing a polygon you can use arcs (just like when tracking) by switching drawing modes using SHIFT+SPACE. If needing a circular cutout then I would suggest simply drawing a circle and converting to a cutout. Draw a shape (using lines, arcs, circles etc) and then in the search box type "conv reg" to activate the command to convert a set of drawing primitives into a region.

    image

    Once a region is created bring up the property dialog (double click or right click > Properties) and change to be a board cutout.

    image

     

    Regarding STEP output, very little is configurable so I don't think there is a way to output random layers and objects.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14softwareuk
    e14softwareuk over 7 years ago

    Hi Frog.

     

    When drawing a polygon you can use arcs (just like when tracking) by switching drawing modes using SHIFT+SPACE. If needing a circular cutout then I would suggest simply drawing a circle and converting to a cutout. Draw a shape (using lines, arcs, circles etc) and then in the search box type "conv reg" to activate the command to convert a set of drawing primitives into a region.

    image

    Once a region is created bring up the property dialog (double click or right click > Properties) and change to be a board cutout.

    image

     

    Regarding STEP output, very little is configurable so I don't think there is a way to output random layers and objects.