Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Altium Circuit Studio Development???
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 118 replies
  • Subscribers 125 subscribers
  • Views 19865 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Altium Circuit Studio Development???

engineereddownunder
engineereddownunder over 7 years ago

My license for Circuit Studio has just come up for renewal, and after just double checking there has been next to no activity in the development world around Circuit Studio - is it worth renewing the license or is this product a dead duck? The last version release was in May last year with apologies for how little it contained and promises of a more major release later in the year - which never came, and which has been followed up by silence (as far as I can tell) from Altium... Thoughts? Anyone seen a recent roadmap for this software? I actually really like the software but don't want to pour money into something that is not being actively developed.

  • Cancel

Top Replies

  • lamabrew
    lamabrew over 7 years ago in reply to e14softwareuk +4
    Only because I just had lunch with a friend today that's looking to move off PADS and thought CS might be a good fit and was asking me questions... IMHO Altium is shooting themselves in the foot (feet…
  • IanJ
    IanJ over 6 years ago in reply to frog +4
    With Autodesk's announcement & video showing Fusion360 & Eagle integration (bloody hell it looks good seeing Eagle with a ribbon)......so surely, but surely Altium will step up the process of developing…
  • engineereddownunder
    engineereddownunder over 7 years ago +3
    So I have been pushing for some more information from element14 and Altium and got a reply which sounds promising (from element14 APAC Technical): There's definitely a major CircuitStudio version coming…
Parents
  • frog
    frog over 7 years ago

    I'm bumping this thread in the hope that there will be some kind of official response...

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • frog
    frog over 7 years ago in reply to frog

    I'm bumping this thread again in the hope that there will be some kind of official response...

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • lamabrew
    lamabrew over 7 years ago in reply to frog

    Seconding that bump...back using CS after doing other things for past 2 months and thought I would poke around here for any news.  I can't figure out what Altium hopes to gain by treating its paying customers like mushrooms...(and again, this is not aimed at Peter who's the closest thing we have here to a spokesperson and is probably the only reason I didn't give up on CS long ago).

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    e14softwareuk over 7 years ago in reply to lamabrew

    Sorry to say that there is still no official roadmap to share.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • mc6800
    mc6800 over 7 years ago in reply to frog

    Agreed, it would be nice to have some news (not a dig at Peter, I'm sure he will post something once there *is* news).

     

    I still suspect that Altium would be better off replacing CS by a pin/layer/size limited version of AD (possibly using the previous year's version for each low-end release to maintain the advantages of the full version). It would almost certainly require much less development time than maintaining the AD and CS codebases separately. They could then simply offer all existing CS licence holders a straight swap to the new software (perhaps subject to having active maintenance) and then end further development of CS.

     

    My suggested limits would be something like:

     

    1) Max 6 Planes, 6 signal layers (so 1-12 layers in total)

    2) Tracks >= 4 mil

    3) Max 10,000 pads/pins/vias (i.e 2x the slowdown limit, but less than the 50,000 upper limit for CS)

    4) No specific upper limit to board size, providing (layers x layer area) <= 6000 cm^2 (so a 4 layer board can be up to 38x38cm, but a 12 layer only 22 x 22 cm). In all cases the calculation would be based on the smallest bounding box that encloses all of the board shape.

     

    In addition a free version could offer 2 layers, 250 pads/pins, tracks >= 6 mil, drill holes >= 0.3mm, boards <= 15cm in any dimension. Upgrading to the low-cost or full version would be just a matter of entering the new licence key (and paying for it, of course!).

     

    Vault access would be an optional paid extra for the free and CS replacement versions

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • tarribred61
    tarribred61 over 7 years ago in reply to mc6800

    OOh, no!  I would prefer not to have simply a limited version of AD (I used Protel99 and AD6 through AD16). CS is pretty good and better than what you suggest.  I think we all agree that some better communications from them and some indication of future release plans would go a long way.

     

    There were some threads a while ago with features we would like to see added.  I'm sure they are aware of what was requested.  For designer who are doing ECAD and especially PCB design all day, everyday then CS likely isn't powerful or productive enough.  If you do occasional design and especially mostly schematic work it is quite good.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • tarribred61
    tarribred61 over 7 years ago in reply to mc6800

    OOh, no!  I would prefer not to have simply a limited version of AD (I used Protel99 and AD6 through AD16). CS is pretty good and better than what you suggest.  I think we all agree that some better communications from them and some indication of future release plans would go a long way.

     

    There were some threads a while ago with features we would like to see added.  I'm sure they are aware of what was requested.  For designer who are doing ECAD and especially PCB design all day, everyday then CS likely isn't powerful or productive enough.  If you do occasional design and especially mostly schematic work it is quite good.