Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Documents Getting Started with CircuitStudio: (#5) Creating the PCB
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14softwareuk
  • Date Created: 6 Jun 2017 12:36 PM Date Created
  • Last Updated Last Updated: 8 Jun 2017 11:34 AM
  • Views 2513 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Getting Started with CircuitStudio: (#5) Creating the PCB

The process of transferring a design from the capture stage to the board layout stage is launched using the Update command Home | Project | Project » Update PCB Document on the Schematic editor Ribbon (or Home | Project | Project » Import Changes from the PCB editor Ribbon).

 

When you run this command the design is compiled and a set of Engineering Change Orders created:

  • List all components used in the design, and the footprint required for each. When the ECOs are executed the software will attempt to locate each footprint in the currently available libraries or available Content Vault, and place each into the PCB workspace. If the footprint is not available, an error will occur.
  • A list of all nets (connected component pins) in the design is created. When the ECOs are executed the software will add each net to the PCB, and then attempt to add the pins that belong to each net. If a pin cannot be added an error will occur - this most often happens when the footprint was not found, or the pads on the footprint do not map to the pins on the symbol.
  • Addition design data is then transferred, such as net and component classes.

 

Although not demonstrated in the video, the ECO process is used when revising a design. For example additional symbols can be added to a schematic, wired up and then all the changes transferred across to the PCB layout.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Next Video • Table of Contents

Attachments:
image5-PreparingthePCBandTransferringtheDesign.pdf