Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Documents Pick and Place Data Format
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14softwareuk
  • Date Created: 10 Jan 2018 10:26 AM Date Created
  • Last Updated Last Updated: 11 Jan 2018 8:25 AM
  • Views 1590 views
  • Likes 2 likes
  • Comments 0 comments
Related
Recommended

Pick and Place Data Format

CircuitStudio includes the ability to generate a pick and place data file for a PCB, typically used by an assembly house to help automate the population of a board. You can configure the units (metric or imperial) and the file format (text or CSV) from the Outputs | Pick and Place menu option. The data columns in the output file are documented below, the files are plain text and so can be viewed with a simple text editor like Notepad or loaded into Excel or other spreadsheet.

 

Column Name
ExampleDescription
DesignatorU91Component reference designator.
FootprintDIP14The name of the footprint, as seen when viewing a list of library components or viewing the property dialog of the component (Footprint : Name field)
Mid X1050milCenter point of component, automatically calculated by CircuitStudio.
Mid Y700mil
Ref X900milLocation of reference point set in the library editor for the component (set using Home | References menu). This is also the point that the cursor snaps to when moving a component on the PCB*.
Ref Y900mil
Pad X900milLocation of pin 1 of the component, automatically calculated by CircuitStudio.
Pad Y1000mil
TBTFlag to indicate if component is located on Top or Bottom of the board.
Rotation0.00Rotation angle set for this component. A library component added to a PCB starts at 0.00 (regardless of if the footprint looks to be horizontal, vertical or some other angle).
CommentSN74LS00NSN74LS00NText extracted from the Comment field of the component (Comment : Text field within the component property dialog).

 

*It is a good idea to make sure the reference point is set to coincide with a pin to help keep components on grid when re-positioning them on the PCB.

  • cam
  • circuitstudio