Products
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
AMD
  • Products
  • Manufacturers
  • AMD
  • More
  • Cancel
AMD
Forum Problem with PYNZ-Z2 and HDMI output from camera
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join AMD to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 16 answers
  • Subscribers 53 subscribers
  • Views 10197 views
  • Users 0 members are here
  • pynq z2
  • hdmi
  • pynq
  • pynqstarter
Related

Problem with PYNZ-Z2 and HDMI output from camera

Fred27
Fred27 over 6 years ago

I'm currently making sure I'm in a good position to hit the ground running with the upcoming PYNQ-Z2 workshops. I bought the recommended kit including an Apeman A77 camera and thought I'd just have a quick poke around in advance. I ran through the "getting started" and the Pynq 2.5 image includes some simple HDMI examples. (I hope I'm not jumping too far ahead, but like to be prepared.)

 

Anyway, as I start to run the HDMI example I get a kernel died error (as shown). You can see on screen what's been run. This is just wiring HDMI out to show what's on HDMI in. The error is completely repeatable. Nothing noteworthy in /var/log/jupyter.log to give any clue.

image

 

As quick Google suggested that maybe the image is too high resolution, and when I checked the camera on my TV it outputs 1080p at 60fps regardless of the resolution of video being captured. Could 1080p be too much?  Time to switch to a Raspberry Pi 4 where I can change resolution properly. The above example ran quite happily with the Pi at a lower resolution, but surprised me when it also ran using the Pi at 1920x1080 at 60fps too.

 

Is this camera (Apeman A77) compatible with the HDMI on the PYNQ-Z2? I'd have expected it to be as it was the recommended kit and the Crosstour one listed now is essentially the same model.

 

I'll try to do more digging into any subtle differences between the HDMI output of the Pi and the camera, but all I have is a TV that shows some info on the input. Anyone else have any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 6 years ago +3 suggested
    Are you aware that the HDMI out IP provided in the PYNQ-Z2 the base overlay doesn't fully support 1080p video ? https://pynq.readthedocs.io/en/v2.5.1/pynq_overlays/pynqz2/pynqz2_base_overlay.html#hdmi…
  • Fred27
    Fred27 over 6 years ago +3
    Thanks for all your help beacon_dave My TV reports that the Pi and the camera are outputting the same format - 1080p60, sYCC601 colourspace, 8-bit depth, and YCbCr 4:2:2 pixel format. I tried connecting…
  • Fred27
    Fred27 over 6 years ago in reply to beacon_dave +2 suggested
    I wasn't aware of those details. Maybe that's it - a borderline implementation of 1080p where output from the Pi 4 works and the camera doesn't. If that's the case it's frustrating that a recommended camera…
Parents
  • dimiterk
    0 dimiterk over 6 years ago

    PYNQ Z2 implements the HDMI Codec for transmit and receive sides as IP blocks on the PL side wired via TMDS configured pins to buffers and then to the HDMI connectors.

    This is presumably done to save on cost as official development boards use external chipset codecs from ADI/Silabs which are configured via I2C.

    The downside of this is that it's using a couple of hundred LUT's from FPGA fabric.

     

    The HDMI INPUT on the above example is NOT connected directly to HDMI out port strictly speaking. According to the PYNQ Vivado HW design for this overlay, the HDMI input is piped to the processor DDR memory and via VDMA is then transferred to the HDMI out IP block.  This allows breaking the loop so that one can implement image processing algorithms on the PS side using OpenCV.

     

    I don't have a PYNQ-Z2, but it looks like that notebook has not been updated for PYNQ V2.5.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dimiterk
    0 dimiterk over 6 years ago

    PYNQ Z2 implements the HDMI Codec for transmit and receive sides as IP blocks on the PL side wired via TMDS configured pins to buffers and then to the HDMI connectors.

    This is presumably done to save on cost as official development boards use external chipset codecs from ADI/Silabs which are configured via I2C.

    The downside of this is that it's using a couple of hundred LUT's from FPGA fabric.

     

    The HDMI INPUT on the above example is NOT connected directly to HDMI out port strictly speaking. According to the PYNQ Vivado HW design for this overlay, the HDMI input is piped to the processor DDR memory and via VDMA is then transferred to the HDMI out IP block.  This allows breaking the loop so that one can implement image processing algorithms on the PS side using OpenCV.

     

    I don't have a PYNQ-Z2, but it looks like that notebook has not been updated for PYNQ V2.5.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer