AMD
  • Products & Partners
  • Manufacturers
  • AMD
  • More
  • Cancel
AMD
Forum Problem with PYNZ-Z2 and HDMI output from camera
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join AMD to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 16 answers
  • Subscribers 53 subscribers
  • Views 10264 views
  • Users 0 members are here
  • pynq z2
  • hdmi
  • pynq
  • pynqstarter
Related

Problem with PYNZ-Z2 and HDMI output from camera

Fred27
Fred27 over 6 years ago

I'm currently making sure I'm in a good position to hit the ground running with the upcoming PYNQ-Z2 workshops. I bought the recommended kit including an Apeman A77 camera and thought I'd just have a quick poke around in advance. I ran through the "getting started" and the Pynq 2.5 image includes some simple HDMI examples. (I hope I'm not jumping too far ahead, but like to be prepared.)

 

Anyway, as I start to run the HDMI example I get a kernel died error (as shown). You can see on screen what's been run. This is just wiring HDMI out to show what's on HDMI in. The error is completely repeatable. Nothing noteworthy in /var/log/jupyter.log to give any clue.

image

 

As quick Google suggested that maybe the image is too high resolution, and when I checked the camera on my TV it outputs 1080p at 60fps regardless of the resolution of video being captured. Could 1080p be too much?  Time to switch to a Raspberry Pi 4 where I can change resolution properly. The above example ran quite happily with the Pi at a lower resolution, but surprised me when it also ran using the Pi at 1920x1080 at 60fps too.

 

Is this camera (Apeman A77) compatible with the HDMI on the PYNQ-Z2? I'd have expected it to be as it was the recommended kit and the Crosstour one listed now is essentially the same model.

 

I'll try to do more digging into any subtle differences between the HDMI output of the Pi and the camera, but all I have is a TV that shows some info on the input. Anyone else have any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 6 years ago +3 suggested
    Are you aware that the HDMI out IP provided in the PYNQ-Z2 the base overlay doesn't fully support 1080p video ? https://pynq.readthedocs.io/en/v2.5.1/pynq_overlays/pynqz2/pynqz2_base_overlay.html#hdmi…
  • Fred27
    Fred27 over 6 years ago +3
    Thanks for all your help beacon_dave My TV reports that the Pi and the camera are outputting the same format - 1080p60, sYCC601 colourspace, 8-bit depth, and YCbCr 4:2:2 pixel format. I tried connecting…
  • Fred27
    Fred27 over 6 years ago in reply to beacon_dave +2 suggested
    I wasn't aware of those details. Maybe that's it - a borderline implementation of 1080p where output from the Pi 4 works and the camera doesn't. If that's the case it's frustrating that a recommended camera…
Parents
  • adamtaylorcengfiet
    0 adamtaylorcengfiet over 6 years ago

    In your case with the apeman camera you need to set the resolution to anything below 1080P quite easy to do via the menu, I usually run mine at 720P with no issues

     

    In the lab we have developed for this course we are using the VGA settings which is how the VDMA is configured.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • adamtaylorcengfiet
    0 adamtaylorcengfiet over 6 years ago

    In your case with the apeman camera you need to set the resolution to anything below 1080P quite easy to do via the menu, I usually run mine at 720P with no issues

     

    In the lab we have developed for this course we are using the VGA settings which is how the VDMA is configured.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Fred27
    0 Fred27 over 6 years ago in reply to adamtaylorcengfiet

    Adam, - thanks for your input. Unfortunately changing the resolution that the camera records at does not change the resolution of the HDMI output. This is always fixed at 1080p on my Apeman A77 - whether it's recording in 720p or in 4K.

     

    I think I'll go back my original "Plan A" of using a Raspberry Pi and Pi camera as a HDMI video source. That's working fine.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ralphjy
    0 ralphjy over 6 years ago in reply to adamtaylorcengfiet

    Hi Adam,

     

    We've been discovering that the different Apeman cameras seem to have quite a variation in functionality.  I was just wondering which camera you have.  And how you have it configured.

     

    I have an A80 which appears to work just fine but Fred and Dave have an A77 and an A66 which don't seem to work as a live video source via the HDMI output.

     

    Thanks,

     

    Ralph