AMD
  • Products
  • Manufacturers
  • AMD
  • More
  • Cancel
AMD
Forum Importing Arduino library files into PYNQ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join AMD to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 52 subscribers
  • Views 3253 views
  • Users 0 members are here
  • pynq
Related

Importing Arduino library files into PYNQ?

kevin_v
kevin_v over 6 years ago

Hello,

 

Does anyone here have experience with taking Arduino .h file type and was able to modify it to be used with pynq and juptyer? If so, could you include a modified file and the original file it was based off of, so i can take a look at both to understand what changes are needed to be made.

 

I know there is a document on the pynq website that explains how to make a header files but at least for me its not easy to follow. Here is the link to the document i am referring to:

https://pynq.readthedocs.io/en/latest/overlay_design_methodology/pynq_microblaze_subsystem.html?_ga=2.228378772.86472398…

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 6 years ago +3
    What exactly are you trying to achieve? The primary function of C header files is to describe the signature of functions that are implemented elsewhere - either in a matching C source file or a compiled…
  • beacon_dave
    beacon_dave over 6 years ago +1 suggested
    Not sure if you have seen it or not but there is an example included with the PYNQ-Z1/Z2 build on using the Adafruit 1.8" LCD (Arduino) Shield on the PYNQ-Z1/Z2 and accessing it with Jupyter Notebooks…
  • phoenixcomm
    phoenixcomm over 6 years ago +1
    kevin_v Ok, let me show you the relationship between .h and .cpp or .c. First a file.h is a header file that only allows access to some (public) functions in file.cpp. Second, both of the processors in…
Parents
  • Fred27
    0 Fred27 over 6 years ago

    What exactly are you trying to achieve? The primary function of C header files is to describe the signature of functions that are implemented elsewhere - either in a matching C source file or a compiled library. There would be no point including the header file unless you had also ported over the code that goes with it.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kevin_v
    0 kevin_v over 6 years ago in reply to Fred27

    Yes, it would be best for me to explain what i am doing. I am trying to get my RA8875 display to work with my pynq board.

    Below is the link to the display i am using:

    https://learn.adafruit.com/ra8875-touch-display-driver-board/arduino

     

    For any .c files i make to work with the screen i need to include both Adafruit_RA8875 library and Adafruit-GFX-Library.

    Here are links to both bellow:

    https://github.com/adafruit/Adafruit_RA8875

    https://github.com/adafruit/Adafruit-GFX-Library

     

    When i look through both libraries i noticed so many .h and .cpp were being used that it didn't make sense to use  %%microblaze base_overlay.arduino.

     

    Right now i am trying to decide if it worth taking the time to go through every file (probably 10 or less files) and modify them to work with pynq to get this screen to work.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kevin_v
    0 kevin_v over 6 years ago in reply to Fred27

    Yes, it would be best for me to explain what i am doing. I am trying to get my RA8875 display to work with my pynq board.

    Below is the link to the display i am using:

    https://learn.adafruit.com/ra8875-touch-display-driver-board/arduino

     

    For any .c files i make to work with the screen i need to include both Adafruit_RA8875 library and Adafruit-GFX-Library.

    Here are links to both bellow:

    https://github.com/adafruit/Adafruit_RA8875

    https://github.com/adafruit/Adafruit-GFX-Library

     

    When i look through both libraries i noticed so many .h and .cpp were being used that it didn't make sense to use  %%microblaze base_overlay.arduino.

     

    Right now i am trying to decide if it worth taking the time to go through every file (probably 10 or less files) and modify them to work with pynq to get this screen to work.