AMD
  • Products
  • Manufacturers
  • AMD
  • More
  • Cancel
AMD
Forum Importing Arduino library files into PYNQ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join AMD to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 52 subscribers
  • Views 3253 views
  • Users 0 members are here
  • pynq
Related

Importing Arduino library files into PYNQ?

kevin_v
kevin_v over 6 years ago

Hello,

 

Does anyone here have experience with taking Arduino .h file type and was able to modify it to be used with pynq and juptyer? If so, could you include a modified file and the original file it was based off of, so i can take a look at both to understand what changes are needed to be made.

 

I know there is a document on the pynq website that explains how to make a header files but at least for me its not easy to follow. Here is the link to the document i am referring to:

https://pynq.readthedocs.io/en/latest/overlay_design_methodology/pynq_microblaze_subsystem.html?_ga=2.228378772.86472398…

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 6 years ago +3
    What exactly are you trying to achieve? The primary function of C header files is to describe the signature of functions that are implemented elsewhere - either in a matching C source file or a compiled…
  • beacon_dave
    beacon_dave over 6 years ago +1 suggested
    Not sure if you have seen it or not but there is an example included with the PYNQ-Z1/Z2 build on using the Adafruit 1.8" LCD (Arduino) Shield on the PYNQ-Z1/Z2 and accessing it with Jupyter Notebooks…
  • phoenixcomm
    phoenixcomm over 6 years ago +1
    kevin_v Ok, let me show you the relationship between .h and .cpp or .c. First a file.h is a header file that only allows access to some (public) functions in file.cpp. Second, both of the processors in…
Parents
  • phoenixcomm
    0 phoenixcomm over 6 years ago

    kevin_v Ok, let me show you the relationship between .h  and .cpp or .c. First a file.h is a header file that only allows access to some (public) functions in file.cpp.

    Second, both of the processors in question PYNQ and Arduino are two different hardware platforms. Third not only would you have to change all of the addressing but look at

    pinmode(n, INPUT): what are you going to do now? Yes this will have to change to the PYNQ code.  along with any ping definitions. again what abut digital.Write() same o' same o', etc.

    So in closing  "Never Give Up, Never Surrender!" .. Capt. Jason Nesmith, NSEA Protector

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kevin_v
    0 kevin_v over 6 years ago in reply to phoenixcomm

    Thanks for pointing out some of the areas i should look into to when modifying the .h and .cpp files. Sure seems like a lot of stuff to go through though. If you look at my response to Fred's comment you will see a description of what i am trying to achieve. I probably have to import 10 or less files. Do you think it worth me taking the time to modify each files or just make my own header files of what i need to make the screen to work?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kevin_v
    0 kevin_v over 6 years ago in reply to phoenixcomm

    Thanks for pointing out some of the areas i should look into to when modifying the .h and .cpp files. Sure seems like a lot of stuff to go through though. If you look at my response to Fred's comment you will see a description of what i am trying to achieve. I probably have to import 10 or less files. Do you think it worth me taking the time to modify each files or just make my own header files of what i need to make the screen to work?