Amphenol
  • Products & Partners
  • Manufacturers
  • Amphenol
  • More
  • Cancel
Amphenol
Amphenol Sensors Blog How to Boost Data Center Sustainability With Sensors
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Amphenol to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Julianne
  • Date Created: 11 Jun 2026 12:46 PM Date Created
  • Views 258 views
  • Likes 5 likes
  • Comments 2 comments
  • sensors
  • custom sensors
  • data centers
  • Sensor Technology
  • sensor manufacturer
Related
Recommended

How to Boost Data Center Sustainability With Sensors

Julianne
Julianne
11 Jun 2026
How to Boost Data Center Sustainability With Sensors

Cloud computing keeps expanding at lightning speed, but the growth isn’t free. 

Data centers power everything from online shopping and streaming to AI tools, and in the process, they consume huge amounts of electricity (up to 6.7% – 12% of U.S. by 2028) and water (up to 5 million gallons per day). With sustainability key performance indicators (KPIs) now part of most corporate strategies, operators are under pressure to shrink their carbon footprint without compromising uptime or performance.

Advanced sensing technologies offer a practical path forward. Sensors give operators a real-time look at the conditions that matter most, helping them cut energy use, run cooling systems more efficiently, and stay on top of carbon reduction goals.

 

Why Data Center Sustainability Matters

The conversation around sustainability isn’t just a buzzword; it’s a growing expectation from regulators, customers, and communities. Before diving into how sensors help, it’s important to understand why reducing energy, water, and carbon use is such a pressing issue for data center operators.

Data centers account for a growing share of global energy demand. According to the International Energy Agency, their electricity use could double by 2026 if left unchecked. All that demand means more carbon in the air and extra pressure on local power. 

Water is another piece of the puzzle, since cooling systems can use more than communities can spare, especially in places prone to droughts. At the end of the day, efficiency isn’t just about saving money; it’s also about proving you take sustainability seriously.

Sensors play a critical role in bridging that gap. They provide the granular insights operators need to understand how much energy and water their systems consume, where waste occurs, and how to correct it in real time.

 

Key Areas Where Sensors Reduce Environmental Impact

While sustainability is a broad challenge, it often comes down to a handful of operational factors inside the data center. Sensors give operators the visibility they need to measure, manage, and reduce resource use across power, cooling, water, and emissions. 

Here are some of the most impactful areas where sensing technology makes a measurable difference.

PUE Monitoring

Power usage effectiveness (PUE) is one of the most common metrics for tracking data center efficiency. Sensors placed throughout the facility monitor electrical loads across IT equipment, cooling systems, and auxiliary infrastructure.

By watching PUE in real-time, operators can quickly spot when something’s off, such as cooling systems pulling more power than the servers they’re meant to support. With that kind of visibility, it’s easier to make targeted changes and put money into upgrades that actually cut energy use.

Cooling Optimization & HVAC Control

Cooling accounts for nearly 40% of a data center’s total energy use. Temperature and humidity sensors give operators precise visibility into airflow, hot spots, and environmental fluctuations.

Here are a few ways facilities apply those insights:

  • Adjust setpoints to reduce unnecessary overcooling.

  • Optimize airflow with hot aisle/cold aisle containment.

  • Balance humidity to reduce static risk and equipment stress.

  • Extend equipment lifespan by avoiding thermal strain.

Rather than blasting cool air through the whole facility, operators can use localized data to fine-tune HVAC performance. In practice, that might mean running the room a little warmer, fine-tuning airflow to trouble spots, or arranging systems in a smarter way. Done right, it cuts back on energy use and helps the equipment last.

Water Conservation

Water scarcity is becoming a global issue, and data centers with H2O-intensive cooling methods face increasing scrutiny. Flow and pressure sensors provide insight into the amount of water that cooling towers and chiller systems consume.

Armed with accurate data, operators can transition to hybrid or air-based cooling solutions, adjust water cycles for efficiency, or even reclaim water for reuse. These steps directly reduce a facility’s environmental footprint while supporting sustainability KPIs.

Air Quality & Carbon Emissions Tracking

As sustainability rules get tougher, operators need to track more than just energy and water use – they also have to keep an eye on greenhouse gas emissions. Gas sensors can measure CO₂ and other pollutants in and around the facility, giving teams a clearer picture of their impact.

Indoor air quality sensors add another layer of protection, making sure conditions stay safe for both equipment and the people who work there. Together, this data feeds into ESG reports and shows investors and regulators that the facility is committed to being transparent and accountable.

 

From Reactive to Predictive Sustainability

Once the fundamentals of efficiency are in place, the next step is moving beyond short-term fixes. Sensors enable operators to anticipate issues before they escalate, shifting the strategy from damage control to long-term sustainability planning.

One of the most powerful aspects of advanced sensing is the shift it enables from reactive maintenance to predictive sustainability. Instead of waiting for inefficiencies to balloon into larger problems, operators can act proactively.

For example, vibration and thermal sensors detect early signs of equipment strain. Addressing these issues before failure prevents both downtime and the excessive energy draw caused by inefficient machines.

Over time, predictive insights powered by sensors help create a truly energy-efficient data center – one that aligns with global sustainability goals and corporate commitments.

 

Meeting Today’s Sustainability KPIs With Sensors

Sustainability goals are no longer optional checkboxes; they’re tied directly to business reputation and compliance. Here’s how advanced sensing helps operators demonstrate measurable progress toward carbon, water, and energy reduction targets.

Sustainability KPI Relevant Sensors Example Benefit
Energy Efficiency Power, thermal, vibration Reduce PUE, catch inefficient equipment early
Water Conservation Flow, pressure Track usage, optimize cooling tower cycles
Carbon Emissions Gas, air quality Monitor CO₂ output and improve ESG reporting
Equipment Reliability Vibration, temperature Prevent downtime and cut excess energy draw


Data centers are under growing pressure to shrink their environmental footprint, but tackling the problem doesn’t have to feel overwhelming. Sensors give operators a practical way to track carbon emissions, water use, and energy consumption, and then make changes based on real data.

When facilities invest in smarter monitoring, they’re not just checking boxes for today’s sustainability goals. They’re also showing customers, investors, and regulators that they take environmental responsibility seriously – which builds trust in an industry that’s always in the spotlight.

 

Moving Forward With Sensors

The push for greener data centers is ongoing, and there’s no single solution. But by embedding sensors throughout their infrastructure, operators gain the insights and control needed to make meaningful changes today, and prepare for stricter requirements tomorrow.

Data centers may never be completely “green,” but sensors bring them much closer to the goal of responsible, sustainable operations. Through PUE tracking, smarter cooling, maintaining optimal environmental conditions, emissions monitoring, and predictive maintenance, sensors equip operators with the insights to lower their footprint and still meet the world’s rising demand for digital services.

  • Sign in to reply
  • SensoredHacker0
    SensoredHacker0 3 months ago

    At work we make heatpumps, in a datacenter campus complex the excess heat is routed from the holding tanks to building heating in the floor, and all the sidewalks, and parking lots so that they dont have to pay for plowing. 
    Im all for sensor deployment, but i think if these AI data-centers popping up every where were held to the same standards as every other building complex most of the woes regarding their deployments could be avoided. Stop giving these companies exemptions to install AI data-centers doesn't require any intelligence at all. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB 3 months ago

    Since excess heat is a big problem, I would move all of the data centers to cold areas so that I could use the local environment temperatures to cool the centers.

    Same Idea works for areas with local water bodies where you could do heat exchanges with the planet.