Amphenol
  • Products & Partners
  • Manufacturers
  • Amphenol
  • More
  • Cancel
Amphenol
Amphenol Communication Solutions Blog Designs Choices that Quietly Reduce System Lifetime
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Amphenol to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: CalvinTerence
  • Date Created: 20 Jan 2026 8:13 AM Date Created
  • Views 219 views
  • Likes 2 likes
  • Comments 1 comment
  • designs
  • Amphenol Communications Solutions
  • board-to-board
  • System Lifetime
  • Ampehnol
  • industrial ethernet
Related
Recommended

Designs Choices that Quietly Reduce System Lifetime

CalvinTerence
CalvinTerence
20 Jan 2026

Most systems don't fail suddenly. They wear out quietly - often long before anyone expects - because of design decisions that seemed reasonable at the time. 

In many cases, reduced system lifetime isn't caused by a single flaw, but by small tradeoffs made under pressure from cost, space or timelines. Over time, these decisions compound and begins to show their impact. 

Treating Interconnects as Secondary Components

Connectors are often selected late in the design process, sometimes with minimal consideration beyond basic electrical requirements. Over time, inadequate retention, limited mating cycles, or insufficient environmental protection can lead to intermittent failures that are difficult to diagnose.

Ignoring Thermal Stress in Dense Designs

As systems become faster and more compact, heat becomes a silent reliability killer. Even when components operate within specified limits, sustained thermal stress can accelerate material aging, loosen contacts, and reduce long-term stability.

Overlooking Mechanical and Environmental Factors

Vibration, shock, dust, and moisture are common in industrial environments. Designs that don’t account for these factors often experience premature degradation at connection points, especially in automation and robotics systems.

Designing for Initial Performance Instead of Lifetime

Many designs perform flawlessly during validation and early deployment. However, systems exposed to continuous operation, temperature cycling, and repeated mating over time require components selected with long-term durability in mind.

Prioritizing Short-Term Cost Over Long-Term Reliability

Cost-driven decisions can appear justified early on, but the real expense often surfaces later through downtime, maintenance, and reduced equipment life.

Where Interconnect Strategy Makes the Difference

This is where thoughtful interconnect selection becomes critical. Amphenol's broad portfolio of connectors and cable solutions - spanning Industrial Ethernet, Board-to-Board, High Speed I/O, memory, and Power - are engineered to address the real-world challenges of thermal stress, mechanical reliability, and harsh environments. By designing interconnects with longevity in mind, engineers can significantly extend system lifetime and improve overall reliability across Industrial Automation, Robotics, and embedded computing platforms.

Which design choice has surprised you most when you saw its long-term impact in real-world operation?

  • Sign in to reply
  • colporteur
    colporteur 9 months ago

    Button pushes that triggered an animation, comes to mind when I think, interconnects meets the real world. I purchased some real cheap push buttons for a project where the public pushes a button to trigger an animation. The buttons didn't survive the first day of the show before they became intermittent. I learned ten push button for under $2 is not such a good deal after all.

    The additional lesson learned is building into a design troubleshooting tools (i.e. LEDs) to reduce the need to get out the multi meter to uncover faults is not such a bad idea.