Amphenol
  • Products & Partners
  • Manufacturers
  • Amphenol
  • More
  • Cancel
Amphenol
Forum Raspberry pi 2 is it worth it?
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Amphenol to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 28 subscribers
  • Views 2261 views
  • Users 0 members are here
  • raspberry
  • pi
Related

Raspberry pi 2 is it worth it?

e14 Contributor
e14 Contributor over 11 years ago

I Am in high school and I have a iPad and I am in need of some kind of computer I can type on a keyboard but I don't want to be out $500 at the same time so I was wondering if it would be worth my while to just buy a raspberry pi 2 and use it for typing essays andresearching along with some editing that I would do with my go pro. Is it worth it to me to get this raspberry pi 2?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Yes, you should buy a Pi. Not only can you attach a (USB, or wireless through BT) keyboard to it, you can use the HDMI port to connect to a monitor, either to the monitor's HDMI port or with an adapter…
Parents
  • amgalbu
    0 amgalbu over 11 years ago

    According to the specs. Raspberry Pi2 is absolutely capable of handling the kind of tasks you are talking about... but I don't have any direct experience with that. Anyway, I used the Raspberry B platfrom (which is mush less performant than Raspberry Pi 2) and I was able to perform simple tasks without any issue...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • amgalbu
    0 amgalbu over 11 years ago

    According to the specs. Raspberry Pi2 is absolutely capable of handling the kind of tasks you are talking about... but I don't have any direct experience with that. Anyway, I used the Raspberry B platfrom (which is mush less performant than Raspberry Pi 2) and I was able to perform simple tasks without any issue...