Analog Devices
  • Products & Partners
  • Manufacturers
  • Analog Devices
  • More
  • Cancel
Analog Devices
Blog Powering Your Drive – Final Thoughts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Analog Devices to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: brianc
  • Date Created: 3 Mar 2025 12:07 PM Date Created
  • Views 2447 views
  • Likes 8 likes
  • Comments 4 comments
  • overvoltage
  • Power Monitor Control and Protection
  • control
  • Surge Stopper
  • ADIMotorDrives
  • Interface and Isolation
  • power management
  • protection
  • power monitor
  • Precision Technology
  • cybersecurity
  • Powering Your Drive
Related
Recommended

Powering Your Drive – Final Thoughts

brianc
brianc
3 Mar 2025
Powering Your Drive – Final Thoughts

We addressed the requirements and circuits needed within a variable speed drive (VSD) to provide the main control power supply and the power supplies for the inverter electronics – namely gate drivers and current sense circuits in the previous blog in the series.
These are highlighted once again in graphical form in Figure 1, which shows a generalized view of a typical VSD architecture.

image

Figure 1: Detailed Variable Speed Drive Architecture

This blog addresses two more important power supply topics within the highlighted block of the VSD in Figure 1:

  • protecting the main control power supply
  • deriving the downstream low-voltage point-of-load (POL) power rails (these were referenced in the last blog, but not specifically addressed).

Control Power Protection

Protection of the main control power supply (usually 24V) from transients and anomaly conditions is extremely important within a VSD. The reason for this is that there are generally two paths for this supply rail. The first path is that described in the last blog in which the 24V control power supply is derived from the AC mains, or high voltage DC bus via an isolated power conversion stage. However, this 24V rail can also usually be supplied directly from an auxiliary power input connected to the VSD. Most automation environments distribute 24V supplies around the control cabinets for a range of control equipment, and the VSD usually taps into this supply. This auxiliary 24V input is usually diode OR’ed with the converter-derived 24V supply, to ensure that only one supply source is active at a time. The advantage of having this available is that even if the AC mains drops out or trips, usually the auxiliary 24V supply will keep running, meaning the VSD’s control electronics can stay energized, resulting in the capability to quickly restart the VSD and not lose any context information. The disadvantage is that the VSD power supplies are now exposed to all of the voltage transients existing on the factory-wide 24V supply system – these can occur through switching loads that excite voltage ringing on distribution cables, lightning events that propagate through the system, electrostatic discharge from nearby electric fields or human contact, as well as electromagnetic interference picked up on cables. Hence the a need for solid protection on this auxiliary supply input. 

The VSD functional safety standard IEC 61800-5-2 Annex A (Section B.3.2) shows a recommended Power Supply (PS) and Voltage Monitor (VM) subsystem for such a 24VDC rail. It consists of protection against a variety of common faults such as reverse polarity, overcurrent, and voltage transients.

image

Figure 2: Recommended auxiliary supply protection per IEC 61800-5-2

As the transients involved can vary in energy level and duration, designing a discrete circuit can be time-consuming and prone to error, and may have poor long-term reliability. Integrated solutions such as Analog Devices Surge Stopper family integrate all of the IEC 61800 requirements, including input reverse polarity detection and protection, overcurrent, short circuit and inrush current detection and protection, and high voltage transient disconnect.

image

Figure 3: Analog Devices’ Surge Stopper implementation of IEC 61800-5-2

Figure 3 depicts the use of surge stopper solutions from Analog Devices as a potential implementation of IEC61800-5-2 protection recommendations.  Components such as the LT4363 or the integrated MOSFET variant LTC4381 can provide robust and reliable protection solutions for the main control power supply.

Low Voltage Point-Of-Load (POL) Power

Downstream of the main control power supply sit the low voltage (<12V) power rails. These are by and large the point-of-load (POL) supplies that directly power the main controller devices (CPU, FPGA), other digital components (memory, transceivers, interfaces) analog circuitry (ADC, DAC, op-amps, etc), and I/O devices and terminals. The specific design of these power architectures is unique to each VSD, and it is difficult to speak in generalizations, but the typical approaches to these power supplies are illustrated in Figure 4 and Figure 5. In Figure 4, single-stage switching regulators are utilized for some key low voltage rails, with downstream low-dropout (LDO) regulator being added for noise-sensitive analog rails or very low current rails at lower voltage levels.

image

Figure 4: Single-stage switcher approach

In Figure 5, a single intermediate rail is generated (in this case 5V) and this is further stepped down to individual rails as needed by the POL devices. Also shown here, is the potential need for startup sequencing or tracking of supply rails, which can be important in the complex multi-controller systems used in many VSDs.

image

Figure 5: Multi-stage switcher approach

POL power supply architecture design is complex and involves many tradeoffs related to overall efficiency, cost, space, and noise. Tools such as LTpowerCAD, LTpowerPlanner, and LTSPICE, from Analog Devices can significantly ease the design challenge.

Summary

This blog has completed the topic of power supplies within the VSD, underlining the importance of protection circuits for the main control power supply, and touching on the challenges related to POL low voltage supply design.  In the next blog post, we will start looking at the main DC/AC inverter stage that implements the power conversion to control the motor itself. 

  • Sign in to reply
  • robogary
    robogary over 1 year ago in reply to brianc

    agree, some folks will do $1000 damage to try and save a nickel. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • brianc
    brianc over 1 year ago in reply to robogary

    While this can certainly be the case, unfortunately it is something that is not always guaranteed in a system, and in such cases protection is still important.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 1 year ago

    "The disadvantage is that the VSD power supplies are now exposed to all of the voltage transients existing on the factory-wide 24V supply system" ....I've usually seen 24Vdc ( other other control power volts) for the VFDs are fed from a dedicated bulk 24V supply in the DCS system that excludes discrete IO. Discrete IO is fed from local panels, distributed, 24V power supplies. Suppressed 24V small relays coils are OK , once solenoids and big contactor coils get involved, those are fed by another bulk supply that can be tolerant of "dirty" transients.    

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • svanderwolf
    svanderwolf over 1 year ago
    1. #PoweringYourDrive
    2. #VariableSpeedDrive
    3. #ControlPowerSupply
    4. #AnalogDevices
    5. #SurgeProtection