Analog Devices
  • Products & Partners
  • Manufacturers
  • Analog Devices
  • More
  • Cancel
Analog Devices
Forum how to compute heart rate and SPO2 from MAX30100
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Analog Devices to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 10 answers
  • Subscribers 56 subscribers
  • Views 19754 views
  • Users 0 members are here
Related

how to compute heart rate and SPO2 from MAX30100

lavr2016
lavr2016 over 10 years ago

Hello, everybody. I work with Pulse Oximeter and Heart-Rate Sensor MAX30100 from Maxim Intergarted. I get raw data from sensor, but don't find an algorithm, how to compute heart rate and SPO2 level. Can anybody help me? I will be grateful for C code.

  • Sign in to reply
  • Cancel

Top Replies

  • koudelad
    koudelad over 9 years ago +3 suggested
    Hello, I know this is a year old discussion, but I got to this topic even after searching for MAX30100 example on Google I also own a Heart Rate clickboard and I found this article about a setup of MAX30100…
  • aswinvenu
    aswinvenu over 6 years ago in reply to eswar123 +3 suggested
    Hi Eswar, There are couple of libraries available online for MAX30102. Most of them are for arduino or mbed platforms. But with some effort you can re-write it for Atmega16A. Please take a look. https…
  • aswinvenu
    aswinvenu over 6 years ago +2 suggested
    Hi, Please check this TI app note for calculating SpO2. The same approach is applicable to maxim chip. http://www.ti.com/lit/an/slaa655/slaa655.pdf in brief SpO2 can be calculated R = (AC RMS of Red /…
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    How did u get the I2C to work on max30100? i can make it in arduino but i'm having a lot of trouble doing the same for xmega128a3u

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lavr2016
    0 lavr2016 over 10 years ago in reply to e14 Contributor

    Hello!

    You can use library from github: https://github.com/kontakt/MAX30100

    I work with Arduino pro mini(atmega328), communication is ok. (are you know, the I2C voltage for MAX30100 <=3.6 Volt and need a pull-up resistors?).

    Also i try to connect MAX30100 and 30102 to FRDM-K64f(Freescale).

    I get a ADC data from MAX but can't calculate it into normal heartrate or SPO2 - heart rate change from 60-80 BPM(i think, it normal) to 180-250. May be I use an incorrect algorithm?

    MAXIM don't provide a sample code or appnote for this sensor (it's official response from Maxim support centre!!!) , I think it very BAD!

    too many sensors from another company have a lot of documentation for calculation sensor's data!

    good luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to lavr2016

    I used that library in arduino also and it also worke. I was talking about xmega 128 a3u comunnication since i want to use the max 30100 with that microprocessor.

    You are probably detecting false positive peaks due to noise or motion artefacts, try to use a moving average filter and a low passa filter to smooth the signal. In your algorithm try to use an adaptative treshold and guaranty that you can't detect 2 peaks too close to each other. give them a minimum distance of samples between them.

    And yes MAXIM should provide sample code or appnotes.

     

    Good luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • lavr2016
    0 lavr2016 over 10 years ago in reply to e14 Contributor

    can You share Your code for calculate heart-rate?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • koudelad
    0 koudelad over 9 years ago

    Hello,

    I know this is a year old discussion, but I got to this topic even after searching for MAX30100 example on Google image

    I also own a Heart Rate clickboard and I found this article about a setup of MAX30100 with a lot of useful information. It even links to a great general article about pulse oximetry.

    Looks like quite a challenge. Unfortunately, Maxim provides only a datasheet and no application note etc.

     

    BTW MAX30100 is not recommended for new designs and superseded by MAX30101 and MAX30102.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • aswinvenu
    0 aswinvenu over 6 years ago

    Hi,

    Please check this TI app note for calculating SpO2. The same approach is applicable to maxim chip.

    http://www.ti.com/lit/an/slaa655/slaa655.pdf

     

    in brief SpO2 can be calculated

     

    R = (AC RMS of Red / DC of Red)/ (AC RMS of IR / DC of IR)

     

    SpO2 is a percentage value. Using the R value you can calculate the %SpO2

     

    % SpO2= 110 – 25 × R

     

    AC RMS is the RMS value of voltage difference between peak and trough of the RED/IR waveform.

    DC is the voltage difference between ground and the trough waveform.

     

    image

    Please ping me in case if you want any more help.

     

    Regards,

    Aswin

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • eswar123
    0 eswar123 over 6 years ago in reply to aswinvenu

    hi friends
    im new to iot and im doing a project which includes MAX 30102
    can someone provide me the libraries for atmega 16a and some sample codes so it could help me alot
    thank you


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • aswinvenu
    0 aswinvenu over 6 years ago in reply to eswar123

    Hi Eswar,

     

      There are couple of libraries available online for MAX30102. Most of them are for arduino or mbed platforms. But with some effort you can re-write it for Atmega16A. Please take a look.

     

    https://os.mbed.com/users/Filea/code/MAX30102/file/02f411fefe6f/max30102.cpp/

    https://platformio.org/lib/show/4010/MAX30102

    https://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&cad=rja&uact=8&ved=2ahUKEwiyr4nWuYLoAhX5wzgGHd9JCtoQFjAA…

     

    Here is my suggestion. MAX30102 is drivers are not very complicated. You can write one if you read the Datasheet very carefully. Since you are a beginner I would suggest you to do it by your self. Please follow the steps.

     

    1) Download the data sheets for both target Microcontroller and Sensor.

    https://datasheets.maximintegrated.com/en/ds/MAX30102.pdf

    http://ww1.microchip.com/downloads/en/devicedoc/atmel-8154-8-bit-avr-atmega16a_datasheet.pdf

     

    2) Read and understand how I2C functions. Understand the registers used in the Microcontrollers for handling I2C

    3) Write a function to configure I2C in the Microcontroller

    4) Write two sets of functions to read and write a byte through I2C. (twi_read(), twi_write())

    5) Now understand the state diagram of MAX30102 operation.

    6) Use read and write function to configure the registers in the MAX30102

     

    Rest of the things are very well explained in the MAX30102 datasheet.

     

    Happy Coding.

     

    Regards,

    Aswin

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • eswar123
    0 eswar123 over 6 years ago in reply to aswinvenu

    hi aswin sir
    can u please sugest me some tutorial which teaches me the step by step coz im new here and im unable start
    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • aswinvenu
    0 aswinvenu over 6 years ago in reply to eswar123

    Please go through these tutorials. They are really good and easy to follow.

    https://www.newbiehack.com/MicrocontrollerIntroductionABeginnersGuidetotheAtmelAVRAtmega32.aspx

     

    I2C tutorials can be found here.

    https://www.newbiehack.com/I2C-TWI-FirstExample.aspx

     

    Take your time and understand it thoroughly. This will help later.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>