Analog Devices
  • Products & Partners
  • Manufacturers
  • Analog Devices
  • More
  • Cancel
Analog Devices
Forum Why Is Analog Design Harder Than Digital Design?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Analog Devices to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 53 subscribers
  • Views 13709 views
  • Users 0 members are here
  • why is analog design harder than digital design?
  • precision measurement
  • digital design
  • analog design
  • reliable circuit protection
  • rugged connectivity
  • efficient power
Related

Why Is Analog Design Harder Than Digital Design?

rscasny
rscasny over 6 years ago

Are you an analog design engineer or digital? By most standards, the marketplace is producing more digital design engineers than analog. Ask most engineers and they would tell you why: analog design is harder than digital, and requires more knowledge and more factors to consider such as a deep understanding of efficient power, precision measurement, wireless connectivity, and reliable circuit protection. What  do you think?

 

Let's talk about that a bit more. Is analog design just a matter of knowledge, or is there something more involved? It likely boils down to that fact that analog design involves more than just analog. It's influenced by circuit theory, signal processing, control systems, and device physics, and more. When you consider that circuits and components are more integrated and operated at ultra low power, one needs to consider both pow power, low noise, and stability over the required temperature range.

 

What's analog design require? Efficient power ICs to extend the lifetime and reduce heat dissipation for your design. Precision measurement ICs to feature high accuracy and high performance for across-the-board precision analog applications. Rugged connectivity to offer the industry’s highest level of protection for connectivity in hazardous environments. Reliable protection ICs to protect systems from faults by maintaining and monitoring proper voltage, current, and temperature levels.

 

For sure, analog design has always been more complicated than digital design. While both require the engineer to make design compromises, analog beats digital design in the arena of complexity. All the variables involved just make it nothing but hard.

 

I've told you what I think. How about you?

 

Why do you think analog design is more difficult than digital design? If you have an example, share it with the element14 community?

 

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 6 years ago +6
    Digital is On or Off, where Analog is continuous. Because of this difference, designing Analog circuits becomes much more difficult, as there are so many considerations that need to taken into account…
  • neuromodulator
    neuromodulator over 6 years ago +6
    I think digital is more of an illusion as signals are analog, and that fact will at some point have practical implications even if one tries to ignore that. I also think not that many are into analog because…
  • dougw
    dougw over 6 years ago +6
    Until digital becomes analog (high frequency) it is a bit like a cookbook - just follow the datasheet. With analog, the datasheet is just the start of an adventure.
Parents
  • colporteur
    colporteur over 6 years ago

    I would challenge the statement "Analog Design Harder Than Digital Design". Define harder for me?

     

    Either discipline taken into the real word (i.e practical application) is hard. What cushions the application of the discipline is experience. You could argue knowledge is also a cushion but I have found it only works well after the fact

     

    I tell the story of an RF engineer designing a radio transmission/receiver system. The individual was an iron ring engineer and I was a technologist. The site we were working on, had reception issues. The replacement design was suppose to resolve the issue. The engineer design used the latest technology. He used the engineer specifications of the replacement equipment to maximize the RF energy available.

     

    After reviewing his design I asked him some questions regarding theory applied. I agreed the specification indicates the RF connections has .5dB  loss. If that connection was made by an installer in -35 Celsius temperature and the cable was rolled out in a snow storm would he still feel confident in his design. My comments were to help him understand what happens in the real world.

     

    I continue to discover, even after retirements, what works in the my lab doesn't work the way I think it should when it meets the real world. I thought this pic was a great visual of applied theory.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 6 years ago

    I would challenge the statement "Analog Design Harder Than Digital Design". Define harder for me?

     

    Either discipline taken into the real word (i.e practical application) is hard. What cushions the application of the discipline is experience. You could argue knowledge is also a cushion but I have found it only works well after the fact

     

    I tell the story of an RF engineer designing a radio transmission/receiver system. The individual was an iron ring engineer and I was a technologist. The site we were working on, had reception issues. The replacement design was suppose to resolve the issue. The engineer design used the latest technology. He used the engineer specifications of the replacement equipment to maximize the RF energy available.

     

    After reviewing his design I asked him some questions regarding theory applied. I agreed the specification indicates the RF connections has .5dB  loss. If that connection was made by an installer in -35 Celsius temperature and the cable was rolled out in a snow storm would he still feel confident in his design. My comments were to help him understand what happens in the real world.

     

    I continue to discover, even after retirements, what works in the my lab doesn't work the way I think it should when it meets the real world. I thought this pic was a great visual of applied theory.