Analog Devices
  • Products & Partners
  • Manufacturers
  • Analog Devices
  • More
  • Cancel
Analog Devices
Forum Why Is Analog Design Harder Than Digital Design?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Analog Devices to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 53 subscribers
  • Views 13698 views
  • Users 0 members are here
  • why is analog design harder than digital design?
  • precision measurement
  • digital design
  • analog design
  • reliable circuit protection
  • rugged connectivity
  • efficient power
Related

Why Is Analog Design Harder Than Digital Design?

rscasny
rscasny over 6 years ago

Are you an analog design engineer or digital? By most standards, the marketplace is producing more digital design engineers than analog. Ask most engineers and they would tell you why: analog design is harder than digital, and requires more knowledge and more factors to consider such as a deep understanding of efficient power, precision measurement, wireless connectivity, and reliable circuit protection. What  do you think?

 

Let's talk about that a bit more. Is analog design just a matter of knowledge, or is there something more involved? It likely boils down to that fact that analog design involves more than just analog. It's influenced by circuit theory, signal processing, control systems, and device physics, and more. When you consider that circuits and components are more integrated and operated at ultra low power, one needs to consider both pow power, low noise, and stability over the required temperature range.

 

What's analog design require? Efficient power ICs to extend the lifetime and reduce heat dissipation for your design. Precision measurement ICs to feature high accuracy and high performance for across-the-board precision analog applications. Rugged connectivity to offer the industry’s highest level of protection for connectivity in hazardous environments. Reliable protection ICs to protect systems from faults by maintaining and monitoring proper voltage, current, and temperature levels.

 

For sure, analog design has always been more complicated than digital design. While both require the engineer to make design compromises, analog beats digital design in the arena of complexity. All the variables involved just make it nothing but hard.

 

I've told you what I think. How about you?

 

Why do you think analog design is more difficult than digital design? If you have an example, share it with the element14 community?

 

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 6 years ago +6
    Digital is On or Off, where Analog is continuous. Because of this difference, designing Analog circuits becomes much more difficult, as there are so many considerations that need to taken into account…
  • neuromodulator
    neuromodulator over 6 years ago +6
    I think digital is more of an illusion as signals are analog, and that fact will at some point have practical implications even if one tries to ignore that. I also think not that many are into analog because…
  • dougw
    dougw over 6 years ago +6
    Until digital becomes analog (high frequency) it is a bit like a cookbook - just follow the datasheet. With analog, the datasheet is just the start of an adventure.
Parents
  • dougw
    dougw over 6 years ago

    Until digital becomes analog (high frequency) it is a bit like a cookbook - just follow the datasheet.

    With analog, the datasheet is just the start of an adventure.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to dougw

    Douglas,

     

    I can still remember in one of my microwave lecturers being informed that at higher frequencies that if the copper tracks on a PCB were at too sharp an angle the signal just kept going in the original direction. I was a lad from the countryside, we didn't have weird stuff like that.

     

    Dubbie

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dubbie
    dubbie over 6 years ago in reply to dougw

    Douglas,

     

    I can still remember in one of my microwave lecturers being informed that at higher frequencies that if the copper tracks on a PCB were at too sharp an angle the signal just kept going in the original direction. I was a lad from the countryside, we didn't have weird stuff like that.

     

    Dubbie

    • Cancel
    • Vote Up +4 Vote Down