Analog Devices
  • Products & Partners
  • Manufacturers
  • Analog Devices
  • More
  • Cancel
Analog Devices
Forum MAX32664D doesn't work
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Analog Devices to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 49 subscribers
  • Views 6046 views
  • Users 0 members are here
  • max30102
  • max32664
Related

MAX32664D doesn't work

AliMozaffari
AliMozaffari over 3 years ago

I'm trying to build an spo2 measurement with MAX30102 and MAX32664D. I'm sending my commands from TI CC2640R2F using I2C 400KHz mode. I made a library for MAX32664D and tried to send commands below and I explained the results that I got by running these commands:

1 MAX32664_EnterBootLoaderMode();
2 MAX32664_ReadDeviceMode();
3 MAX32664_ReadMCUType();
4 MAX32664_ReadBootloaderVersion();
5 MAX32664_ReadBootloaderPageSize();
6 MAX32664_EnterAppMode();
7 MAX32664_ReadDeviceMode();
8 MAX32664_BPTalgorithmMode(0x02);
9 MAX32664_SetOutputMode(0x01);
10 MAX32664_SetFifoInterruptThreshold(0x04);
11 MAX32664_SensorEnable(true);
12 MAX32664_ReadSensorMode();
13 MAX32664_ReadSensorHubVersion();
14 MAX32664_GetNumOfSamplesInFifo();
15 receivedData = MAX32664_GetFifoData();
16 MAX32664_ReadSensorFifoLength();
17 MAX32664_ReadNumOfSamplesInSensorFifo();

line 1&2: device goes into boot loader mode successfully
line 3 : command works and indicates that MCU is MAX32664 or MAX32660
line 4 : command doesn't work and returns 0xFE that is ERR_TRY_AGAIN but trying agail also doesn't work - boot loader version is not sent to host by MAX32664D
line 5 : command doesn't work and returns 0xFE that is ERR_TRY_AGAIN but trying agail also doesn't work - boot loader pagesize which must be 8192 is not sent to host by MAX32664D
line 6&7: device goes into application mode successfully
line 8 : command doesn't work and returns 0xFE that is ERR_TRY_AGAIN but trying agail also doesn't work - unable to select estimation mode for BPT algorithm
line 9 : command worked and sensor data is selected as MAX32664D output
line 10 : command worked and interrrupt threshold is set to 0x04
line 11: command doesn't work and returns 0xFE that is ERR_TRY_AGAIN but trying agail also doesn't work - the MAX30102 deosn't get enabled
line 12: command works and indicates that MAX30102 is disable
line 13: command works and indicates that msbl file version is 40.2.2
line 14: command works and indicates that there is 0 samples in output fifo
line 15: command works and recieved data is LED1 = 0x202 , LED2 = 0x440109 ,LED3 = 0x70000 and other data are all zero.
line16: command works and indicates that input fifo length is 160
line17: command works and indicates that there is 160 samples in input fifo
why some of command do not work? is any thing I can do? is it a physical issue or corrupted msbl file? what should I do to be able to read data?
below is my library codes for each command:

bool MAX32664_EnterBootLoaderMode(void){
bool successful;
uint8_t TxBuffer[3];
uint8_t RxBuffer[1];
TxBuffer[0] = 0x01;//Family byte
TxBuffer[1] = 0x00;//Index byte
TxBuffer[2] = 0x08;//Enter boot loader mode
RxBuffer[0] = 0xFF;//Initialization
I2C_Send(TxBuffer, 3, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 1, MAX32664_ADDR);
successful = (RxBuffer[0] == 0x00)? true:false;
#ifdef DEBUG_PRINTS
System_printf(successful ? "BootLoader Mode Enabled\n" : "BootLoader Mode Failed\n");
System_flush();
#endif
return successful;
}

uint8_t MAX32664_ReadDeviceMode(void){
uint8_t TxBuffer[2];
uint8_t RxBuffer[2];
TxBuffer[0] = 0x02;//Family byte
TxBuffer[1] = 0x00;//Index byte
RxBuffer[0] = 0xff;//Reset
RxBuffer[1] = 0xff;//Initialization
I2C_Send(TxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 2, MAX32664_ADDR);
#ifdef DEBUG_PRINTS
switch(RxBuffer[1]){
case 0x00:
System_printf("Device is in application mode\n");
break;
case 0x02:
System_printf("Device is reset\n");
break;
case 0x08:
System_printf("Device is in bot loader mode\n");
break;
default:
System_printf("Invalid data received\n");
}
System_flush();
#endif
return RxBuffer[1];
}

void MAX32664_ReadMCUType(void){
uint8_t TxBuffer[2];
uint8_t RxBuffer[2] = {0xff,0xff};
TxBuffer[0] = 0xFF;//Family byte
TxBuffer[1] = 0x00;//Index byte
I2C_Send(TxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 2, MAX32664_ADDR);
#ifdef DEBUG_PRINTS
switch(RxBuffer[1]){
case 0x00:
System_printf("MCU is MAX32625\n");
break;
case 0x01:
System_printf("MCU is MAX32664 or MAX32660\n");
break;
default :
System_printf("Unknown MCU\n");
}
System_flush();
#endif
}


void MAX32664_ReadBootloaderVersion(void){
uint8_t TxBuffer[2];
uint8_t RxBuffer[4] = {0xff,0xff,0xff,0xff};
TxBuffer[0] = 0x81;//Family byte
TxBuffer[1] = 0x00;//Index byte
I2C_Send(TxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 4, MAX32664_ADDR);
#ifdef DEBUG_PRINTS
System_printf("Bootloader firmware version is %d.%d.%d \n",RxBuffer[1],RxBuffer[2],RxBuffer[3]);
System_flush();
#endif
}


uint16_t MAX32664_ReadBootloaderPageSize(void){
uint16_t pageSize;
uint8_t TxBuffer[2];
uint8_t RxBuffer[3] = {0xff,0xff,0xff};
TxBuffer[0] = 0x81;//Family byte
TxBuffer[1] = 0x01;//Index byte
I2C_Send(TxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 3, MAX32664_ADDR);
pageSize = (RxBuffer[1]<<8) + RxBuffer[2];
#ifdef DEBUG_PRINTS
System_printf("page size is %d\n",pageSize);
System_flush();
#endif
return pageSize;
}


bool MAX32664_EnterAppMode(void){
bool successful;
uint8_t TxBuffer[3];
uint8_t RxBuffer[1];
TxBuffer[0] = 0x01;//Family byte
TxBuffer[1] = 0x00;//Index byte
TxBuffer[2] = 0x00;//Exit boot loader mode,Enter application mode
RxBuffer[0] = 0xFF;//Initialization
I2C_Send(TxBuffer, 3, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 1, MAX32664_ADDR);
successful = (RxBuffer[0] == 0x00)? true:false;
#ifdef DEBUG_PRINTS
System_printf(successful ? "Application Mode Enabled\n" : "Application Mode Failed\n");
System_flush();
#endif
return successful;
}

bool MAX32664_BPTalgorithmMode(uint8_t modeByte){
bool successful;
uint8_t TxBuffer[3];
uint8_t RxBuffer[1];
TxBuffer[0] = 0x52;//Family byte
TxBuffer[1] = 0x04;//Index byte
TxBuffer[2] = modeByte;
RxBuffer[0] = 0xff;//Initialization
I2C_Send(TxBuffer, 3, MAX32664_ADDR);
Task_sleep(DURATION_MS(20));//command delay
I2C_Receive(RxBuffer, 1, MAX32664_ADDR);
successful = (RxBuffer[0] == 0x00)? true:false;
return successful;
}


bool MAX32664_SetOutputMode(uint8_t formatByte){
bool successful;
uint8_t TxBuffer[3];
uint8_t RxBuffer[1];
TxBuffer[0] = 0x10;//Family byte
TxBuffer[1] = 0x00;//Index byte
TxBuffer[2] = formatByte;
RxBuffer[0] = 0xff;//Initialization
I2C_Send(TxBuffer, 3, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 1, MAX32664_ADDR);
successful = (RxBuffer[0] == 0x00)? true:false;
return successful;
}


bool MAX32664_SetFifoInterruptThreshold(uint8_t thrByte){
bool successful;
uint8_t TxBuffer[3];
uint8_t RxBuffer[1];
TxBuffer[0] = 0x10;//Family byte
TxBuffer[1] = 0x01;//Index byte
TxBuffer[2] = thrByte;
RxBuffer[0] = 0xff;//Initialization
I2C_Send(TxBuffer, 3, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 1, MAX32664_ADDR);
successful = (RxBuffer[0] == 0x00)? true:false;
return successful;
}


bool MAX32664_SensorEnable(bool enable){
bool successful;
uint8_t TxBuffer[3];
uint8_t RxBuffer[1];
TxBuffer[0] = 0x44;//Family byte
TxBuffer[1] = 0x03;//Index byte
TxBuffer[2] = (enable)? 0x01:0x00;
RxBuffer[0] = 0xff;//Initialization
I2C_Send(TxBuffer, 3, MAX32664_ADDR);
Task_sleep(DURATION_MS(40));//command delay
I2C_Receive(RxBuffer, 1, MAX32664_ADDR);
successful = (RxBuffer[0] == 0x00)? true:false;
return successful;
}


uint8_t MAX32664_ReadSensorMode(void){
uint8_t TxBuffer[2];
uint8_t RxBuffer[2];
TxBuffer[0] = 0x45;//Family byte
TxBuffer[1] = 0x03;//Index byte
RxBuffer[0] = 0xff;//Initialization
RxBuffer[1] = 0xff;//Initialization
I2C_Send(TxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 2, MAX32664_ADDR);
#ifdef DEBUG_PRINTS
switch(RxBuffer[1]){
case 0x00:
System_printf("MAX30101/2 is disabled\n");
break;
case 0x01:
System_printf("MAX30101/2 is enabled\n");
break;
}
System_flush();
#endif
return RxBuffer[1];
}

void MAX32664_ReadSensorHubVersion(void){
uint8_t TxBuffer[2];
uint8_t RxBuffer[4];
TxBuffer[0] = 0xff;//Family byte
TxBuffer[1] = 0x03;//Index byte
RxBuffer[0] = 0xff;//Initialization
RxBuffer[1] = 0xff;//Initialization Major version byte
RxBuffer[2] = 0xff;//Initialization Minor version byte
RxBuffer[3] = 0xff;//Initialization Revision byte
I2C_Send(TxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 4, MAX32664_ADDR);
#ifdef DEBUG_PRINTS
System_printf("SensorHub Version is %d.%d.%d \n",RxBuffer[1],RxBuffer[2],RxBuffer[3]);
System_flush();
#endif
}


uint8_t MAX32664_GetNumOfSamplesInFifo(void){
uint8_t TxBuffer[2];
uint8_t RxBuffer[2];
TxBuffer[0] = 0x12;//Family byte
TxBuffer[1] = 0x00;//Index byte
RxBuffer[0] = 0xff;//Index byte
RxBuffer[1] = 0xff;//Index byte
I2C_Send(TxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
return RxBuffer[1];
}


fifoData MAX32664_GetFifoData(void){
fifoData receivedData;
uint8_t TxBuffer[2];
uint8_t RxBuffer[20]={0};
TxBuffer[0] = 0x12;//Family byte
TxBuffer[1] = 0x01;//Index byte
I2C_Send(TxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 20, MAX32664_ADDR);
receivedData = MAX32664_RawDataToFifoData(RxBuffer);
Task_sleep(DURATION_MS(45));//command delay
return receivedData;
}


fifoData MAX32664_RawDataToFifoData(uint8_t *RxBuffer){
fifoData receivedData;
receivedData.err = RxBuffer[0];
receivedData.led_1 = (RxBuffer[1]<<16) + (RxBuffer[2]<<8) + RxBuffer[3];
receivedData.led_2 = (RxBuffer[4]<<16) + (RxBuffer[5]<<8) + RxBuffer[6];
receivedData.led_3 = (RxBuffer[7]<<16) + (RxBuffer[8]<<8) + RxBuffer[9];
receivedData.led_4 = (RxBuffer[10]<<16) + (RxBuffer[11]<<8) + RxBuffer[12];
receivedData.status = RxBuffer[13];
receivedData.progress = RxBuffer[14];
receivedData.hr = RxBuffer[15];
receivedData.sys = RxBuffer[16];
receivedData.dia = RxBuffer[17];
receivedData.spo2 = RxBuffer[18];
receivedData.r = RxBuffer[19];
receivedData.hrAboveResting = RxBuffer[20];
return receivedData;
}


uint16_t MAX32664_ReadSensorFifoLength(void){
uint16_t fifoLength;
uint8_t TxBuffer[2] ;
uint8_t RxBuffer[3] = {0xff};
TxBuffer[0] = 0x13;
TxBuffer[1] = 0x01;
I2C_Send(TxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 3, MAX32664_ADDR);
fifoLength = (RxBuffer[1]<<8) + RxBuffer[2];
#ifdef DEBUG_PRINTS
System_printf("fifo length is %d\n",fifoLength);
System_flush();
#endif
return fifoLength;
}


uint16_t MAX32664_ReadNumOfSamplesInSensorFifo(void){
uint16_t numOfSamples;
uint8_t TxBuffer[2] ;
uint8_t RxBuffer[3] = {0xff};
TxBuffer[0] = 0x13;
TxBuffer[1] = 0x01;
I2C_Send(TxBuffer, 2, MAX32664_ADDR);
Task_sleep(DURATION_MS(2));//command delay
I2C_Receive(RxBuffer, 3, MAX32664_ADDR);
numOfSamples = (RxBuffer[1]<<8) + RxBuffer[2];
#ifdef DEBUG_PRINTS
System_printf("number of samples currently in the sensor FIFO is %d\n",numOfSamples);
System_flush();
#endif
return numOfSamples;
}

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +2 verified
    Have you tried comparing with the Maxim example code? According to the documentation: Sample Python code to perform IAP using the MAX32630FTHR as the host can be found in the folder “max32660_bootloader_src…
  • dougw
    dougw over 3 years ago +1
    Have you tried using a longer command delay?
  • AliMozaffari
    AliMozaffari over 3 years ago in reply to shabaz +1
    thanks. I tried it and I'm waiting for maxim engineers response
Parents
  • shabaz
    +1 shabaz over 3 years ago

    Have you tried comparing with the Maxim example code?

    According to the documentation:

    Sample Python code to perform IAP using the MAX32630FTHR as the host can be found in the folder “max32660_bootloader_src\scripts\py.” Download the MAX32660 bootloader software, sample host code, .msbl generator, and the sample .msbl code from the MAX32660 Design Resources tab.

    I've not used this device, so I don't know the solution, but it may be good to compare, in case they are setting anything else (e.g. timeout to exit bootloader mode may be too low perhaps?). That's assuming that documentation is referring to code that interacts with the bootloader in int MAX32664 of course. I have not found that code.

    Otherwise, it's best to ask Maxim to provide demo code (for any target device), which they should have, at least for their MAX3xxxxx microcontrollers, and then at least you have known working code to compare yours with, even though you are using a different microcontroller.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • shabaz
    +1 shabaz over 3 years ago

    Have you tried comparing with the Maxim example code?

    According to the documentation:

    Sample Python code to perform IAP using the MAX32630FTHR as the host can be found in the folder “max32660_bootloader_src\scripts\py.” Download the MAX32660 bootloader software, sample host code, .msbl generator, and the sample .msbl code from the MAX32660 Design Resources tab.

    I've not used this device, so I don't know the solution, but it may be good to compare, in case they are setting anything else (e.g. timeout to exit bootloader mode may be too low perhaps?). That's assuming that documentation is referring to code that interacts with the bootloader in int MAX32664 of course. I have not found that code.

    Otherwise, it's best to ask Maxim to provide demo code (for any target device), which they should have, at least for their MAX3xxxxx microcontrollers, and then at least you have known working code to compare yours with, even though you are using a different microcontroller.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • AliMozaffari
    0 AliMozaffari over 3 years ago in reply to shabaz

    thanks. I tried it and I'm waiting for maxim engineers response