Bridgetek
  • Products & Partners
  • Manufacturers
  • Bridgetek
  • More
  • Cancel
Bridgetek
Documents Press Release - Latest Higher Resolution EVE ICs from Bridgetek Now Designed into High-End Riverdi Displays
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Bridgetek to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 12 Mar 2021 1:57 AM Date Created
  • Last Updated Last Updated: 6 Oct 2021 10:34 PM
  • Views 872 views
  • Likes 2 likes
  • Comments 0 comments
Related
Recommended

Press Release - Latest Higher Resolution EVE ICs from Bridgetek Now Designed into High-End Riverdi Displays

1st February 2021 - Bridgetek has gained a high-profile endorsement for its latest generation of embedded video engine (EVE) graphic controllers. Relying on the recently announced BT817 EVE4 devices, leading optoelectronics manufacturer Riverdi has introduced a new family of displays. These industrial-grade units are targeted at challenging higher-end applications, but are positioned at attractive price points that are in line with commercial level products. 

 

Thanks to the heightened degrees of precision associated with the BT817 ICs, the new Riverdi displays are able to benefit from 1280x800 pixel resolution. Treating the rendered content as a series of objects reduces the data overheads involved dramatically. This translates into a more streamlined solution, with a substantially lower component count plus accelerated responsiveness. 

 

“By engaging with Bridgetek, we have been able to develop a display family that sets new benchmarks. The ultra-integrated EVE4 solution means that quicker reaction times and superior resolution levels are possible, while still saving valuable board space and keeping power budgets down,” states Kamil Kozłowski, CTO at Riverdi. “Consequently, we have decided to take a platform approach and apply it across the whole family, from the smaller units all the way up to the largest formats,”

 

“It is clear that the user experiences which people are familiar with from interacting with consumer goods have set elevated expectations for HMIs in other areas too,” adds Bridgetek’s founder and CEO Fred Dart. “Higher resolution displays with faster responsiveness are now mandated in a wide array of different sectors. This is why the value of our BT817 and BT818 is becoming so apparent to OEMs, giving them the opportunity to meet their customers’ requirements without needing complex expensive subsystems that take up board real estate or draw excessive power.”

 

The EVE-based Riverdi displays are available in a wide range of different size formats, spanning from 3.5-inch all the way through 4.3-inch, 5.0-inch and 7.0-inch to 10.1-inch. Use of in-plane switching (IPS) technology results in a brighter output (delivering up to 1000cd/m2). It also means that these units have enhanced colour rendering and much wider viewing angle capabilities. Optical bonding is incorporated into the display assemblies as standard, even for single pieces - thereby preventing condensation, mitigating internal reflections and boosting optical performance, as well as delivering far greater durability. The projected capacitive touchscreens featured in these displays allow touch interaction through protective glass that is as much as 15mm thick, and also enables gloved operation to be supported.

 

Assisted by innovative Bridgetek engineering, the new Riverdi displays are optimised for addressing the most demanding tasks. They will be implemented into medical diagnostic instrumentation, home healthcare monitoring equipment, electric vehicle charging infrastructure, industrial automation systems, vending machines, etc. Exceptionally strong electro-magnetic interference (EMI) and electro-static discharge (ESD) immunity characteristics are exhibited, along with a working temperature range covering -20°C to +70°C.

 

About Bridgetek

Founded in 2016, Bridgetek supplies highly advanced ICs and board level products to meet the exacting demands of a constantly evolving global technology landscape. The company's Embedded Video Engine (EVE) graphic controller ICs each integrate display, audio and touch functionality onto a single chip, thereby dramatically reducing the time period and bill-of-materials costs associated with developing next generation Human Machine Interface (HMI) systems. These are complemented by its highly differentiated, speed-optimized microcontroller units (MCUs) with augmented connectivity features.

 

For more information go to www.brtchip.com

  • bridgetekeve
  • bridgetek
  • press release
  • evechip