Connective Peripherals
  • Products
  • Manufacturers
  • Connective Peripherals
  • More
  • Cancel

Connective Peripherals

  • Blog
  • Forum
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Connective Peripherals to participate - click to join for free!

image

Welcome to the Connective Peripherals page on element14. Here you can find things such as our latest news, training videos, and product details. Additionally, you can engage with us in our forums.

Featured Video

image

Recent Videos
  • You don't have permission to edit metadata of this video.
    Edit media
    x
    Upload Preview
    CP Type C Cables - Application Examples
    over 2 years ago
  • You don't have permission to edit metadata of this video.
    Edit media
    x
    Upload Preview
    Connective Peripherals - Isolated Adapter Pro Series Configuration Video
    over 2 years ago
  • You don't have permission to edit metadata of this video.
    Edit media
    x
    Upload Preview
    Applications of USBC-H-422/485-M PRO Series Adapters
    over 2 years ago
Have a Question?
Related Products
Connective Peripherals Pte Ltd is a supplier of communications and instrumentation products, with expertise in serial connectivity solutions that are based on USB, CAN and RS232/RS422/RS485 interfaces. The company’s products encompass adapter boards and cables delivering connectivity between USB and serial interfaces, plus award-winning USB based oscilloscopes, data loggers and logic analysers. OEM and ODM design services are also offered. Headquartered in Singapore, in the heart of the Asia Pacific region, the company’s dedication to quality of service and exceptional technical support has been appreciated by both corporate and individual customers. As a result, its sales have extensively expanded into the global market.
Latest News
  • Applications of the CP-CANFD Adapters

    BRT-Marketing
    BRT-Marketing

    Introduction 

    The renowned CAN (Controller Area Network) Bus was originally designed to address requirements for automotive applications, bringing reliability, high speed, multi-master capabilities, and simplified wiring, amongst other important benefits. However, it has been adopted by a wide range of other industries whose requirements align closely with these features. The CAN protocol has also evolved to meet the greater demands of today’s applications. For example, CAN FD (CAN Flexible Data Rate) offers much higher performance and flexibility whilst remaining backward compatible with the Classical CAN Bus.  

    Some of the many applications of the CP-CANFD

    Connecting CAN to Computers 

    Whilst CAN and CAN FD are primarily used to network a series of ECUs (Electronic Control Units) and other MCU-based (Microcontroller) modules, interfacing them to a computer is often required for tasks such as:  

    • Development, Test and Debug of components and modules 
    • Monitoring of industrial systems and buildings 
    • Controlling devices via a computer-based user interface
    • Configuration, Diagnostics and Firmware Updates

    image

    Connecting a CAN / CAN FD Network to a computer over USB

    Challenges in Selecting an Interface 

    There are several challenges in finding the right interface solution for the application, including:  

    • Support for CAN Protocols used in the application now and in future  
    • Robust Hardware Features for a long-term reliable operation
    • Extensive Software Support ensuring application requirements can be met

    CP-CANFD Adapters 

    The CP-CANFD USB to CAN/CAN FD adapters have a range of features which address these challenges including: 

    Support for CAN Protocols 

    Support for both CAN FD and Classical CAN 

    The CP-CANFD communicates with both CAN and CAN FD nodes on the same bus seamlessly. This is a significant benefit for development of systems or components for Automotive and EV (Electric Vehicle) applications, where a combination of CAN and CAN FD nodes reside on the same bus. The Hi-Speed USB connection to the computer also avoids common concerns about throughput. 

    image

    Dual Channel Versions 

    USB to CAN interfaces are a very useful tool when designing and validating devices which use CAN and CAN FD. This includes development of Integrated Circuits and MCUs, hardware modules and the associated firmware. One channel of the CP-CANFD can act as a CAN node to exercise the Device Under Test and the other channel to capture bus data in Listen-Only mode. 

    Robust Hardware Features 

    Galvanic Isolation  

    Applications such as factory and building automation involve high-power machines and systems connected to different mains power sources. Galvanic isolation in the isolated versions of the CP-CANFD (with part number ending in -ISO) provides a protective barrier between the CAN and USB ports, preventing spikes, surges and ground loops from damaging the computer. Additional surge protection helps protect the CP-CANFD itself from spikes on the CAN Bus. These features are also invaluable for R&D and testing purposes where a connection error or fault in a connected CAN device could result in damage to the computer. 

    Compact Unit with USB Connection 

    The CP-CANFD is supplied in a robust industrial grade enclosure. Mounting ears provide secure mounting in fixed applications. The compact and lightweight unit, powered entirely over USB, is ideal for diagnostics and firmware updates in the field. 

     image

    Extensive Software Support 

    Ready-To-Use Software 

    Software is an important factor in the useability and functionality of a USB to CAN solution. The CP-CANFD includes the ready-to-use CP-CANFD Utility as well as support for popular 3rd party applications such as Busmaster. The driver of CP-CANFD can be easily installed on computers running Windows 7 to 11, Windows Server and Linux, with Linux SocketCAN (SLCAN) support. 

    Software Development 

    By providing libraries in various programming languages and control via the CP-CANFD's Virtual COM Port (VCP), it offers a wealth of options for developing custom control software and user interfaces. This flexibility also allows users to implement additional layers on top of the CAN protocol, such as ARINC 825 for aerospace applications. 

     

    Find Out More 

    CAN continues to be one of the go-to protocols for a wide range of applications which require reliable communications, even more so with the introduction of enhanced versions such as CAN FD. The essential role that computers play in developing, configuring, monitoring and controlling CAN and CAN FD devices demands an effective interface between the computer and CAN Bus.  

    With their comprehensive hardware features and software support, the new CP-CANFD adapters offer an easy to use solution for flexible and reliable USB to CAN/CAN FD interfacing across a wide range of applications.  

    The following models are available now at www.connectiveperipherals.com 

    CP-CANFD-1P  

    USB to single CAN FD Adapter (non-isolated) 

    CP-CANFD-1P-ISO 

    USB to single CAN FD Adapter (galvanic isolation) 

    CP-CANFD-2P 

    USB to dual CAN FD Adapter (non-isolated) 

    CP-CANFD-2P-ISO 

    USB to dual CAN FD Adapter (galvanic isolation) 

     For more information on the new CP-CANFD range, please visit our CP-CANFD product page or contact our Sales team 

    • 8 May 2025
  • Introducing USB to CAN-FD Adapters

    BRT-Marketing
    BRT-Marketing
    Introducing the new industrial-grade CP-CAN FD USB to CAN FD (Controller Area Network Flexible Data-Rate) adapters from Connective Peripherals. With these adapters, you can easily monitor and control devices which communicate via classical CAN bus and the higher performance CAN FD from computers and notebooks. Four models are available, with single and dual CAN FD channel versions, as well as galvanically isolated (-ISO) versions of each.
    image
    Product Highlights include:
    • Connect one or two CAN FD Buses to a computer via a single USB connection
    • Support for both CAN FD (up to 8Mbps) and Classical CAN 2.0 A/B (up to 1Mbps)
    • Hi-Speed USB connection ensures high performance yet simple installation
    • Galvanically Isolated versions protect the computer from CAN bus surges and spikes
    • Drivers for Windows 7 to 11, Windows Server, and Linux. Linux SocketCAN (SLCAN) support
    Applications of the CP-CAN FD adapters include:
    • Automotive
    • Transportation
    • Robotics
    • Building automation
    • Factory automation
    • Industrial equipment
    • 24 Apr 2025
  • Type C Cables - Application Examples

    BRT-Marketing
    BRT-Marketing
    Our Type C USB interface cables are ideal for connecting serial devices to a USB Type C port on your computer without additional adapters!
    We have versions with RS232, UART, High Speed UART and MPSSE (for SPI, I2C, JTAG and GPIO)
    Perfect for connecting all kinds of devices to the computer including:
    - Legacy RS232 products
    - Microcontrollers and logic devices via UART and JTAG
    - Sensors via SPI/I2C/JTAG/GPIO
    - And many more….
    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image
    • 6 Mar 2024
  • Technical Insight – USBC-H-422/485-M PRO and -ISO PRO Series

    BRT-Marketing
    BRT-Marketing

    CP PRO series adapters are designed from the ground up to address many of the common challenges in setting up and using USB-RS422/485 adapters.

    No more configuration by jumpers or DIP switches - configuration is now achieved via Software over USB - EASY!

    Read more : https://bit.ly/42omP5i

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • 2 Feb 2024
  • Applications of USBC-H-422/485-M PRO Series Adapters

    BRT-Marketing
    BRT-Marketing
    CP PRO series adapters are designed from the ground up to address many of the common challenges in setting up and using USB-RS422/485 adapters.
    Our reliable and convenient solution also helps you save time with its simple configuration.
    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image
    • 29 Jan 2024
  • USB to Serial converters with Optical Isolation

    cp_marketing
    cp_marketing

    Connective Peripherals offer a wide range of USB to serial solutions for a variety of applications.

    Attachments:
    imageUSB to Serial converters with Optical Isolation.pdf
    • 7 Jul 2021
Documentation
  • ChristyZ
    Group Intro Widget Content
    By ChristyZ > > over 4 years ago

  • Matt
    Setup
    By Matt > > over 4 years ago

  • Matt
    Featured Video
    By Matt > > over 4 years ago

  • Matt
    Main Group Widget
    By Matt > > over 4 years ago

  • cp_marketing
    Press Release - High-Speed & Full-Speed USB Type-C Serial Adapter Cables
    By cp_marketing > > over 4 years ago

  • migration.user
    Polls
    By migration.user > > over 4 years ago

  • migration.user
    Documents
    By migration.user > > over 4 years ago