Digilent, a National Instruments Company
  • Products & Partners
  • Manufacturers
  • Digilent, a National Instruments Company
  • More
  • Cancel
Digilent, a National Instruments Company
Blog Digilent launches The Analog Discovery Pro model ADP3450
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Digilent, a National Instruments Company to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jomoenginer
  • Date Created: 8 Apr 2021 8:30 PM Date Created
  • Views 9322 views
  • Likes 5 likes
  • Comments 2 comments
  • logic analyzer
  • ocilloscope
  • spectrum analyzer
  • digilent analog discovery pro
  • matlab
  • labview
  • test & measurement
Related
Recommended

Digilent launches The Analog Discovery Pro model ADP3450

jomoenginer
jomoenginer
8 Apr 2021

Digilent has officially launched their new Analog Discovery Pro model ADP3450 with a price of $1295 US.  The Analog Discovery Pro ADP3450 is a professional bench-top tool which includes a wide variety of features.  This might not be the cheapest option for the Maker type, but it does look like a nice mid range tool for more of a professional or consulting application.

 

It would make for a cool RoadTest though.

 

Digilent Analog Discovery Pro ADP3450

https://store.digilentinc.com/analog-discovery-pro-3000-series-portable-high-resolution-mixed-signal-oscilloscopes/

 

Digilent Analog Discovery Pro 3000 Series

 

Some of the features include:

Analog Inputs:

 

  • ADP3450: Four analog input channels accessible via front panel BNC connectors
    • ADP3250 Two analog input channels (coming soon)
  • Analog bandwidth: 55+ MHz @ 3 dB
  • Noise limiting hardware bandwidth filter: 20 MHz
    • 14-bit resolution (16-bit resolution with oversampling)
  • Input range ±25 V (±50 V diff)
  • Input protected to ±50 V
  • Max sampling rate:
    • 0.5 GS/s (with oversampling enabled)
    • 100 MS/s default
  • AC or DC coupling

 

Analog Outputs:

  • Used in the Waveform Generator, Impedance Analyzer, and Network Analyzer
  • Two arbitrary waveform generator channels, accessible via front panel BNC connectors
  • 14-bit Resolution
  • AC amplitude (max): ±5 V
  • Analog bandwidth: 15 MHz @ 3 dB
  • Maximum Sampling Rate: 125 MS/s

 

Digital Inputs and Outputs:

 

  • Channels: 16
  • Input logic standard: LVCMOS (adjustable 1.2 V to 3.3 V, 5 V tolerant)
  • Output logic standard: LVCMOS (adjustable 1.2 V to 3.3 V, 8 mA)
  • Max sampling rate: 125 MS/s
  • Logic analyzer buffer memory:
  • 64 MS total in Record Mode
  • 32 k+ per channel in Repeated/Shift/Screen modes

 

Connectivity:

 

  • Device to computer: USB or Ethernet connection (in Linux or Standard Modes)
  • 4 High-speed USB 2.0 ports for peripheral connection (enabled in Linux mode)
  • Enabled for set and tested WiFi dongles (in Linux Mode)

 

Software

  • WaveForms
    • Oscilloscope
    • Waveform Generator
    • Power Supplies
    • Voltmeter
    • Data Logger
    • Logic Analyzer
  • Pattern Generator
  • Static I/O
  • Spectrum Analyzer
  • Network Analyzer
  • Impedance Analyzer
  • Protocol Analyzer
  • Supported with:
    • LabVIEW
    • MATLAB
    • Python
    • C++
  • Sign in to reply
  • michaelkellett
    michaelkellett over 5 years ago

    Thanks for the heads up. It's interesting , but .............................

     

    4 channel scope 55 MHz for $1300 - very poorly specified (I don't mean bad figures, just an absence of figures )

    For example I can't tell how many ranges it has - looks like 2.

    Update rate not specified.

     

    Compare with the specs for Tek, Keysight,R&S, Rigol and Pico - all of them provide this information and much more.

    (Pico 5442D MSO is flex resolution £1365, 60MHz, all the others offer scopes with screens in this price range)

    The Digilent price does not include probes.

     

    It does have some interesting features - like the network analyser but the spec says so little about performance that I can't tell if it would be much use.

    (Pico offer free software add on for bode plotting (on scopes with AWG) - other scopes have similar offerings)

     

    If NI/Digilent want to break into the serious scope market they'll need to raise their game.

     

    A RoadTest would be good idea - it would answer some of my questions.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kk99
    kk99 over 5 years ago

    Awesome tool.