Digilent, a National Instruments Company
  • Products & Partners
  • Manufacturers
  • Digilent, a National Instruments Company
  • More
  • Cancel
Digilent, a National Instruments Company
Blog DPS3340 Discovery USB Programmable Power Supply
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Digilent, a National Instruments Company to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: steveradecky
  • Date Created: 17 Apr 2023 4:18 PM Date Created
  • Views 5363 views
  • Likes 4 likes
  • Comments 2 comments
Related
Recommended

DPS3340 Discovery USB Programmable Power Supply

steveradecky
steveradecky
17 Apr 2023

DPS3340 is a three channel variable DC programmable power supply. It allows users to control the power provided to external circuits. Providing both constant voltage and constant current modes with built in readback sensors and optional tracking for the output channels, users can confidently power circuits according to their requirements.

image

The included WaveForms software application enables the use of three programmable DC outputs. The software features a friendly user interface that has the feel of traditional benchtop software. The Discovery USB Programmable Power Supply communicates with WaveForms via a USB connection to your computer, allowing users to control the power supply outputs and enable overcurrent protections.  In addition to the use of instruments in the application, the WaveForms application has a script editor tool, which allows custom scripting of the instrument in JavaScript. WaveForms is designed to be run on a laptop or desktop computer and is Mac, Windows, and Linux compatible. The DPS3340 can also be used with other Digilent Test and Measurement devices like the Analog Discovery Series of products.

image

  • The following instruments are available in the WaveForms application for the Discovery USB Programmable Power Supply:
    • In stand-alone mode:
      • Power Supplies
      • Waveform Generator
      • Meter
    • In conjunction with another Digilent Test and Measurement device:
      • Power Supplies

For even more customization potential, the WaveForms Software Development Kit (SDK) can be used to create custom applications and scripts in Python, C, and additional languages. The Discovery USB Programmable Power Supply is also compatible with LabVIEW and the Digilent Toolbox add-on available for MATLAB.

DPS3340 specs:

  • 1 V to 5 V / 10 mA to 3 A output
  • -1 V to -15 V / -10 mA to -500 mA output
  • 1 V to 15 V / 10 mA to 500 mA output
  • Optional tracking between the -15 V and 15 V outputs
  • Overcurrent protection options provided through WaveForms
  • Auxiliary powered — 19 V +/- 5%, 3.2 A maximum, 60 W maximum, 5.5 mm x 1.65 mm, center positive
  • Sign in to reply

Top Comments

  • colporteur
    colporteur over 3 years ago +1
    I thought it might be a replacement for my project board PS but at $750 US that is some serious coin for such a device. I looked through the specs and found nothing that suggests I would purchase the unit…
  • steveradecky
    steveradecky over 3 years ago in reply to colporteur

    The price should be $495. Looks like there is an error in the listing you're seeing. Should be updated soon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 3 years ago

    I thought it might be a replacement for my project board PS but at $750 US that is some serious coin for such a device. I looked through the specs and found nothing that suggests I would purchase the unit for this reason. Can anyone provide some insight? What am I missing?