Digilent, a National Instruments Company
  • Products
  • Manufacturers
  • Digilent, a National Instruments Company
  • More
  • Cancel
Digilent, a National Instruments Company
Blog New Product Release - Analog Discovery 2 Pro Bundle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Digilent, a National Instruments Company to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: alexwonglik1
  • Date Created: 25 Aug 2019 10:06 AM Date Created
  • Views 2198 views
  • Likes 3 likes
  • Comments 2 comments
  • bundle
  • ad2
  • analog discovery bundle
  • digilent bundle
  • digilent pro bundle
  • bnc
  • bnc adaptor
  • pro bundle
  • digilent
  • analog discovery 2
  • analog discovery
Related
Recommended

New Product Release - Analog Discovery 2 Pro Bundle

alexwonglik1
alexwonglik1
25 Aug 2019

image

 

Start verifying and testing a wide range of projects with the Analog Discovery 2 Pro Bundle. With the addition of the BNC adapter and scope probes, professional or experienced engineers can access the full 30MHz bandwidth oscilloscope and 12MHz bandwidth waveform generator.

 

Analog Discovery 2 Pro Bundle Includes:

  • BNC Adapter Board for the Analog Discovery 2
  • BNC Oscillosope x1/x10 Probes (Pair)
  • Mini Grabber Test Clips (6 pack)
  • Analog Discovery 2

 

 

 

 

image

 

Analog Discovery 2

 

Digilent Analog Discovery 2 is a USB oscilloscope and multi-function instrument that allows users to measure, visualize, generate, record, and control mixed-signal circuits of all kinds. Analog Discovery 2 is small enough to fit in your pocket, but powerful enough to replace a stack of lab equipment, providing engineering students, hobbyists, and electronics enthusiasts the freedom to work with analog and digital circuits in virtually any environment, in or out of the lab. Driven by the free WaveForms (Mac, Linux and Windows Compatible) software, Analog Discovery 2 can be configured to work as anyone of several traditional instruments including an Oscilloscope, Waveform Generator, Power Supply, Voltmeter, Data Logger, Logic Analyzer, Pattern Generator, Static I/O, Spectrum Analyzer, Network Analyzer, Impedance Analyzer, and Protocol Analyzer.

 

 

image

 

BNC Adapter for Analog Discovery 2

 

The BNC Adapter Board for the Analog Discovery 2 is intended to be used with the Analog Discovery 2 tool to enable the use of standard BNC-terminated test leads and probes. It provides BNC terminations to each of the two oscilloscope channels on the Analog Discovery 2. Each channel of the oscilloscope can be selected as AC or DC coupled by adjusting the jumper that is located behind that channel's BNC input connector. In addition, the two AWG channels are also equipped with BNC terminations, and each channel can have either the 50-ohm or the 0-ohm termination selected. This enables the user to match the Analog Discovery 2's output impedance with either standard 50-ohm test leads or to be directly tied to the lead.

 


image

 

BNC Oscilloscope x1/x10 Probes (Pair)

 

A pair of BNC-terminated oscilloscope probes, perfect for use with the Analog Discovery 2 in conjunction with the BNC Adapter Board for the Analog Discovery 2.

 

 

image

 

Mini Grabber Test Clips (6-pack) for use with Instrumentation Flywires

 

These micro-hook test clips allow the Analog Discovery 2 signal wires to be connected to component leads, wires, and other circuit components. The spring-action clips use two-lead pincers to grab onto conductors up to 1.27mm in diameter. When released, the pincers hold tightly for good electrical contact.

  • Sign in to reply

Top Comments

  • alexwonglik1
    alexwonglik1 over 6 years ago in reply to clem57 +1
    Hey! We don’t plan to have a roadtest at the moment, but there will be a webinar about Analog Discovery 2. You can register for the webinar here: Expanding your Test and Measurement Workbench Beyond the…
Parents
  • clem57
    clem57 over 6 years ago

    Hope there is a plan for  RoadTests & Reviews. I bet many would be interested. Thanks alexwonglik1 for pointing out the release of the Analog Discovery 2 bundle.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 6 years ago

    Hope there is a plan for  RoadTests & Reviews. I bet many would be interested. Thanks alexwonglik1 for pointing out the release of the Analog Discovery 2 bundle.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • alexwonglik1
    alexwonglik1 over 6 years ago in reply to clem57

    Hey! We don’t plan to have a roadtest at the moment, but there will be a webinar about Analog Discovery 2.

    You can register for the webinar here: Expanding your Test and Measurement Workbench Beyond the Lab with the Analog Discovery 2

    Thanks!