Eaton
  • Products & Partners
  • Manufacturers
  • Eaton
  • More
  • Cancel
Eaton
Forum Help with Eaton easy-E4-UC-12RC1
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Eaton to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 26 subscribers
  • Views 2254 views
  • Users 0 members are here
Related

Help with Eaton easy-E4-UC-12RC1

lopes47
lopes47 over 2 years ago

Good afternoon everyone,
I don't know if you can help me but I have a problem where I am using an eaton easy-E4-UC-12RC1 plc and I have simply programmed it so that when a box passes the photocell it triggers an electrovalve. But when I pass a box through the photocell, it doesn't activate the solenoid valve. If you could help me, I'd really appreciate it.
The programming I have is I01--------()Q01.

image 

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 2 years ago +1
    Which model of photocell are you using? And is that a PSU top left?
  • kmikemoo
    kmikemoo over 2 years ago +1
    After writing a bunch of hardware "try this", I'm opting for a simple programming idea; use the input to set a variable and the variable to drive the output. PLC's read inputs, run the logic (ladder) and…
Parents
  • kmikemoo
    0 kmikemoo over 2 years ago

    After writing a bunch of hardware "try this", I'm opting for a simple programming idea; use the input to set a variable and the variable to drive the output.  PLC's read inputs, run the logic (ladder) and write outputs.  You may need the internal variable to bridge from read to write.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kmikemoo
    0 kmikemoo over 2 years ago

    After writing a bunch of hardware "try this", I'm opting for a simple programming idea; use the input to set a variable and the variable to drive the output.  PLC's read inputs, run the logic (ladder) and write outputs.  You may need the internal variable to bridge from read to write.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mp2100
    0 mp2100 over 2 years ago in reply to kmikemoo

    Lopez47. You’re concept is correct but I agree with kmikemoo and phoenixcomm.  Are you sure the photocell is sending a signal? That the PLC can read?  Is the solenoid getting the voltage it requires?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • CAPDRILL
    0 CAPDRILL over 1 year ago in reply to mp2100

    Eaton showing no connection 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer