Fluke
  • Products & Partners
  • Manufacturers
  • Fluke
  • More
  • Cancel
Fluke
Forum Benchtop multimeters
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Fluke to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 19 subscribers
  • Views 2036 views
  • Users 0 members are here
  • Fluke Connect
  • Digital Multimeters
  • Motor & Drives
Related

Benchtop multimeters

deoli
deoli over 6 years ago

Hi

New to this site.

Cant decide between  two benchtop multimeters

1 Fluke 8808A

2 Keithly 2110 240

Any advice out there?

thanks

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +1
    I wouldn't buy either of those meters - both rather old designs of 5.5 digit DMM. If you don't need high accuracy and USB/network connectivity - think about getting a Fluke handheld meter - the only problem…
Parents
  • Gough Lui
    0 Gough Lui over 6 years ago

    I reviewed the Keithley Model 2110 quite a while ago and posted a follow-up:

    • Review of Keithley 2110-120 Digital Multimeter
    • One Year after the RoadTest: Keithley 2110 Digital Multimeter

     

    Other RoadTesters have also reviewed the 2110:

    • Review of Keithley 2110-120 Digital Multimeter
    • Review of Keithley 2110-120 Digital Multimeter

     

    Note that the final three digits is just the voltage the Keithley comes pre-configured for. You can change that by rotating the fuse block. In all, it has been a reliable meter and I'm still using it now, even though it seems to be manufactured for Keithley by Picotest by the looks of it and stock of the 2110 seem to be fairly rare now.

     

    I took a quick look at the Fluke specifications and it seems like an older type of meter. The accuracy specifications are generally similar or slightly lower for the Fluke, and it seems that it doesn't have as many types of supported measurements (e.g. thermocouples, capacitor) and the remote control interface is more old fashioned using RS-232RS-232 whereas the Keithley has USB. On the other side, Fluke does have an innovative 4-wire measurement system assuming you also buy their lead-set, and they have a brand reputation that might be a bit more recognisable than a Keithley OEMed by Picotest. For those that need a display with a great viewing angle, the Fluke has a real VFD where the Keithley 2110 uses an inverse-LCD. That being said, I'm not sure if the 8808A is a "real" Fluke at heart either, having never used one myself.

     

    Really, it depends on what you value most and what your requirements are. What sort of measurements will you be doing? Is automation a big deal? Is accuracy most important? What about warranty/support where you are? etc.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 6 years ago

    I reviewed the Keithley Model 2110 quite a while ago and posted a follow-up:

    • Review of Keithley 2110-120 Digital Multimeter
    • One Year after the RoadTest: Keithley 2110 Digital Multimeter

     

    Other RoadTesters have also reviewed the 2110:

    • Review of Keithley 2110-120 Digital Multimeter
    • Review of Keithley 2110-120 Digital Multimeter

     

    Note that the final three digits is just the voltage the Keithley comes pre-configured for. You can change that by rotating the fuse block. In all, it has been a reliable meter and I'm still using it now, even though it seems to be manufactured for Keithley by Picotest by the looks of it and stock of the 2110 seem to be fairly rare now.

     

    I took a quick look at the Fluke specifications and it seems like an older type of meter. The accuracy specifications are generally similar or slightly lower for the Fluke, and it seems that it doesn't have as many types of supported measurements (e.g. thermocouples, capacitor) and the remote control interface is more old fashioned using RS-232RS-232 whereas the Keithley has USB. On the other side, Fluke does have an innovative 4-wire measurement system assuming you also buy their lead-set, and they have a brand reputation that might be a bit more recognisable than a Keithley OEMed by Picotest. For those that need a display with a great viewing angle, the Fluke has a real VFD where the Keithley 2110 uses an inverse-LCD. That being said, I'm not sure if the 8808A is a "real" Fluke at heart either, having never used one myself.

     

    Really, it depends on what you value most and what your requirements are. What sort of measurements will you be doing? Is automation a big deal? Is accuracy most important? What about warranty/support where you are? etc.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • deoli
    0 deoli over 6 years ago in reply to Gough Lui

    Thanks Gough

    I mainly repair PCB for  drives and general repairs of electronics boards.

    I want fast continuity function and diode testing with buzzer indication "good/fail", fast readings as well.

    Accuracy to 4 decimals not required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 6 years ago in reply to deoli

    Strongly agree with michaelkellett on this one - it sounds like you're probably better served by a handheld meter of some type. The Fluke stuff are bulletproof, but I personally go for Keysight DMMs myself because they tend to have the edge on accuracy at a given price point and I'm quite fond of the connectivity options. That being said, each has their own preferences.

     

    In fact, the main draw of higher-resolution bench meters is to do fine measurements, automate measurements via remote control interfaces, do data logging, etc. In fact, often higher-resolution measurements often mean slower conversion times as well. If you don't even need 5-digits, many premium handheld meters can offer 4 and 4.5-digits easily, at a lower price and with the convenience of being able to take anywhere and troubleshoot on site. As an advantage, they'll also work on a power outage image.

     

    - Gough