Fluke
  • Products & Partners
  • Manufacturers
  • Fluke
  • More
  • Cancel
Fluke
Forum Is there a way of making RS232 communication with fluke 8846a faster?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Fluke to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 17 subscribers
  • Views 636 views
  • Users 0 members are here
Related

Is there a way of making RS232 communication with fluke 8846a faster?

MANVI27
MANVI27 over 2 years ago

I’m using Fluke 8846A for measuring current in a setup where the current range is set to 10A. I’m using MEASure method to read value from Fluke 8846a using RS232 communication at baud rate of 115200 with one stop bit and no parity in remote mode. The time taken from the query to receiving the response is roughly 275ms which is a bit high for my application. I would ideally want it to be less than or equal to 50ms. Is there a way to make this communication faster?
Also I’m trying to synchronize this reading from another source so I want to collect data by single trigger which I think MEASure method provides.

Code snippet used for profiling:

query_msg = "MEAS:volt:dc? 10\r"
ser.write(query_msg)
# Receive data until   
print(time())
received_data = ser.read(17)
print(time())  


Time printed(s) in terminal:
1717717621.2261405
1717717621.5009155

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 2 years ago +3
    The 'Extended Specifications' document has a table (scroll down right at the end) of measurement rates which includes the integration times dam-assets.fluke.com/.../2748044_6200_ENG_B_W_1.PDF It looks…
Parents
  • jc2048
    jc2048 over 2 years ago

    The 'Extended Specifications' document has a table (scroll down right at the end) of measurement rates which includes the integration times

    dam-assets.fluke.com/.../2748044_6200_ENG_B_W_1.PDF

    It looks like you can go faster than you're seeing if you're prepared to accept less resolution.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jc2048
    jc2048 over 2 years ago

    The 'Extended Specifications' document has a table (scroll down right at the end) of measurement rates which includes the integration times

    dam-assets.fluke.com/.../2748044_6200_ENG_B_W_1.PDF

    It looks like you can go faster than you're seeing if you're prepared to accept less resolution.

    • Cancel
    • Vote Up +3 Vote Down