Welcome to the Fluke page on element14. Here you can find things such as our latest news, training videos, and product details. Additionally, you can engage with us in our forums.
The environmental test team at Fluke tries to break new products during development. Here, from this fun-loving, happy-go-luck crew, are their top-ten torture chamber favorites:
10. Let’s drop the packaged product, on all faces and corners - 24 drops - from 1 meter onto a hardwood floor.
When the test team can no longer get a unit to fail, it can be released to production. Why go to all this trouble? So that when you take your Fluke meter into the hazards and hassles of the real world, the last thing you need to worry about is whether your meter still works.
Bio: Rick Pirret recently retired from Fluke following 30 years in product design and marketing. Previously, he was with Bell Labs for 10 years in product and facility design. Rick studied mechanical engineering at Cornell and Stanford, and completed an MBA at Seattle University. Over the years, hobbies have included scuba diving, white water canoeing, flying, motorcycling, and bicycling. More recently, Rick likes to be outdoors in the Cascades Mountains or on-track in a BMW
What is great industrial design? You know it when you see it – art and science, function and feel, color and texture blended in a magical way. The “celebrity” designers often got it right; Henry Dreyfuss in the 1965 Trimline phone, Raymond Loewy in the Air Force One graphics and Harley Earl in the 1953 Corvette.
Fluke has a long history of meticulous industrial design. Del King started it, George McCain carried it forward, and Chris Lagerberg leads the team now. They have given Fluke handhelds a clean, functional look, with a brand image you can spot across the room. Instruments fit the hand right and feel solid. Rotary knobs have a lush, silky feel. Pushbuttons give crisp, tactile feedback. Displays are sharp and readable in a broad range of light conditions. Control layouts are intuitive. Users around the world can pick up a unit and make it work – with gloves on.
Throughout the design process, the goal is to include as many pleasant surprises, or "delight factors" as possible. In its Olympic campaign, BMW claimed "we don't just make cars. We make joy". Fluke shares that spirit, and it’s it is part of the difference you enjoy when you select a Fluke product.
Bio: Rick Pirret recently retired from Fluke following 30 years in product design and marketing. Previously, he was with Bell Labs for 10 years in product and facility design. Rick studied mechanical engineering at Cornell and Stanford, and completed an MBA at Seattle University. Over the years, hobbies have included scuba diving, white water canoeing, flying, motorcycling, and bicycling. More recently, Rick likes to be outdoors in the Cascades Mountains or on-track in a BMW
John Fluke said "the customer should always get more than they thought they paid for". One of those extras is diligence, or in dictionary-speak, "persevering application". Here’s a behind-the-scenes look at the care that goes into a new Fluke product.
Diligence in product definition begins with the "voice of the customer", or VOC. Fluke engineers research not only WHAT users do, but HOW they do it. They try to understand not just the measurement functions and ranges that a task requires, but also the work methods or processes that real people actually use. What should the user interface be? How could that user interface help the customer work faster or work smarter? What would delight this customer? Several iterations of VOC research and planning are necessary to ensure that new products meet customer expectations. Finally, beta testing confirms that the product definition matches original intent.
Diligence in design applies both art and science to resolve the tug-of-war between the constraints on a new instrument. The circuit design needs to deliver the specified measurement performance, but it must also protect against misconnected inputs and inputs above stated limits. The circuit must perform over a wide range of temperature, humidity, and altitude, while being subjected to electromagnetic interference and electrostatic discharge. Now add the constraints that the new meter is expected to be compact, handheld, easy to use, and rugged, and the problem becomes very difficult to solve. Each iteration of a design is tested for durability, safety, and measurement performance. Refinement continues until each test is passed with a substantial margin. Only then is a new design released to production.
Diligence in metrology has two aspects. First, a Fluke spec includes allowance for drift due to time, temperature, and humidity. You can be confident that your meter still performs within spec when it returns for its scheduled calibration. Second, each Fluke meter is adjusted and verified, traceable to recognized international standards, by a branch of the Fluke standards lab that resides within the production cell.
What does all this diligence mean to you? Care in definition, design, and metrology means you can count on your tools to safely deliver a professional result, and that your investment will continue to perform well over a long and useful life.
Bio: Rick Pirret recently retired from Fluke following 30 years in product design and marketing. Previously, he was with Bell Labs for 10 years in product and facility design. Rick studied mechanical engineering at Cornell and Stanford, and completed an MBA at Seattle University. Over the years, hobbies have included scuba diving, white water canoeing, flying, motorcycling, and bicycling. More recently, Rick likes to be outdoors in the Cascades Mountains or on-track in a BMW.
Blog One: Diligence; by Rick PirretIt was a record cold day in Tacoma, and a bright sun could not ease the chill of the light wind that wrapped itself around the dozen tidy homes of Larabee Terrace.
The cold snap provided the first big test of the heating systems, insulation and construction techniques used by the Habitat for Humanity volunteers and low-income homeowners who built these homes. Conditions were ideal for a quick course in thermography and weatherization. It was a great opportunity for Habitat staff members to learn to use their new Fluke TiR1 thermal imager.
Thermographer, and Sr. Product Manager, Michael Stuart had driven down from Fluke headquarters for the orientation. The Washington State University team, representing the Department of Energy Building America program, was there with their blower door setup. A blower door test used in conjunction with some thermal imagers from Fluke in one of the newly-built homes would reveal any gaps in the way they were built and point the way to greater energy efficiency.
The homes at Larabee terrace step down a west-facing hillside in an old Tacoma neighborhood of smaller homes. It's the latest project of Tacoma Pierce County affiliate of Habitat for Humanity International. Habitat works in partnership with people in need to build and renovate decent, affordable housing. The houses then are sold to those in need at no profit and with no interest charged.
Since 1985, Habitat has built more than 162 homes in Pierce County, providing home ownership opportunities to households making 30 percent to 60 percent of the Area Median Income. And the benefits extend beyond the homeowners and their neighborhoods. The volunteers who devote their time to building the homes enjoy the warm feeling of giving back to their community. Each Habitat family must complete 500 hours of "sweat equity" through work on their and other people's homes or other work that helps the Habitat run. Habitat is a partnership that builds houses together with the families who will live in them.
"Our goal is to try and make these homes more energy-efficient and more affordable to live in," said Gomer Roseman, Site Development Director, Tacoma Pierce County affiliate of Habitat for Humanity International. "If we can reduce the utility bill by $25 a month, somebody who earns $25,000 a year would be very happy about it."
Modest in size (averaging 1500 square feet) and affordably priced, the Larabee Terrace homes are built to save energy. Their heating systems, designed by a retired Boeing engineer, get double duty from an on-demand gas water heater used to warm domestic water and provide under-floor radiant heat. Foam exterior sheathing boosts wall insulation from a standard R20 to R30.
"That shows up in the infrared imaging," said Mike Lubliner, Sr. Building Sciences Specialist for the WSU Extension Energy Program. "You don't see the distinct heat loss normally caused by the studs in the walls." As Stuart demonstrated its use, the imager made other construction details and areas for possible future improvement surprisingly easy to see. The infrared scans revealed the normally expected cooler areas where walls and ceilings come together—and were even sensitive enough to see where sheetrock screws were under the paint.
After a quick thermography introduction, the WSU team set up a blower door in a recently completed home. The door-mounted fan drew air from the structure, reducing the interior pressure and pulling in cold outside air through openings visible and unseen.
Though the house performed well, some fixes were needed. In the imager's scan, some electrical outlets in outside walls took on a cooler blue tint where air infiltration was occurring through the electrical chase. In another area, cool "air fingers" lightly streamed from a ceiling fixture -- evidence that cooler air was coming in through the fixture and cooling off her surface of the ceiling around it. A few areas even showed where a little more attention could have been given to the placement of the fiberglass bat insulation in the upper part of some wall cavities. Roseman said the results will help produce a better, more efficient, Habitat house by indicating where improvements can easily and inexpensively be made during the construction process and afterward.
"Everything that we've seen as a result of this test indicates something we could be doing differently that would give us a better result," said Roseman. "What we've learned today is that we need to provide better sealing around our electrical penetrations in the walls, and we need to pay more attention to the connection at the top plate. Those are things we're going to work on now and try and build a tighter house.
"If we can build a better house for the same price, and it results in a saving for the owner, we've accomplished something. Tools like this allow us to see the hidden movement of air, things that aren't visible to the naked eye—things that enable us to do a better job without spending a lot of money."
According to Lubliner, infrared testing could be even more productive as Habitat moves into rehabilitating existing homes, built without the energy-conscious techniques of today. "I believe there will be more and more focus on existing homes," he said. "I think the infrared technology and blower door technology will get us more low-hanging fruit in the existing sector than they will in new homes."
In this issue of FIXIT - Fluke Nation:
Thought for the month
Like many of you, we're still waiting for an economic recovery to really kick in. But are those mythical "green shoots" starting to show? One leading economist (we'll tell you who) is predicting an upturn in residential construction-and when's the last time you heard that?
More in this issue:
By Bennie Kennedy, Instructor, Curriculum Developer Prairie State College
| ||||||
|