Intel
  • Products & Partners
  • Manufacturers
  • Intel
  • More
  • Cancel
Intel
Blog CapperLabs Greenhouse Controller - Blog 2 - System Components
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Intel to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rsc
  • Date Created: 9 Jan 2017 6:59 PM Date Created
  • Views 712 views
  • Likes 3 likes
  • Comments 1 comment
  • capperlabs
  • greenhouse
  • intel_project
  • intel edison
Related
Recommended

CapperLabs Greenhouse Controller - Blog 2 - System Components

rsc
rsc
9 Jan 2017
CapperLabs Greenhouse Controller Table of Contents
Blog 1 Introduction
Blog 2 System Components
Blog 3 Intel Edison
Blog 4 Grove-y
Blog 5 Round and Round
Blog 6 Automatic Vent

1) The Greenhouse:

     The greenhouse is a Palram Harmony 6ft x 8ft model with one door and one window vent.  The vent came with a manual linkage for opening and an automatic lifter that opens with temperature changes.  The vent is one of the items that needs to be controlled with the Intel Edison board.

image

2) Environmental Temperature Control:

    The temperature of the greenhouse is currently controlled by either opening the vent for cooling, or turning on an electric portable space heater.

image

The space heater has some problems keeping the room at a specific temperature, so I plan to bypass its internal control and use a feedback system using the Edison board.

Sometimes just opening the vent won't cool the room down enough either, so fans or other cooling will also be required.

On the hottest days last summer, I had to put a tarp on the roof to keep the room cool.

 

3) Watering:

  The current watering system is simple:

image

The house water will be piped into the greenhouse if I can find a way to keep the pipe from freezing, and a sprinkler system will be installed.

 

4) Security:

The current security system is a Samsung IP webcam.  Door interlock and motion detection will be added.

image

5) Sensors:

Outdoor and Indoor Temperature and Humidity are currently being monitored using an AcuRite weather station.  Soil temperature and moisture level sensors will be added.

  • Sign in to reply
  • CharlesGantt
    CharlesGantt over 9 years ago

    Can't wait to see this get started!