Microchip
  • Products
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum Need technical help from Microchip? Ask our Expert!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 112 replies
  • Subscribers 31 subscribers
  • Views 11226 views
  • Users 0 members are here
  • help
  • microchip
  • expert
  • mike_mcglade
  • questions
Related

Need technical help from Microchip? Ask our Expert!

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

MikeMcGlade

Mike McGlade

Mike has 16 years of experience with Microchip products including MCU, Memory & Analog.  He also has significant knowledge of lighting, safety & security and vending industries.

 


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Mike

     

    I am using the AR1010 resistive touch screen controller. I have constructed the circuit and in order to test if my circuit is working I have sent some commands to the controller via serial comms. However, if i send the following command " 55 01 12", which is to enable touch, I get the following response from the controller: "55 BF 5F 31 00". The response i was expecting was "55 02 response 12", this was given in the datasheet. in fact any command i send, the response is different to what the datasheet says it should be. Also if i send the disable touch command then the serial still receives data when the screen is touched.Please all the help will be appreciated. Could it be that the parity settings and stop bit settings are not correct as this information is not in the datasheet, only baud rate is given.

     

    Regards, Kippie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Mike

     

    I am using the AR1010 resistive touch screen controller. I have constructed the circuit and in order to test if my circuit is working I have sent some commands to the controller via serial comms. However, if i send the following command " 55 01 12", which is to enable touch, I get the following response from the controller: "55 BF 5F 31 00". The response i was expecting was "55 02 response 12", this was given in the datasheet. in fact any command i send, the response is different to what the datasheet says it should be. Also if i send the disable touch command then the serial still receives data when the screen is touched.Please all the help will be appreciated. Could it be that the parity settings and stop bit settings are not correct as this information is not in the datasheet, only baud rate is given.

     

    Regards, Kippie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • MicrochipRTCfr
    MicrochipRTCfr over 14 years ago in reply to e14 Contributor

    Hi Kippie,

     

    For such detailed question, I suggest you access on-line technical support : http://support.microchip.com

     

    Regards