Microchip
  • Products
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum Need technical help from Microchip? Ask our Expert!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 112 replies
  • Subscribers 31 subscribers
  • Views 11175 views
  • Users 0 members are here
  • help
  • microchip
  • expert
  • mike_mcglade
  • questions
Related

Need technical help from Microchip? Ask our Expert!

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

MikeMcGlade

Mike McGlade

Mike has 16 years of experience with Microchip products including MCU, Memory & Analog.  He also has significant knowledge of lighting, safety & security and vending industries.

 


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi, I'm looking for a MCU with board like TI MSP-EXP430F5438..MSP-EXP430F5438.. but the problem with this generation is that cannot support direct USB transfer and power. So, I know that MSP430F55XX is a nice product for USB. But, I cannot find a board to put it and program it in C Language to do the job I need. I use it to receive IR Led Receiver information and calculate  the exact position of a finger on a table. 2 adjacent side have IR Led receiver and 2 others adjacent sides have ID Led emitter.

     

    Thanks you to help me to find a product with fast cpu, low energy consumption and USB transfer.

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to e14 Contributor

    Hi,

     

    There are several 16 bits USB microcontrollers in the PIC24F family which you can find here : http://www.microchip.com/USB

    The largest one is the PIC24FJ256GB210 but the PIC24FJ256GB110-I/PT.PIC24FJ256GB110-I/PT. is also an option

    Of course there are smaller device which also have a smaller power consumption.

     

    Regarding tools you can use the EXPLORER16 board + the adequate processor module (PIM) + USB PICTAIL plus board

     

    A pickit3 (or better), an  ICD3 will be needed to debug / program. The C30 compiler and the MPLAB IDE can be downloaded free of charge.

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to e14 Contributor

    Hi,

     

    There are several 16 bits USB microcontrollers in the PIC24F family which you can find here : http://www.microchip.com/USB

    The largest one is the PIC24FJ256GB210 but the PIC24FJ256GB110-I/PT.PIC24FJ256GB110-I/PT. is also an option

    Of course there are smaller device which also have a smaller power consumption.

     

    Regarding tools you can use the EXPLORER16 board + the adequate processor module (PIM) + USB PICTAIL plus board

     

    A pickit3 (or better), an  ICD3 will be needed to debug / program. The C30 compiler and the MPLAB IDE can be downloaded free of charge.

     

    regards