Microchip
  • Products
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum Need technical help from Microchip? Ask our Expert!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 112 replies
  • Subscribers 31 subscribers
  • Views 11182 views
  • Users 0 members are here
  • help
  • microchip
  • expert
  • mike_mcglade
  • questions
Related

Need technical help from Microchip? Ask our Expert!

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

MikeMcGlade

Mike McGlade

Mike has 16 years of experience with Microchip products including MCU, Memory & Analog.  He also has significant knowledge of lighting, safety & security and vending industries.

 


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello,  I hoping I can get a solution to my problem.

     

    I'm using a PIC24FJ256GB210 for a project , Developing on a Explorer 16 Board.

     

    The Code I'm Using is Bellow.

    (ConfigPins(); Just Handles The Mapping of the OC1-OC4 to the Pins)

     

    #define USE_AND_OR    

    #include <p24FJ256GB210.h> 

    #include <timer.h>

    #include <outcompare.h>

    #include "PinConfig.h"

     

    _CONFIG1( JTAGEN_OFF & GCP_OFF & GWRP_OFF & FWDTEN_OFF & ICS_PGx2) 

    _CONFIG2( FCKSM_CSDCMD & OSCIOFNC_OFF & POSCMOD_XT & FNOSC_PRI) 

     

    void __attribute__ ((interrupt,no_auto_psv)) _T3Interrupt( void) {LATA = PORTA ^ 0x0001;T3_Clear_Intr_Status_Bit;} 

     

    int main() 

    { 

    ConfigPins();

     

    OpenTimer3(T3_ON|T3_PS_1_8|T3_SOURCE_INT, 399);

    ConfigIntTimer3(T3_INT_ON|T3_INT_PRIOR_1);      

     

    OpenOC4(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_TMR3, 0, 0);

    OpenOC3(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_TMR3, 10, 0);

    OpenOC2(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_TMR3, 399, 0);

    OpenOC1(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_TMR3, 400, 0);

    while(1);

    }

    now when I run the above code (with required changes for a P24FJ128GA010) I get the Correct PWM Outputs of Low / 10 Cycles / 399 / High
    But on the P24FJ256GB210, Only OC1 Is Running.
    now If I change the OpenOCn Code to
    OpenOC4(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_TMR3, 0, 0);
    OpenOC3(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_OC4, 10, 0);
    OpenOC2(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_OC3, 399, 0);
    OpenOC1(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_OC2, 400, 0);
    [/qiote]
    I Get a PWM Output on all 4 Channels, with Problems
    Problems
    1) If I set the OC4RS value to 0 (OFF)  I get a Sig that is equivilent to the Timer3 Cycle (On / Off)
    2) If I set the OC4RS value to 400 (Fully On) OC4 Will Go High, But OC1-OC3 Go Low with No Signal Output.
    3) Any OCnRS Value that is set to 0(OFF) I still get a signal out in sync with Timer3.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello,  I hoping I can get a solution to my problem.

     

    I'm using a PIC24FJ256GB210 for a project , Developing on a Explorer 16 Board.

     

    The Code I'm Using is Bellow.

    (ConfigPins(); Just Handles The Mapping of the OC1-OC4 to the Pins)

     

    #define USE_AND_OR    

    #include <p24FJ256GB210.h> 

    #include <timer.h>

    #include <outcompare.h>

    #include "PinConfig.h"

     

    _CONFIG1( JTAGEN_OFF & GCP_OFF & GWRP_OFF & FWDTEN_OFF & ICS_PGx2) 

    _CONFIG2( FCKSM_CSDCMD & OSCIOFNC_OFF & POSCMOD_XT & FNOSC_PRI) 

     

    void __attribute__ ((interrupt,no_auto_psv)) _T3Interrupt( void) {LATA = PORTA ^ 0x0001;T3_Clear_Intr_Status_Bit;} 

     

    int main() 

    { 

    ConfigPins();

     

    OpenTimer3(T3_ON|T3_PS_1_8|T3_SOURCE_INT, 399);

    ConfigIntTimer3(T3_INT_ON|T3_INT_PRIOR_1);      

     

    OpenOC4(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_TMR3, 0, 0);

    OpenOC3(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_TMR3, 10, 0);

    OpenOC2(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_TMR3, 399, 0);

    OpenOC1(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_TMR3, 400, 0);

    while(1);

    }

    now when I run the above code (with required changes for a P24FJ128GA010) I get the Correct PWM Outputs of Low / 10 Cycles / 399 / High
    But on the P24FJ256GB210, Only OC1 Is Running.
    now If I change the OpenOCn Code to
    OpenOC4(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_TMR3, 0, 0);
    OpenOC3(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_OC4, 10, 0);
    OpenOC2(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_OC3, 399, 0);
    OpenOC1(OC_TIMER3_SRC|OC_PWM_CENTRE_ALIGN,OC_SYNC_TRIG_IN_OC2, 400, 0);
    [/qiote]
    I Get a PWM Output on all 4 Channels, with Problems
    Problems
    1) If I set the OC4RS value to 0 (OFF)  I get a Sig that is equivilent to the Timer3 Cycle (On / Off)
    2) If I set the OC4RS value to 400 (Fully On) OC4 Will Go High, But OC1-OC3 Go Low with No Signal Output.
    3) Any OCnRS Value that is set to 0(OFF) I still get a signal out in sync with Timer3.