Microchip
  • Products
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum Need technical help from Microchip? Ask our Expert!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 112 replies
  • Subscribers 31 subscribers
  • Views 11211 views
  • Users 0 members are here
  • help
  • microchip
  • expert
  • mike_mcglade
  • questions
Related

Need technical help from Microchip? Ask our Expert!

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

MikeMcGlade

Mike McGlade

Mike has 16 years of experience with Microchip products including MCU, Memory & Analog.  He also has significant knowledge of lighting, safety & security and vending industries.

 


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi mike

     

    I was wondering if this explorer board below is similar

    http://sg.element14.com/microchip/dm240001/kit-picdem-pic24-dspic33-explorer/dp/1146554

     

    http://sg.element14.com/microchip/dm240002/kit-dev-explorer-16-44-pin-board/dp/1754668

     

    Thanks

     

    regards

    calvin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to e14 Contributor

    Hi Calvin,

     

    The links you've given are in fact 2 slightly different products.

     

    Both of these products include the same board (EXPLORER16) but the processor modules which are bundled are different.

    One product includes 2 x 16 bits (100 pin products) and the other include 1 or 2 x 16 bits (44 pin products).

    I recommend you the first one if you need lots of I/Os.

     

    You can buy at anytime additional processor modules called "PIMS" to use up to 30 different processors including PIC32 ;=)

     

    Additionally you can add PICTAIL plus expansion boards to EXPLORER16 to add connectivity (USB, WiFi, ethernet, CAN, AUDIO,...)

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to e14 Contributor

    Hi Calvin,

     

    The links you've given are in fact 2 slightly different products.

     

    Both of these products include the same board (EXPLORER16) but the processor modules which are bundled are different.

    One product includes 2 x 16 bits (100 pin products) and the other include 1 or 2 x 16 bits (44 pin products).

    I recommend you the first one if you need lots of I/Os.

     

    You can buy at anytime additional processor modules called "PIMS" to use up to 30 different processors including PIC32 ;=)

     

    Additionally you can add PICTAIL plus expansion boards to EXPLORER16 to add connectivity (USB, WiFi, ethernet, CAN, AUDIO,...)

     

    regards