Microchip
  • Products
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum Need technical help from Microchip? Ask our Expert!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 112 replies
  • Subscribers 31 subscribers
  • Views 11163 views
  • Users 0 members are here
  • help
  • microchip
  • expert
  • mike_mcglade
  • questions
Related

Need technical help from Microchip? Ask our Expert!

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

MikeMcGlade

Mike McGlade

Mike has 16 years of experience with Microchip products including MCU, Memory & Analog.  He also has significant knowledge of lighting, safety & security and vending industries.

 


  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi Mike,

     

    Is the F1 kit suppose to consist of 16F1937, XLP version ? Because my customer saw the below note in his kit.
    ATTENTION: This version of the F1 evaluation platform is populated with non-XLP PIC 16F1937.
    Pls advise. Thanks!
    Regards
    Kevin
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 16 years ago

    Hi Mike,

     

    Hope you are doing well.

     

    I was wondering about running MPLAB in Linux. I have both a Pickit 2 and a Pickit 3 and I was wondering if it is possible use them to program my projects while running MPLAB in Ubuntu 10.04.

     

    Does Microchip have any plans to port MPLAB to linux?

     

    Any suggestions on how I could make things work without having to resort to a Windows setup would be appreciated.

     

    Best Regards,

    Jorge Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 16 years ago in reply to Jorge_Garcia

    Hi Jorge,

     

    You may want to read this thread about your question.


    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to Jorge_Garcia
    Jorge ,  we have no immediate plans to release a version of MPLAB that runs under Linux - but it's under discussion - please keep asking the question though . Regards , Mike
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago
    hello

    i m have a  big probleme with a DSPIC30F4011
    we delopped an electronic ignition for VHC car

    i m have no response in the web and i m need to finisch this project before tomorow
    could you help us

    we make more test

    and is the pic who lost the signal in OC1 and put all impuls in OC3

    if we put out the coil who was connected at OC3 we refined the good signal on the two OC
    if we deconecte the  coil attached to OC1 we have change in OC3

    we have 1 optocoupleur and 3 darlington transistor to isolate the pic from the "bobine"
    Attachments:
    2816.schéma.DSN.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Vincent , please provide me with the Microchip Support Webticket Number and I will try and get help for you .

     

    Regards , Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    the number of the webticket was 1-182702

     

    best regards

     

    vincent

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi,

     

    We're developing a new circuit to control ignition and flame of the water heater burner. that means MCUs' software has to fulfil 60730 Class C safety software requirements.

     

    We're using

    - PIC16F946 as Safety controller and SPI communication master.

    - PIC16F77 as Safety monitor/supervisor and SPI communication slave.

     

    both MCUs share information about the safety field sensors and its own status in order to shut down gas valve case of any default detection or misunderstood between MCUs

     

    In order to warrant reliability and safety in communication and to avoid collisions, some "guru"s propose to add a signal from the slave to the master MCU to notify when it is ready to send/receive a 8- bit-packet.

     

    Do you agree that solution? any other proposal?

     

    Does Anyone know bibliography about this topic?

     

    Thanks in advance....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hİ,

     

    I want to buy OLIMEX STM-P103 development board on farnell. And study on arm microproseccor.

     

    Can I use KEİL uvision4 C Compailer with this product. Can I programming the MCU via this software?

     

    Have a nice day...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • samplerman
    samplerman over 16 years ago in reply to e14 Contributor

    HI Yusuf

    I have asked  Keil about this device, their respones was:

    yes MDK-ARM does support the device:
    http://www.keil.com/dd/chip/4231.htm
    Thanks
    Carl
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>