Microchip
  • Products
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum Need technical help from Microchip? Ask our Expert!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 112 replies
  • Subscribers 31 subscribers
  • Views 11174 views
  • Users 0 members are here
  • help
  • microchip
  • expert
  • mike_mcglade
  • questions
Related

Need technical help from Microchip? Ask our Expert!

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

MikeMcGlade

Mike McGlade

Mike has 16 years of experience with Microchip products including MCU, Memory & Analog.  He also has significant knowledge of lighting, safety & security and vending industries.

 


  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi, have you any clues as to where to get the pic18f24j50.lkr  linker file for the Microchip C18 complier. It's not included in the lkr directory although it's listed as supported. In fact almost none of the 18F usb devices are apart from the 64 pin and up. I can't contact microchip support via their centre as it keep throwing out my password and wont send me a new one. Stupid really as we are a Microchip Design Partner but I just can't find this file ANYWHERE. Last resort will be to talk directly to Microchip if I can.  I have downloaded and installed the very latest version of the compiler.

     

    Regards

     

    Ron Ashby, Director of Engineering, Synatel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Ron , I have a colleague who handles design partners in the UK - let me ask him to contact you . FYI I've had the same issue with getting new passwords out of our Support System !!!

     

    Regards , Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 16 years ago in reply to e14 Contributor

    Hi Ron,

     

    I'm not sure which compiler version of the C18 you use. Latest can be downloaded here : http://www.microchip.com/C18.

     

    The file you're looking for seem to relate to an old C18 version.

     

    For the current C18, the linker files are located here :    C:\MCC18\bin\LKR\  (assuming you let C18 install in the root)

     

    Nowadays, there's only one generic file used for both Debug\Program modes : 18f24j50_g.lkr

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi, I'm looking for a MCU with board like TI MSP-EXP430F5438..MSP-EXP430F5438.. but the problem with this generation is that cannot support direct USB transfer and power. So, I know that MSP430F55XX is a nice product for USB. But, I cannot find a board to put it and program it in C Language to do the job I need. I use it to receive IR Led Receiver information and calculate  the exact position of a finger on a table. 2 adjacent side have IR Led receiver and 2 others adjacent sides have ID Led emitter.

     

    Thanks you to help me to find a product with fast cpu, low energy consumption and USB transfer.

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to e14 Contributor

    Hi,

     

    There are several 16 bits USB microcontrollers in the PIC24F family which you can find here : http://www.microchip.com/USB

    The largest one is the PIC24FJ256GB210 but the PIC24FJ256GB110-I/PT.PIC24FJ256GB110-I/PT. is also an option

    Of course there are smaller device which also have a smaller power consumption.

     

    Regarding tools you can use the EXPLORER16 board + the adequate processor module (PIM) + USB PICTAIL plus board

     

    A pickit3 (or better), an  ICD3 will be needed to debug / program. The C30 compiler and the MPLAB IDE can be downloaded free of charge.

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    bonjour,

     

    j'utilise un DSPIC30F3013-30I/SODSPIC30F3013-30I/SO

    j'ai un problème avec la programmation de la memoire eeprom

    je relis bien les position mais je n'arrive pas a effacer le contenu , ni à le programmer

    y a t'il un vérouillage quelconque qui existe?

    voici le code que j'utilise, ou y at'il un bug?

     

      mov  #tblpage(posit_P1),w0
      mov  w0,NVMADRU
      mov  #tbloffset(posit_P1),w0
      mov   w0,NVMADR
      call CEEPROM
      MOV  #tblpage(posit_P1),W0
      MOV  W0,TBLPAG
      MOV  #tbloffset(posit_P1),W0
      call EEEPROM

    ;..............................................................................
    ; sous programme efface eeprom
    ;..............................................................................

    CEEPROM:
      ; Setup NVMCON to erase one word of data EEPROM
      mov  #0x4044,w0
      MOV  w0,NVMCON
      ; Disable interrupts while the KEY sequence is written
      PUSH  SR
      MOV  #0x00E0,W0
      IOR  SR
      ; Write the KEY sequence
      MOV  #0x55,W0
      MOV  W0,NVMKEY
      MOV  #0xAA,W0
      MOV  W0,NVMKEY
      nop
      nop
      ; Start the erase cycle
      BSET  NVMCON,#WR
      nop
      nop
    CEE1:
      ; attente fin ecriture
      btsc    NVMCON,#WR
      goto    CEE1  ; Re-enable interrupts
      POP  SR
      return

    ;..............................................................................
    ; sous programme ecrit eeprom
    ;..............................................................................

    EEEPROM:
      ; Write data value to holding latch
      TBLWTL  W2,[ W0]
      ; NVMADR captures write address from the TBLWTL instruction.
      ; Setup NVMCON for programming one word to data EEPROM
      MOV  #0x4004,W0
      MOV  W0,NVMCON
      ; Disable interrupts while the KEY sequence is written
      PUSH  SR
      MOV  #0x00E0,W0
      IOR  SR
      ; Write the key sequence
      MOV  #0x55,W0
      MOV  W0,NVMKEY
      MOV  #0xAA,W0
      MOV  W0,NVMKEY
      nop
      nop
      ; Start the write cycle
      BSET  NVMCON,#WR
      nop
      nop
    EEE1:
      ; attente fin ecriture
      btsc    NVMCON,#WR
      goto    EEE1
      ;Re-enable interrupts, if needed
      POP  SR
      return

     

    merci pour votre aide

     

    Gérard Micoud

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to e14 Contributor

    Bonjour,

     

    Je vous recommande de suivre la procédure décrite dans la datasheet du dsPIC30F3013.

    Il existe aussi un exemple en langage C : CE017

     

    N'oubliez pas de consulter le manuel dédié à chaque périphérique pour toute la famille dsPIC30 . Dans le cas de la mémoire E2PROM il s'agit de la section 05 que vous trouverez sur cette page, ainsi que des notes d'application.

     

    Vous pouvez vous faire aider par la communauté des utilisateurs Microchip, qui possède un forum dédié aux dsPIC : http://forum.microchip.com

     

    Des formations sur les dsPIC sont proposées tout au long de l'année dans notre centre de formation français : http://www.microchip.com/RTC

     

    Ci-joint le catalogue de nos formations

     

    Salutations

    Attachments:
    imageMicrochip_catalogue_formations_Q3B_2010_100812.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to MicrochipRTCfr

    merci pour votre réponse,

     

    j'applique bien la procedure donnée dans le datasheet . j'ai communiqué mon code dans le précedent message.

    le problème est que la memoire n'est pas écrite et qu'aucune erreur n'est générée

    je dois dire que je bute, alors que j'utilise depuis assez longtemps ce type de dspic!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi, Mike.  We are about to develop a USB connected data logging system with four channels.

    The device needs to fit into a mini package, preferably ca. keyfob size and powered from the USB port.

     

    There a a few Microchip products we have looked at but nothing entirely suitable.

     

    Can you suggest best chips to use, please?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi Peter , I probably need to know a little bit more about your application , is the logger permanently tethered to the PC/ Master or does it have it's own battery for when untethered , what are you using for memory to store the logged data - or does it smply get passed to the PC. What sort of ADC do you need ? We've recently released a host of new larger memory USB MCUs - you should see them in our 2nd Half Focus Products Guide .

    If the logger has it's own lithium cell - we offer USB charge ICs too.

     

    Regards , Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>