Microchip
  • Products
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum Need technical help from Microchip? Ask our Expert!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 112 replies
  • Subscribers 31 subscribers
  • Views 11219 views
  • Users 0 members are here
  • help
  • microchip
  • expert
  • mike_mcglade
  • questions
Related

Need technical help from Microchip? Ask our Expert!

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

MikeMcGlade

Mike McGlade

Mike has 16 years of experience with Microchip products including MCU, Memory & Analog.  He also has significant knowledge of lighting, safety & security and vending industries.

 


  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Mike

     

    I am using the AR1010 resistive touch screen controller. I have constructed the circuit and in order to test if my circuit is working I have sent some commands to the controller via serial comms. However, if i send the following command " 55 01 12", which is to enable touch, I get the following response from the controller: "55 BF 5F 31 00". The response i was expecting was "55 02 response 12", this was given in the datasheet. in fact any command i send, the response is different to what the datasheet says it should be. Also if i send the disable touch command then the serial still receives data when the screen is touched.Please all the help will be appreciated. Could it be that the parity settings and stop bit settings are not correct as this information is not in the datasheet, only baud rate is given.

     

    Regards, Kippie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 14 years ago in reply to e14 Contributor

    Hi Kippie,

     

    For such detailed question, I suggest you access on-line technical support : http://support.microchip.com

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Bonjour, Je viens de recevoir un module ethernet equipé d'un pic 18f67j60 concus par elektor (' http://www.elektor.fr/100552 '). Malheuresement je ne reussis par à mettre en oeuvre ce module qui sert de server web pour une petite page html. Je ne comprend pas comment dialoguer avec le pic et si deja le projet et compilet sur le pic. Je n'ai aucune information supplémentaire de livré et de même que sur leur page dédie au projet. J'aimerai savoir si il me faut un tool de dev (pickit ou icd3 voir real ice) pour que je puisse faire mon developpement.

    Merci d'avance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 14 years ago in reply to e14 Contributor

    Bonjour,

     

    Si votre module vient d'Elektor il serait plus simple de s'adresser à eux concernant la documentation.

    Pour ce qui concerne les outils de programmation, si Elektor a prévu un port ICSP, cela signifie qu'il est possible de reprogrammer la carte à la condition que vous ayez tous les fichiers sources.

     

    Vous pouvez vous inspirer de la pile de protocole TCP/IP de Microchip et des projets (webserveur,...) téléchargeables gratuitement ici : http://www.microchip.com/MAL

     

    Le choix de l'outil dépend de votre budget et de votre objectif. Pour les particuliers, un Pickit3 est suffisant. Pour une société préferrer un ICD3 beaucoup plus robuste et plus rapide. Le real-Ice n'a du sens que pour les 16 et 32 bits (PIC24/dsPIC et PIC32).

     

    Une formation dédiée ( COM4201 ) à la fonction webserveur de la pile de protocole TCP/IP est proposée régulièrement au centre de formation de Microchip France.

    Les sessions prévues sont visibles ici : http://www.microchip.com/RTC   La prochaine session (non encore planifiée aura probablement lieu en janvier 2012. Pour tout renseignement adressez-vous à Microchip France et demandez le responsable formation.

     

    Salutations

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to MicrochipRTCfr

    Merci pour vôtre réponse rapide. Je vais opter pour un ICD3 et puis une formation pour le début de l'an prochain aussi.

    Je n'hesiterais pas à vous redemander vôs conseils.

    Merci encore.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    hello
    i am designing a home automation system .
    the system will be simple . it will just use a remote control to switch on and swich off  devices(maximum of 64) of a house.
    it is first project of my life .
    please guide me .
    thanks i advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    hello
    i am designing a home automation system .
    the system will be simple . it will just use a remote control to switch on and swich off  devices(maximum of 64) of a house.
    it is first project of my life .
    please guide me .
    thanks i advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 14 years ago in reply to e14 Contributor

    Hi,

     

    Thanks for your request.

    Your specification can be fulfilled with multiple circuits.

    Do you have microcontroller experience ?

    If yes, I would recommend that you look at the brand new single-chip transmitter able to operate in the 434 or 868MHz bands : PIC12LF1840T48

     

    This device had extremely low operating & standby currents and can operate from a 3.0V battery.

     

    If you are looking for bidirectional communication, then I suggest you look at MiWi protocole : http://www.microchip.com/MiWi

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to MicrochipRTCfr

    thank you very much.
    i have doubt about which type of remote contol (RF or IR) should be used to give good value of money?
    remote will have around 20  keys and should have range of 10 metres.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    hi, I want to design a pedometer project using PIC18F4520-E/PPIC18F4520-E/P, can you suggest the most appropriate Sensor to detect steps taken by user and to convert into calories..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>