• Products and Partners
    Products and Partners
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
Microchip
  • Products and Partners
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum PIC18 USB mass storage
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 25 subscribers
  • Views 502 views
  • Users 0 members are here
Related

PIC18 USB mass storage

e14 Contributor
e14 Contributor over 15 years ago

Hi,

 

I'm using PIC18F46J50 in mass storage volume application and i've a problem when i use it with MAC computers. I need only 4ko for my application, but when i connect my µC to a MAC, it create some hidden files into my volume, and it make it full, so i can't add or modify my file.

How i can stop this effect?

 

Thank you

  • Sign in to reply
  • Cancel
Parents
  • KennyMillar
    KennyMillar over 15 years ago

    Well, this is a Mac question and not a PIC question because it happens to every removable storage device you place in a Mac.

    The solution is to create a zero length file called ".metadata_never_index" (Without the quotes, but with the leading dot).

     

    This will prevent the Mac from creating spotlight indexes on the device. I'm pretty sure it'll be the spotlight index which is taking up your space.

     

    I hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • KennyMillar
    KennyMillar over 15 years ago

    Well, this is a Mac question and not a PIC question because it happens to every removable storage device you place in a Mac.

    The solution is to create a zero length file called ".metadata_never_index" (Without the quotes, but with the leading dot).

     

    This will prevent the Mac from creating spotlight indexes on the device. I'm pretty sure it'll be the spotlight index which is taking up your space.

     

    I hope this helps.