• Products and Partners
    Products and Partners
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
Microchip
  • Products and Partners
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Documents PRESS RELEASE - Microchip - 8-pin Microcontroller Features 3.5 kB Self-Programmable Flash Memory
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rwang
  • Date Created: 28 Jan 2010 2:53 AM Date Created
  • Last Updated Last Updated: 27 Oct 2013 5:21 AM
  • Views 519 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

PRESS RELEASE - Microchip - 8-pin Microcontroller Features 3.5 kB Self-Programmable Flash Memory

MCU Enables Higher-Performing Designs in a Variety of Applications

image

CHANDLER, Ariz., Jan. 25, 2010 [NASDAQ: MCHP] — Microchip Technology Inc., a leading provider of microcontroller and analog semiconductors, today announced a new member of its popular 8- and 14-pin PIC16F61X 8-bit PICRegistered microcontroller (MCU) family, targeting cost-effective general-purpose applications. The PIC12F617 MCU features 3.5 kB of self-programmable Flash program memory, and peripherals such as a 10-bit Analog-to-Digital Converter (ADC), comparator, Pulse-Width Modulator (PWM) and VREF for closed-loop-control applications—all in a miniature 3 mm x 3 mm DFN package. The new MCU provides an excellent migration path for customers using previous-generation 8-pin PIC MCUs who wish to upgrade to a larger-memory, more peripheral-rich MCU for future designs. This product is well-suited for a variety of general-purpose applications in the consumer, appliance, industrial, medical and other markets.

 

 

Block Diagram available through editorial contact or Flickr (feel free to publish):

 

http://www.microchip.com/get/R93Rimage

 

The PIC12F617 MCU provides 3.5 kB of Flash programmable memory with a self read-write capability. This serves as a low-cost alternative to data EEPROM and is useful when an application requires remote updates, or the ability to store system data or look-up tables. The microcontroller features an 8 MHz internal oscillator, an on-chip 4-channel 10-bit ADC, a comparator with hysteresis and a PWM with complementary outputs that provide a framework for applications such as LED lighting control, motor control, capacitive touch keys and system monitors. Along with this new product introduction, Microchip also announced a price reduction on the rest of the PIC16F61X family members, including the PIC12F609, PIC12F615, PIC16F610, PIC16F616 MCUs, and their corresponding high-voltage variants.

 

“Engineers often want to add more features and functionality to their design without having to drastically alter their design,” said Steve Drehobl, vice president of Microchip’s Security, Microcontroller and Technology Development Division. “The PIC12F617 MCU provides engineers with more features, such as self-programmable Flash, while maintaining pin compatibility with Microchip’s more than 20 other 8-pin PIC12 MCUs.”

 

Development Tool Support

 

Microchip’s complete suite of standard development tools can be used with the PIC12F617 MCU, including the user-friendly and free MPLABRegistered IDE, along with the HI-TECH CRegistered compiler for PIC12 MCUs. The HI-TECH Lite edition is a completely free, fully-functional compiler with no time limitations.  For applications with limited program space, the Standard and PRO editions offer denser code and improved performance.  Additionally, there is a variety of debugging hardware, from the popular PICkitTm 3 In-Circuit Debugger/Programmer ($44.95), to the MPLAB ICD 3 In-Circuit Debugger, ($219.99), MPLAB PM3 Universal Device Programmer ($895) and MPLAB REAL ICETm In-Circuit Emulator ($495.00). The MPLAB ICD 8- and 14-pin Debugging Header (part # AC162083, $35) is required for debugging the PIC16F616 and PIC12F617 devices. All of these tools can be purchased today at microchipDIRECT (http://www.microchip.com/get/563P). More information on Microchip development tools is available at http://www.microchip.com/get/KWWH.

 

Packaging, Pricing & Availability

 

The new PIC12F617 MCU is available in 8-pin PDIP, SOIC, MSOP and 3 mm x 3 mm DFN packages, starting at $0.56 each, in 10,000-unit quantities. The PIC12F609-I/MSPIC12F609-I/MS and PIC12F615 MCUs are available in 8-pin SOIC packages, for $0.49 and $0.52 each, respectively, in 10,000-unit quantities. The PIC16F610 and PIC16F616 MCUs are available in 14-pin SOIC packages, for $0.56 and $0.65 each, respectively, in 10,000-unit quantities.

Samples of all of the MCUs can be ordered today, at http://www.microchip.com/get/26LF. The devices can be purchased today at microchipDIRECT (http://www.microchip.com/get/563P). For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s Web site at http://www.microchip.com/get/9X5D.

 

About Microchip Technology

 

Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller and analog semiconductors, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/9X5D.

 

Note: The Microchip name and logo, HI-TECH C, MPLAB, and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A., and other countries. PICkit and REAL ICE are trademarks of Microchip Technology Inc. in the U.S.A., and other countries. All other trademarks mentioned herein are the property of their respective companies.

 

Photo and Block Diagram available through editorial contact or Flickr (feel free to publish):

 

Block Diagram

 

http://www.microchip.com/get/R93R

 

Photo

 

http://www.microchip.com/get/KLKT

 

Tags / Keywords: 8-bit, Microchip, PIC, MCHP, microcontroller, MCU, MPLAB, PICkit, ICD 3, general purpose, semiconductor, self read/write Flash program memory, closed-loop control, self programmable

 

RSS Feed for Microchip Product News:

 

http://www.microchip.com/get/CX50

  • pt;microcontroller
  • tc:embedded
  • sp:microchip
  • at:press_release