Molex
  • Products & Partners
  • Manufacturers
  • Molex
  • More
  • Cancel
Molex
Blog 3D Medical Device Design—Efficiency and Simplicity Using Flexible Print Circuit Technology
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Molex to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: MolexConnectors
  • Date Created: 17 Mar 2015 3:17 PM Date Created
  • Views 12887 views
  • Likes 1 like
  • Comments 1 comment
  • connectors
  • molex
  • devices
  • copper
  • flex
  • medical
Related
Recommended

3D Medical Device Design—Efficiency and Simplicity Using Flexible Print Circuit Technology

MolexConnectors
MolexConnectors
17 Mar 2015

As global healthcare needs soar, demand is on the rise for mobile monitoring, therapeutic, and diagnostic devices.  Medical devices have gone from bulky to portable to handheld to the latest wearable technologies for health conscious consumers.  Manufacturers are sellingtoincreasingly tech-savvy clinicians and patients accustomed to using a myriad of portable and handheld electronic devices in their daily lives.  Devices such as smart phones have set high consumer expectations for powerful features in small form factor medical devices.

Incredible shrinking medical devices require circuitry within tight space and weight parameters, and fast heat dissipation with increased airflow.  Anybody who ever packed a suitcase or organized a cluttered closet knows firsthand that the ability of contents to bend or flex is essential to maximizing space and efficiency.  Among a number of proventechnologies migratingfrom consumer electronics into medical devices, flex circuits and flexible printed circuit connectors can help designers optimize space in tightly packaged medical devices.

Occupying three dimensions, flexible printed circuits can be bent around packaging and even folded over to fit in a much smaller device enclosure.  There are a number of other distinct advantages.  Flexible substrates with single, double-sided, and multi-layered circuitry are ideal for high performance signal and power connections at an economical applied cost.  Flex products can also be mounted in through-hole, surface mount and press-fit configurations.

Copper Flex Family Photo

Molex flex circuits give the designer greater flexibility and make electronic interconnection simpler and more reliable.  Unlike hard board containing woven glass fibers that tend to result in signal loss, the materials, such as polyimide, used in flex circuits maintain signal integrity. Polyimide dissipates heat quickly, so flex does not require cooling from both sides.  The flex materials closely match thermal expansion rates, which make it more reliable in hot and cold temperature extremes and temperature fluctuations in mobile healthcare applications.

Device miniaturization using flex circuit technology does require adaptations in production for tighter copper flex spacing and trace width.  A precise develop-etch-strip process is required to etch circuits without removing too much copper.  Incorporating blind and buried vias can help retain flexibility in designs requiring multiple layers on a flex circuit.  Product handling requires extra care to prevent damage to circuit traces.

Using the right materials and manufacturing processes, Molex copper flex delivers sturdy circuitry with high speed capability, impedance control and minimal signal loss for a robust finished medical device.  Ultra-reliable flex circuits are excellent for small, lightweight designs with complex high density circuitry.  Significantly thinner and lighter than a traditional circuit board, flex makes any product naturally lighter, which contributes to overall cost savings and, in some cases, improved patient mobility and comfort.

Representing the successful convergence of consumer electronics and medical equipment, markets for mobile healthcare devices are projected to continue growing.  To learn more, visit www.molex.com/link/copperflexbackplanes.html. Read a recent round-up article highlighting Molex flex technologies for medical device design: http://www.mddionline.com/article/circuits-flex-their-muscles



Read More From The Connector by Molex: http://www.connector.com/2015/03/3d-medical-device-design-efficiency-and-simplicity-using-flexible-print-circuit-technology/#ixzz3UekM4TK4

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    Truly demand of mobile monitoring, and diagnostic devices are on the rise these days. Medical devices have seen amazing changes in terms of size, use and handling. Now bulky one’s are converted into portable, handheld are changed to the wearable technologies that not only ease work of doctors, but makes patient’s life comfortable too.