Molex
  • Products & Partners
  • Manufacturers
  • Molex
  • More
  • Cancel
Molex
Blog Applications or Application?  Selecting a Connector (Part 2)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Molex to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: MolexConnectors
  • Date Created: 12 Jul 2011 2:19 PM Date Created
  • Views 863 views
  • Likes 0 likes
  • Comments 0 comments
  • connectors
  • molex
  • interconnect
Related
Recommended

Applications or Application?  Selecting a Connector (Part 2)

MolexConnectors
MolexConnectors
12 Jul 2011

Previously  I noted the importance of knowing the applied cost of a connector.  Here are the  basic questions I start with when helping to design in a product:

  • Not the number of pins, but the number and type.  Signal speed and  maximum power
  • Amperes at what temperature?  Ambient temperature and cooling are  keyMolex Connector 101
  • What is the connector orientation?  Are we talking mating direction or  position relative to the board?
  • How is the connector going to be applied to the board?  Pick-and-place,  hand placing, or press in?
  • Tin or gold plating?  What is truly needed?  If 50 milliohms with less  than 50 contacts and less than 50 cycles, tin may do the job

Given  the opportunity, here are my additional questions:

  • Application:   Board-to-Board, Wire-to-Board, I/O, or Backplane
  • Any space limitations?
  • Number of signals, speed, and single ended or differential  pairs?
  • How many grounds for signals?
  • How much power?  What about power returns?
  • Any higher voltages (> 50V DC)
  • On the PCB (SMT) or through the PCB (wave solder or  pin-in-paste)?
  • Lead-free reflow processes require reflow temperatures at +260°C, Lead  free wave solder processes need +300°C underneath the PCB
  • Height constraints?  We need to factor in any pick-and-place  processes
  • Are there any wire size restrictions when using wires or cables?  Can I  solder, crimp, or IDT?
  • Environmental restrictions and norms such as UL, glow wire, or  halogen-free?
  • Preference for any contact spacing due to mechanical  tolerances?
  • What is the timeline for samples, ramp up, and volume  production?

As soon as all these questions  are answered, I have a very clear view of what is needed.  I can now search my  favorite web site (molex.com ) for the best product for the application.  Always  considering that the application is not where the product ends up, but how the  product is applied!

  About the author  In his role as Director of Technology Marketing, Herbert Endres supports Sales and Divisions in penetrating new markets for existing products, new products for existing customers and new technologies for new markets.  Read More From The Connector by Molex:
http://dev2.moveo.com/connector/2010/08/applications-or-application-selecting-a-connector-part-2/#ixzz1RttlhIgs