Molex
  • Products & Partners
  • Manufacturers
  • Molex
  • More
  • Cancel
Molex
Blog Is Your System 25Gbps-Ready?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Molex to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: MolexConnectors
  • Date Created: 26 Apr 2011 8:18 PM Date Created
  • Views 856 views
  • Likes 0 likes
  • Comments 0 comments
  • connectors
  • products
  • molex
  • gbps
  • 25
  • high
  • speed
Related
Recommended

Is Your System 25Gbps-Ready?

MolexConnectors
MolexConnectors
26 Apr 2011

As data-transmission speeds continue rising, design  engineers are tasked with delivering scalable systems to ease the  transition from 10Gbps speeds to 25Gbps. The proliferation of high-speed  and broadband systems in telecom, datacom, networking and other  industrial and commercial applications yields greater potential for  signal-integrity problems. As bandwidth, signal speed, and port density  increase, so too the number of links (or ports), upping the likelihood  of signal loss, cross talk, reflection, and mode conversion problems  degrading performance, in addition to the potential for serious  electromagnetic interference (EMI) and power integrity issues.

Commercial viability is also a consideration when upgrading data  transmission. Expensive, over-designed components drive up price and  drive away consumers. Systems must be wisely priced, scalable to 25Gbps,  and deliver desired performance. Each component along the signal path  must be analyzed to determine its effect on the link’s performance.  Fortunately, there are viable predictive analytical tools that provide  accurate, component-level and end-to-end channel models for analyzing  and achieving the optimal balance of price versus performance. Three  analysis tools can help system designers minimize design risk by  confirming that a proposed system will work—and be cost effective.

Passive and active link analysis performs a  sensitivity analysis of each channel component to help determine how  each component affects overall link performance. Link analysis results  can help designers select the optimal components, minimize  time-to-market, and avoid costly mistakes. In the past, link analysis  was typically passive, excluding critical silicon components. Today, AMI  tools allow for more generic platforms to analyze both active and  passive components and compare products and bit error rates of multiple  silicon chip vendors. Molex engineers choose representative “corner  cases” (unique cases that include multiple, worst case scenarios) and  use a passive channel analysis and sensitivity analysis to determine the  appropriate solutions. They then perform active link analysis using AMI  platform tools. Component and channel model correlation studies are  performed. Prototype correlation platforms are built to measure corner  cases to demonstrate the models meet the measurements and will work in  the field.

The second crucial tool is PCB power-integrity analysis,  which is affected by increasing voltages and power consumption, reduced  layer counts (lowers cost, improves via effects) and finer pitch BGA  footprints (port density). Achieving DC voltage and current efficiencies  in 10Gbps systems poses challenges. Supporting 25Gbps systems will  require new power design approaches as driving these speeds over long  distances requires additional power. Power fluctuations affect the  signal delay budget in silicon packages and can produce noise in the  PCB. New modeling tools allow board-level power integrity analysis.  Other tools can help analyze the power delivery and distribution systems  and their effect on system level thermal rise, showing “hot zones” in  different mesh densities that could cause chips to overheat. Emerging  power and cooling technologies, coupled with optimized interconnect  systems that support higher current loads and increasing data rates,  will likely prevail in the market.

Electromagnetic Interference (EMI) analysis is the  most challenging of the three.  EMI (or RFI) is a disturbance that may  interrupt or degrade an electrical circuit due to electromagnetic  conduction or electromagnetic radiation emitted from an external source.  Predictive analytical EMI modeling tools are emerging, but not fully  mature. EMI analysis requires measurements of actual systems in EMI  chambers. Molex components undergo optimization studies that involve  build/measure/model cycles to ensure optimal component performance with  minimal electromagnetic emission. This level of testing is critical in  high-speed internal and external I/O applications, as well as some  internal board-to-board applications. It is particularly important to  minimize the potential effect of EMI inside computing devices. If a  device emits large amounts of EMI, it may not comply with certain FCC  standards.

Leveraging the right tools to support best-in-class 25Gbps  performance requires close collaboration between all of the stakeholders  in the physical link, including OEMs, component suppliers, silicon  suppliers, PCB and raw cable suppliers, and contract manufacturers.  Molex is focused on developing optimized interconnect solutions through  strategic partnerships with these partners to ensure we are providing  “complete solutions” that offer the ideal balance of performance versus  price.


Read More From The Connector by Molex: http://www.connector.com/2011/02/is-your-system-25gbps-ready/#ixzz1Kf74obUO