Molex
  • Products & Partners
  • Manufacturers
  • Molex
  • More
  • Cancel
Molex
Blog Why Solid State Lighting Could Reduce our Energy Needs by 50% over CFLs
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Molex to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: MolexConnectors
  • Date Created: 29 May 2012 1:46 PM Date Created
  • Views 1204 views
  • Likes 1 like
  • Comments 1 comment
  • molex
  • saving
  • lighting
  • led
  • renewable
  • solid
  • state
  • energy
  • transcend
  • cfl
Related
Recommended

Why Solid State Lighting Could Reduce our Energy Needs by 50% over CFLs

MolexConnectors
MolexConnectors
29 May 2012

Several years ago, Molex joined a group of companies and government organizations to prove that Solid-State Lighting could be used to provide excellent quality lighting within our homes and offices while dramatically reducing the energy use in the building. The organization is called the ZEBRA (Zero Energy Building Research Alliance) and is a collaboration between the Department of Energy, Oak Ridge National Laboratories, and Schaad Companies.

The objective of the alliance was to evaluate a variety of building technologies, heating and cooling methods, lighting approaches, and appliances to determine which are the most cost effective and have the highest performance. Four homes were constructed in Oak Ridge, Tennessee just outside the “gates” of the Oak Ridge National Laboratory. There were two pairs of homes with homes one and two being identical in appearance, but with entirely different approaches for the construction of them. The same is true for homes three and four.  If you would like to learn more details about how the homes were constructed, please visit www.zebralliance.com.image

Molex’s part in the project was to provide the lighting design for house #4 as well as provide the light sources for this home. Home #3, which was the sister home for the project, was lit with conventional CFL high efficiency light sources.

At the time this project was being completed in the spring of 2010, the SSL light sources we had available to us were the Molex TranscendTm product line. The LED source for these lights was a single AC LED produced by Seoul Semiconductor. It provided roughly 150 lumens of warm (3000K) light and consumed 4 Watts of power. The efficacy of this light source was not nearly as high as the 60-70 lumens per Watt that we are currently providing but with proper lighting design, we have been able to achieve some amazing results.

Kevin Willmorth of Lumenique LLC did the lighting design for house number 4. He completed a lighting simulation for the home and determined where and how many light sources would be needed. Because each source only provided 150 lumens, more sources would be needed to be able to properly distribute the light throughout the rooms. Today, with our 1200 lumen light sources, we could easily reduce the number of sources required to light the same space.

After the homes were completed in the summer of 2010, the public was allowed to tour the homes and to provide comments and feedback on the “look and feel” of the demonstration projects. The feedback from the visitors was very positive on the look of home number 4. They liked the “dramatic” look of the lighting in that the lights were directly at the locations where light was needed.

As we all know, CFL lighting is very non-directional and when it is placed into a room, the fluorescent sources light the ceiling, walls, and fixtures, as much as they light the surfaces, which is where we would actually like to have light.  Please see the two attached pictures to see the difference in the look of home 3 and 4.

 

image
CFL Space- Mixed CFL sources= 192W - 14 Fc@ dining table

 

             

 

 

LED Space - 19 Lights @4W=76W - 38Fc@dining table
LED Space - 19 Lights @4W=76W - 38Fc@dining table

 

Some of the comments we received is that the LED space had more drama, more task light and less glare. But was also of interest to the researchers was that it used 60% less energy to do a better job of lighting the space.

One year later in September of 2011, we have one year of data. The homes have been monitored and data collected on their performance for one year. Dr. Bill Miller from Oak Ridge, who was responsible for the design and build of the homes, called us and said that the performance of the LED lit home was even better than they had expected. The data shows that the LED-lit home actually uses 80% less energy than the CFL-lit home. This result is dramatic if one considers the fact that the CFL is thought to be the most energy efficient light source currently available.

It is expected that as the cost of Solid-State Lighting comes down over the next several years to the point that this will be the only good option for high quality, dimmable, and low energy use lighting, that the United States could reduce its energy use by the equivalent of 150 large power plants.

Although it is taking longer than most of us have expected it to, Solid-State Lighting will be ready to replace both incandescent lights and CFLs in the next several years. With efficacies of 80 lumens per Watt, they are 6 times more efficient than our old “bulbs” and now they have been shown to be at least 3 times as efficient as CFLs.

 

avatar

About the author

Victor Zaderej Advanced Solid State Lighting Development Manager With over 30 years of experience in the design of innovative new products, Vic specializes in the development of next generation solid state light sources within Molex’s Lighting Group. Advanced Solid State Lighting Development Manager With over 30 years of experience in the design of innovative new products, Vic specializes in the development of next generation solid state light sources within Molex’s Lighting Group.



Read More From The Connector by Molex: http://www.connector.com/2011/10/why-solid-state-lighting-could-reduce-our-energy-needs-by-50-over-cfls/#ixzz1wGuv63Vf

  • Sign in to reply
  • DAB
    DAB over 14 years ago

    I agree that LED's are much better than CFL's, but if you want to go to the real money saver, we should build lights powered by radioactive waste material.

    About thirty years ago, I worked with some physicists and engineers and we found that you could take a small amount of low level radioactive material, enclose it in leaded glass with some neon gas and phosphorous for a zero power light.  They would be perfect for any area where lighting is needed 24/7 and have a life expectancy of centuries/millenia.

    It also solves to problem of storage.  The amount in each bulb is very small that there is almost no risk of contamination from a broken bulb.

    The lights would be distributed over a huge area, thus keeping the radiation hazard to a minimum.

     

    So if you want to kill two birds with one stone, lets do it right and reuse the energy sources at hand.

     

    Just my opinion,

    DAB