Molex
  • Products & Partners
  • Manufacturers
  • Molex
  • More
  • Cancel
Molex
Forum SFP(+) to cool or not to cool?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Molex to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 10 subscribers
  • Views 959 views
  • Users 0 members are here
  • connectors
  • herbert_endres
  • sfp
  • sink
  • molex
  • heat
  • cxp
  • qsfp
  • rucksack
  • sfp_cages
Related

SFP(+) to cool or not to cool?

MolexConnectors
MolexConnectors over 16 years ago

With SFP cages  comes always the question whether cooling is necessary or not. There is  no clear answer this question. Mainly because there are several  parameters which have to be taken into consideration:

1.       The heat dissipation of one SFP insert can go from zero  (copper cable) to approx. 2 watts (when using a twin bi-directional LC  insert)

2.       The equipment practice may be a rack with vertical daughter  cards or a pizza box with only a main board or with additional mezzanine  cards on top

3.       The number of ports on a daughter card/mezzanine board

4.       The density of the ports, whether these are single cages  with space in between, ganged cages, or stacked and ganged cages

5.       The airflow in the system, which is always bottom up in a  rack, but it may be different in a pizza box (East->West or  Rear-Front)

6.       The ambient temperature (fan supported approx. +40°C), the  maximum temperature of the insert (typically +70°C) and the air flow  speed

7.       Last but not least the “swelter effect” e.g. the first SFPs are heating up the ones at the end of the airflowimage

We at Molex did a lot of simulations in our thermal labs to  understand the results of the above parameters. However, still we do not  have a universal recipe to have a black and white solution for the  problem. A few guidelines may help.

As long as we are talking single cages with space in between, we are  on the safe side if the dissipated heat is below one watt per insert.  When you start ganging these cages, it is still no problem, assuming you  have a copper ground plane underneath the inserts that distributes the  heat away.

At the moment you are above one watt per insert, care should be  taken, especially when ganged SFP cages are your free choice or forced  decision. Investigating the configuration of a fully SFP-loaded front  panel with inserts above 1.5 watts heat dissipation each insert, we  immediately recognized we have to cool the inserts.

The first hurdle was to find a good thermal connection between the insert and the heat sink. Only QSFP inserts are designed from the beginning to have a flat and smooth  surface on top to have an intimate contact to a heat sink. SFP inserts  do not always have this and – even worse – some inserts have the  manufacturing label on top, which is not a good heat conductor. You may  improve the situation with conductive heat cushions, but the thermal  contact is questionable.

image
Heat Sink Cushion

The  second hurdle was – under a defined insert with a defined heat cushion –  to select the right heat sink in the given environment. The environment  was a rack with vertical daughter cards and 24 ganged SFP ports (4  cages each 6 ports).

image
SFP Thermal Test Bench

Knowing  the height of only 15,2mm above the board, it was clear that a heat  sink on top of the SFP cages just blocks the airflow, which is worse  than using no heat sinks. The heat sinks must have fingers (no ribs) to  create turbulences and get a better thermal conductivity to the air.  Finally, we decided to go for “rucksack” heat sinks since a lower  profile with a rucksack is more efficient than a higher heat sink just  above the cages.

We tested several heat sink configurations and found the lower  profile longer rucksack as the best performer. However, even with the  extended rucksack we had to apply a baffle in order to squeeze the  airflow onto the rucksack area, which is shown on the sketch “Rucksack  with baffle”

image
No Rucksack
image
Rucksack short
image
Rucksack extended
Heat Sink Comparison
Heat Sink Comparison

Last but not least, a heat sink comparison matrix was created which showed clearly:

a)      Heat sinks are sometimes worse than no heat sinks

b)      Without a baffle, the airflow bypasses the heat sink area and airflow is in vain

c)       More baffles do not improve the cooling effect

d)      Most critical is the “swelter effect” in an arrangement as  simulated; the lower SFPs heat up the upper SFPs when airflow is not  controlled

Molex is offering a large variation of cages for SFP, QSFP and CXP.  We investigated, simulated and verified thermal issues with stacked and  ganged configurations of SFP and QSFP as we foresee a wider usage of  cages in the industry. Not only with heat dissipation from fiber optic  transceivers, but also with dissipated heat from active copper cables  where equalizers are integrated into the cable plugs.

 

Read more postings like this on THE CONNECTOR