Molex
  • Products & Partners
  • Manufacturers
  • Molex
  • More
  • Cancel
Molex
Forum Are Discrete Wires Too Outdated For Handheld Devices?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Molex to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 10 subscribers
  • Views 494 views
  • Users 0 members are here
  • connectors
  • molex
  • interconnect
  • microminiature
  • connector
  • pico-ezmate
  • interconnects
  • fpc
  • electrical
Related

Are Discrete Wires Too Outdated For Handheld Devices?

MolexConnectors
MolexConnectors over 16 years ago

Inside a tightly-packaged modern smartphone, flexible circuitry  dominates the space, connecting various modules to the main logic board  using microminiature board-to-board and FPC connectors.  The space-saving and lightweight nature of these  components for relatively high circuit size interconnects has certainly  contributed toward the never-ending drive for miniaturization.  Yet you  still occasionally see some conventional discrete wires.  Modules such  as batteries, speakers and vibra motors are still sometimes connected to  the main logic board by discrete wires.  These modules may be attached  to the chassis of the device, and the flexibility and cost-effective  nature of discrete wires provides phone designers the freedom to  position such modules almost anywhere.  image

imageDesigners  may want to distance certain components from RF modules, which could  otherwise negatively impact the performance of their device.  Thus,  there is still a need for small, low profile wire-to-board interconnect  solutions.  One of the latest products from Molex, called Pico-EZmateTm,  is an ultra-low profile, right angle wire-to-board connector in 1.20mm  pitch, but with a vertical mating direction.  It has a mated height of  1.55mm, and is available in 2 through 5 circuit versions (a 6-circuit  version is also available with a mated height of 1.65mm).  It is  halogen-free and glow-wire compliant.  The vertical mating direction is  design-friendly because it provides freedom to position other components  around the connector on the printed circuit board, whereas conventional  right angle wire-to-board connectors with a horizontal mating action  typically have to be placed around the edge of the printed circuit  board.  Needless to say, the vertical mating direction is also  operator-friendly for the final assembly operation.

Molex’s existing Pico-EZmate connector is being used in applications  as diverse as smartphones, notebook PCs, tablet PCs, e-book readers,  medical devices, gaming machines, barcode readers, digital cameras,  navigation devices, lighting, wireless modems and many, many more.  For  these applications, the existing connector proved to be quite small  enough.  But the question now is whether customers in the future will  require an even smaller version of this already small, yet manageable  product.  Smartphone designers are interested in further component  miniaturization.  But will further miniaturization be practical for  their manufacturing partners, from a final assembly point of view?  What  is your opinion?

Visit "The Connector" to read more blog postings like this from the connector experts at Molex.