Molex
  • Products & Partners
  • Manufacturers
  • Molex
  • More
  • Cancel
Molex
Forum Pros and Cons of Eliminating Hazardous Substances
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Molex to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 10 subscribers
  • Views 523 views
  • Users 0 members are here
  • connectors
  • pvc
  • molex
  • cfr
  • green
  • bfr
Related

Pros and Cons of Eliminating Hazardous Substances

MolexConnectors
MolexConnectors over 15 years ago

 

imageSo  we previously learned some of the risks of BFRs,  CFRs, and PVC.  What  is Molex doing to mitigate these risks?  First, let's take  a look at  the terminology used and some  alternatives.

Terminology /  Definitions

So we want to remove these substances that could cause  harm.  What  do we call this trend?  Well, it seems everyone has come up with  their  own term!  Halogen-Free, Low-Halogen, and BFR/CFR/PVC-Free are common   terms used.  They're all a mouthful, and some don't even accurately  describe the  situation.  Also, what's the acceptable level of these  substances, knowing that  unintentional impurities can exist?  And what  about other brominated and  chlorinated substanceimages?

To be safe, Molex has adopted a conservative definition  for this  trend – one that meets all of our customers' definitions.  A product   that has less than 900 ppm (0.09%) bromine, less than 900 ppm chlorine,  and less  than 1500 ppm (0.15%) of bromine and chlorine combined, meets  the requirement.   For now, we call these products 'Halogen-Free' or   'Low-Halogen.'

BFR/CFR Alternatives

We've decided we want to get away from brominated and  chlorinated  flame retardants.  We'll just use another material ... easy right?    Well, not exactly.  Many Molex connectors use a brominated flame  retardant  (remember – it's used to slow down the spread of fire, so  using a BFR sounds  like a good idea!).  There are three ways we can get  away from  BFRs:

  • Some plastics are  inherently flame-retardant (in other  words, a flame retardant doesn't  need to be added to slow the spread of  fire).  Sounds like an easy choice!   Except that those plastics may  have completely different properties (some are  very brittle and might  break).  And, of course, they're typically more  expensive.
  • What about using a  different kind of flame retardant?  Molex has  been working with its plastic  suppliers, who have been developing  non-brominated, non-chlorinated flame  retardants.  Some of these show  promise and are currently being used.  Again,  there are differences, so  each product needs to be  re-evaluated.
  • The third option is  to remove the flame retardant entirely.  If the  connector is used in an  application where a fire isn't likely to  happen, or the current is low enough,  the plastic may not even need a  flame retardant.  Plastics already exist without  flame retardants, and  are used in many applications.

PVC Alternatives

We've also decided we want to replace PVC with another  material –  one that's just as flexible.  Well, we can't have everything – the   alternatives could be up to ten times as expensive!  Of course, over  time,  prices will drop as supply catches up, but in the meantime, a  premium will be  paid for the substitutes.  Some examples:

  • Polyethylene
  • Fluorinated polymers  (FEP, ETFE, PVDF)
  • Ethylene  propylene diene elastomer (EPDM)
  • Polyurethane

Molex's Activities

Molex has been working with its suppliers and customers  to design new  products that don't contain these substances that could pose  hazards.   We have experience in creating a connector that doesn't have  brominated  or chlorinated flame retardants, and we've worked with cables that   aren't PVC.  Certainly, there are challenges, and not every material can  be  easily replaced.  In the meantime, if a Molex customer needs a  product without  BFRs, CFRs, and PVC, just let your account manager know  – he or she will be able  to work with you to meet your needs!

 

Read More From The Connector by Molex: http://www.connector.com/2010/08/pros-and-cons-of-eliminating-hazardous-substances/#ixzz17S0txwu8