Molex
  • Products & Partners
  • Manufacturers
  • Molex
  • More
  • Cancel
Molex
Forum Barrier terminal strip rating
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Molex to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 11 subscribers
  • Views 753 views
  • Users 0 members are here
Related

Barrier terminal strip rating

e14 Contributor
e14 Contributor over 14 years ago

I want to connect four wires to a Molex barrier terminal strip, (38280-0104). The wires are 24 AWG 1000 VDC rated. The voltage being applied is 1000 VDC @ .5 Amp MAX- 500 watts. The Molex 28 Series is rated at 600 Vrms @ 50 Amp 3000 watts. Is the watt rating allow for safe connection considering the lower amperes or is the voltage rating absolute.

  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 14 years ago

    You are fairly close to the limit of current transfer of 28 AWG of 0.577A (power transmission). Many people like to have a margin of 50-100% on top of the carry capacity. I would recommend 21 or 22 AWG wire instead.

     

    Also, with 28 AWG you will experience a higher resistance. If you only want to experience a 5% voltage drop on the wire (say 1meter long) you will need something along 21 AWG. Which will handle around 500W.

     

    REFERENCE this chart for power carry characteristics of wires.

    G gaugeConductor
    Diameter Inches
    Conductor
    Diameter mm
    Ohms per 1000 ft.Ohms per kmMaximum amps for chassis wiringMaximum amps for
    power transmission
    Maximum frequency for
    100% skin depth for solid conductor copper
    OOOO0.4611.6840.0490.16072380302125 Hz
    OOO0.409610.403840.06180.202704328239160 Hz
    OO0.36489.265920.07790.255512283190200 Hz
    00.32498.252460.09830.322424245150250 Hz
    10.28937.348220.12390.406392211119325 Hz
    20.25766.543040.15630.51266418194410 Hz
    30.22945.826760.1970.6461615875500 Hz
    40.20435.189220.24850.8150813560650 Hz
    50.18194.620260.31331.02762411847810 Hz
    60.1624.11480.39511.295928101371100 Hz
    70.14433.665220.49821.63409689301300 Hz
    80.12853.26390.62822.06049673241650 Hz
    90.11442.905760.79212.59808864192050 Hz
    100.10192.588260.99893.27639255152600 Hz
    110.09072.303781.264.132847123200 Hz
    120.08082.052321.5885.20864419.34150 Hz
    130.0721.82882.0036.56984357.45300 Hz
    140.06411.628142.5258.282325.96700 Hz
    150.05711.450343.18410.44352284.78250 Hz
    160.05081.290324.01613.17248223.711 k Hz
    170.04531.150625.06416.60992192.913 k Hz
    180.04031.023626.38520.9428162.317 kHz
    190.03590.911868.05126.40728141.821 kHz
    200.0320.812810.1533.292111.527 kHz
    210.02850.723912.841.98491.233 kHz
    220.02540.6451616.1452.939270.9242 kHz
    230.02260.5740420.3666.78084.70.72953 kHz
    240.02010.5105425.6784.19763.50.57768 kHz
    250.01790.4546632.37106.17362.70.45785 kHz
    260.01590.4038640.81133.85682.20.361107 kH
    270.01420.3606851.47168.82161.70.288130 kHz
    280.01260.3200464.9212.8721.40.226170 kHz
    290.01130.2870281.83268.40241.20.182210 kHz
    300.010.254103.2338.4960.860.142270 kHz
    310.00890.22606130.1426.7280.70.113340 kHz
    320.0080.2032164.1538.2480.530.091430 kHz
    Metric 2.00.007870.200169.39555.610.510.088440 kHz
    330.00710.18034206.9678.6320.430.072540 kHz
    Metric 1.80.007090.180207.5680.550.430.072540 kHz
    340.00630.16002260.9855.7520.330.056690 kHz
    Metric 1.60.00630.16002260.9855.7520.330.056690 kHz
    350.00560.142243291079.120.270.044870 kHz
    Metric 1.4.00551.14033911140.260.043900 kHz
    360.0050.127414.813600.210.0351100 kHz
    Metric 1.25.004920.125428.214040.200.0341150 kHz
    370.00450.1143523.117150.170.02891350 kHz
    Metric 1.12.004410.112533.817500.1630.02771400 kHz
    380.0040.1016659.621630.130.02281750 kHz
    Metric 1.003940.1000 670.221980.1260.02251750 kHz
    390.00350.0889831.827280.110.01752250 kHz
    400.00310.07874104934400.090.01372900 kHz

     

    Good Luck

     

    Cabe

    http://twitter.com/Cabe_e14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Catwell
    0 Catwell over 14 years ago

    You are fairly close to the limit of current transfer of 28 AWG of 0.577A (power transmission). Many people like to have a margin of 50-100% on top of the carry capacity. I would recommend 21 or 22 AWG wire instead.

     

    Also, with 28 AWG you will experience a higher resistance. If you only want to experience a 5% voltage drop on the wire (say 1meter long) you will need something along 21 AWG. Which will handle around 500W.

     

    REFERENCE this chart for power carry characteristics of wires.

    G gaugeConductor
    Diameter Inches
    Conductor
    Diameter mm
    Ohms per 1000 ft.Ohms per kmMaximum amps for chassis wiringMaximum amps for
    power transmission
    Maximum frequency for
    100% skin depth for solid conductor copper
    OOOO0.4611.6840.0490.16072380302125 Hz
    OOO0.409610.403840.06180.202704328239160 Hz
    OO0.36489.265920.07790.255512283190200 Hz
    00.32498.252460.09830.322424245150250 Hz
    10.28937.348220.12390.406392211119325 Hz
    20.25766.543040.15630.51266418194410 Hz
    30.22945.826760.1970.6461615875500 Hz
    40.20435.189220.24850.8150813560650 Hz
    50.18194.620260.31331.02762411847810 Hz
    60.1624.11480.39511.295928101371100 Hz
    70.14433.665220.49821.63409689301300 Hz
    80.12853.26390.62822.06049673241650 Hz
    90.11442.905760.79212.59808864192050 Hz
    100.10192.588260.99893.27639255152600 Hz
    110.09072.303781.264.132847123200 Hz
    120.08082.052321.5885.20864419.34150 Hz
    130.0721.82882.0036.56984357.45300 Hz
    140.06411.628142.5258.282325.96700 Hz
    150.05711.450343.18410.44352284.78250 Hz
    160.05081.290324.01613.17248223.711 k Hz
    170.04531.150625.06416.60992192.913 k Hz
    180.04031.023626.38520.9428162.317 kHz
    190.03590.911868.05126.40728141.821 kHz
    200.0320.812810.1533.292111.527 kHz
    210.02850.723912.841.98491.233 kHz
    220.02540.6451616.1452.939270.9242 kHz
    230.02260.5740420.3666.78084.70.72953 kHz
    240.02010.5105425.6784.19763.50.57768 kHz
    250.01790.4546632.37106.17362.70.45785 kHz
    260.01590.4038640.81133.85682.20.361107 kH
    270.01420.3606851.47168.82161.70.288130 kHz
    280.01260.3200464.9212.8721.40.226170 kHz
    290.01130.2870281.83268.40241.20.182210 kHz
    300.010.254103.2338.4960.860.142270 kHz
    310.00890.22606130.1426.7280.70.113340 kHz
    320.0080.2032164.1538.2480.530.091430 kHz
    Metric 2.00.007870.200169.39555.610.510.088440 kHz
    330.00710.18034206.9678.6320.430.072540 kHz
    Metric 1.80.007090.180207.5680.550.430.072540 kHz
    340.00630.16002260.9855.7520.330.056690 kHz
    Metric 1.60.00630.16002260.9855.7520.330.056690 kHz
    350.00560.142243291079.120.270.044870 kHz
    Metric 1.4.00551.14033911140.260.043900 kHz
    360.0050.127414.813600.210.0351100 kHz
    Metric 1.25.004920.125428.214040.200.0341150 kHz
    370.00450.1143523.117150.170.02891350 kHz
    Metric 1.12.004410.112533.817500.1630.02771400 kHz
    380.0040.1016659.621630.130.02281750 kHz
    Metric 1.003940.1000 670.221980.1260.02251750 kHz
    390.00350.0889831.827280.110.01752250 kHz
    400.00310.07874104934400.090.01372900 kHz

     

    Good Luck

     

    Cabe

    http://twitter.com/Cabe_e14