Moto Mods
  • Products & Partners
  • Manufacturers
  • Moto Mods
  • More
  • Cancel
Moto Mods
Documents Moto Mods - Transform What a Smartphone Can Do With the Moto Mods Development Kit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Moto Mods to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: KJackson
  • Date Created: 20 Jul 2016 8:23 AM Date Created
  • Last Updated Last Updated: 6 Oct 2021 8:52 PM
  • Views 9137 views
  • Likes 7 likes
  • Comments 15 comments
Related
Recommended

Moto Mods - Transform What a Smartphone Can Do With the Moto Mods Development Kit

Here at element14 we’ve been lucky enough to get our hands on one of the first new Moto Z phones and the Moto Mods Development Kit to go with it. Motorola officially state 5.2mm for the Moto Z phone, whereas we actually measured it to a very impressive 5.19mm. What’s 0.01mm amongst friends when we are here to add a few mm to it’s waist size with the new Moto Mods Development Kit and personality cards for developers exclusively available from element14?

 

image

 

So what is the Moto Mods Development Kit?

The Moto Mods Development Kit is part of Motorola’s Moto Z family, it provides the tools for anyone from makers to established design houses to develop their own Moto Mod, IoT application, or to redefine what a smartphone can do.

 

The purpose of Moto Mod platform is to enable innovative makers and developers  to transform the way people use smartphones. Simply by snapping on the Moto Mods Development Kit to the back of the Moto Z phone, users are provided with endless possibilities to contribute to and design the future of smartphone technology. This is all made possible by the revolutionary Moto Mod Smart Surface.

 

The Smart Surface is a revolutionary concept that enables connectivity, attachment and alignment of Moto Mods. It supports a hot swap architecture without the clunky look and feel of traditional modular systems. All communication and power travels over a system of pins made from 23K gold with a hydrophobic nano coating. A metallic back plate serves as a magnetic attachment point.

 

The unique ‘snap on’ capability of Moto Mods, customizing the phone without the need for internal integration, opens the market up to developers across the globe to design and commercialize their own mods, from a blood pressure monitor or game controller, to a credit card payment system or air pollution sensor.

 

The Moto Mod platform has been designed to ensure the Moto Z phone maintains good wireless, audio and imaging performance whenever a commercial Moto Mod is snapped to the back of the phone.

 

For more in depth details on the Mod Mods concept please continue reading below, and please note that you will require a Moto Z smartphone to operate the Moto Mods Development Kit and the Personality Cards.

Buy Now

View more and discuss.

 

The Moto Mods Platform

The Moto Mods platform allows you to design and build your own Moto Mods. As a developer, you’ll be able to design Moto Mods that include a superspeed USB device or a small sensor  — and everything in between. Read more about the system architecture.

 

Moto has integrated support for many Moto Mod protocols directly into Android. APIs have also been added to enable developers to build their own applications and communicate with their custom-designed Moto Mod. Developers can host their Android apps in the Google Play store. These apps are automatically downloaded and installed when the associated Moto Mod is attached for first time. Read more about thehttp://developer.motorola.com/explore/softwareMoto Mods SDK here.

image

 

Make Anything

Moto Z phones are designed to be compatible with any Moto Mod you create and certify through Motorola. The possibilities are practically limitless, from infrared cameras, e-ink displays, game controllers and printers to metal detectors, inventory tag readers, blood pressure monitors and even air pollution sensors.

 

 

image

The Moto Mods

When attached, the capability of the Moto Z is enhanced and extended by the unique hardware in your Moto Mod.

 

The Moto Mod system is architected around a dual processor computing system that controls your unique hardware and manages communication with the Moto Z. You will need to create your own firmware, customized to your Moto Mod design. To simplify this process, Moto provides an easy-to-learn development environment along with the necessary tools.

 

Your Moto Mod firmware can also be updated by any Moto Z using a custom Android API. This firmware can be hosted in the cloud or embedded into an Android app enabling you to roll out new experiences, features or bug fixes.

 

More info on the Moto Mods firmware.

 

 

The Moto Mods Development Kit

In tandem with the Moto website, the Moto Mods Development Kit (MDK) provides the resources that a developer needs to prototype an idea and develop a commercial Moto Mod. Together with a Moto Z, the MDK is the ideal starting point for developing your own Moto Mod.

imageThere are 3 parts to the Moto Mods Development Kit: the Reference Moto Mod, a Perforated Card and an example cover.

 

Getting started is easy, simply connect the Mods Development Kit to your Moto Z and you’ll be able to test out and explore the “Hello, World!” example.  From there you can start developing your own Moto Mod prototype. You can also design and build your own 3D-printed housing to protect your prototype during development.

 

There are two ways to get started on your prototype using the Reference Moto Mod with either the Perforated Board or HAT Adapter Board. For more details on how to use the MDK please click here.

 

 

Perforated Board

image

The Perforated Board is the primary vehicle for development of your MDK Project (one is included with the MDK, and further spare boards are available to purchase).

 

Perfect for experimentation, the Perforated Board is a blank slate for soldering your own electrical components in place, it brings the 80-pin connector to an accessible surface.

 

With 26 rows of solder points at 2.54mm pitch and power bus pins on each side, there is plenty of space for you to get your idea up and running.

Buy Now

View more and discuss.

HAT Adapter Board

image

The HAT Adapter Board allows you to use existing Raspberry PiTm HATs with the MDK.

 

Motorola has introduced the HAT Adapter Board to further extend the design opportunities available through the MDK, by allowing you to connect existing Raspberry Pi HATs to the MDK.

 

The HAT Adapter Board enables you to attach a wide variety of Raspberry Pi HATs to your Moto Mods Development Kit. It includes the standard 40-pin header, 15-pin camera and 15-pin display header in the exact dimensions and placement.

 

This card plugs into the 80 pin connector that comes with the Reference Moto Mod. You will need to port or create the Moto Mod firmware (and associated Android application) to get your chosen HAT up and running.

Buy Now

View more and discuss.

 

 

Personality Cards

To help you on your way, Motorola has created several Personality Cards that can be inserted into the Reference Moto Mod.

 

Personality Cards connect directly to the Reference Moto Mod and serve as great examples of how you can build your own prototype.

 

 

Each of these Personality Cards is a end-to-end example with open-sourced Moto Mod firmware and an Android app.

 

There are four example Personality Cards:

 

1. Audio Personality Card - Shows how to integrate a speaker and audio output into your MDK Project.

The Audio Personality Card example shows how simple it is to add a loudspeaker or other audio device to your project.

Buy Now   View more and discuss.

 

2. Battery Personality Card - Shows how to integrate a rechargeable battery into your MDK Project.

The Battery Personality Card example shows how you would extend the life of your phone or use it to run your Moto Mod even when it's not attached to a Moto Z.

Buy Now   View more and discuss.

 

3. Display Personality Card - Shows how to integrate a display and backlight into your MDK Project.

The Display Personality Card example shows how to interface and control a display and backlight.

Buy Now   View more and discuss.

 

4. Temperature Sensor Personality Card - Shows how to integrate a custom temperature sensor into your MDK Project.

The Temperature Sensor Personality Card is an example that shows how you would connect a unique sensor on your device and graph it on your phone’s screen.

Buy Now   View more and discuss.

 

Initially the Moto Mods Development Kit, Perforated Board, HAT Adapter Board, and Personality Cards will be available for sale in the US via our Newark element14 and MCM businesses. Global availability for these products is due to follow in autumn 2016.

 

Raspberry Pi is a trademark of the Raspberry Pi Foundation

  • smartphone
  • motorola
  • moto mods hat
  • battery
  • temperature sensor
  • display
  • moto mods
  • personality card
  • hat
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 10 years ago +1
    This sounds great ! But I am curious to know the price, and eventually a bundle smartphone + kit Enrico
  • spannerspencer
    spannerspencer over 10 years ago in reply to balearicdynamics +1
    Hey man! Just at the moment, it's only available in the US. But if you change your country to United States (clicking the flag icon in the top right corner of the page) it'll show you the "Buy Now" buttons…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to spannerspencer +1
    Intriguing and working ! It's a good price, taking in account that it's a novelty. Now I should just find a way to ship from USA to Netherlands... Enrico
  • cvhk
    cvhk over 9 years ago in reply to jackeen

    Just wish i could find a supplier in the Netherlands, El14 mentiones 2 dealer bu they do not supply thisspecific item...,:-(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colehg
    colehg over 9 years ago in reply to colehg

    Oh and also, instead of an extra ram mod why not just make a mod that has all the components a computer needs? I mean, it's kind of a challenge to fit everything in the mod but I assemble and disassemble computers, seems like there is a way with all the new tech and smaller processers, etc. Probably just my ego but I bet something like what I just said actually will happen and no one will even mention me. But just another idea.

     

    Thankyou

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colehg
    colehg over 9 years ago

    Hey, I'm only a kid, I'm 12, so no one will probably read this comment but I have an idea for a Moto modTm and I would like to share it. So because I am 12 I like VR headsets... What if there was a mod that transformed the phone into a VR, now I know this sounds kind of complicated if not impossible 'he is just a kid he has no idea how anything works' which I probably don't but, I think it would be really cool for a VR Moto mod, just wanted to get out my idea. Thanks for reading this.

     

    -Cole

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsc
    rsc over 9 years ago

    How about a Moto-Z road test?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Sparkylabs

    deal image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Sparkylabs
    Sparkylabs over 10 years ago in reply to Jan Cumps

    Ow come on, lets make it at least 0.05mm then you can measure it without breaking the bank image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Sparkylabs

    Ow come on, Simon. Lighten up and save your rants for things that have a substance of 0.02mm or more....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Sparkylabs
    Sparkylabs over 10 years ago

    I can't actually believe that the first paragraph of this so-called article. This is supposed to be a blog for engineers but clearly the journalist and clearly they are just a journalist not an engineer or anybody with an engineering background hasn't the foggiest about measurements. Tell me element 14 what did you measure this 0.01 mm difference with? Was it a caliper? You do realise that most calipers do not have much better accuracy than .05 mm and where did you measure across the phone? It wasn't across a flexible part by any chance what it? 0.01 mm is what we call measurement noise but I would hardly expect the author of this article to understand that concept. Perhaps element 14 and its subsidiary companies like Farnell in the UK to concentrate more on actually doing what they are supposed to do: stock goods, report correct stock quantities on their website and ship said stock to customers in the expected packaging. Why waste time on bull *** like this when you can't even be a good stockist. The only reason I buy from you is because RS is no better and the only people who actually know what they are doing art in America and the carriage is far too expensive for small orders. If it weren't for that you in the UK would be right out of business because you are one of the most unreliable and unhelpful suppliers around. God I would even pay 5% more for my parts if I were guaranteed that my order would go to plan rather than every single order not going to plan but then it seems that you are spending more time working out that something is .01 mm different from a claim despite the fact you are probably measuring it with an instrument that cannot accurately record a measurement of .01 mm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • venkatcse539
    venkatcse539 over 10 years ago

    Is it possible to create  a processor mod or ram increase mod for z devices

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jackeen
    jackeen over 10 years ago in reply to spannerspencer

    I'm pleased to say that the Moto Mods Development Kit and accessories are now available to purchase in the USA, China and Europe from element14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>